otNetifAddress Struct Reference
This structure represents an IPv6 network interface unicast address.
#include <
include/openthread/ip6.h
>
Public Attributes |
|
| otIp6Address | mAddress |
|
The IPv6 unicast address.
|
|
| uint8_t | mPrefixLength |
|
The Prefix length (in bits).
|
|
| bool | mPreferred : 1 |
|
TRUE if the address is preferred, FALSE otherwise.
|
|
| bool | mValid : 1 |
|
TRUE if the address is valid, FALSE otherwise.
|
|
| bool | mScopeOverrideValid : 1 |
|
TRUE if the mScopeOverride value is valid, FALSE otherwise.
|
|
| unsigned int | mScopeOverride : 4 |
|
The IPv6 scope of this address.
|
|
| bool | mRloc : 1 |
|
TRUE if the address is an RLOC, FALSE otherwise.
|
|
| struct otNetifAddress * | mNext |
|
A pointer to the next network interface address.
|
|
This structure represents an IPv6 network interface unicast address.
The documentation for this struct was generated from the following file:
-
include/openthread/
ip6.h