otPlatBleGapConnParams Struct Reference

This structure represents BLE connection parameters.

#include < include/openthread/platform/ble.h >

Public Attributes

uint16_t mConnMinInterval
Preferred minimum connection interval in OT_BLE_TIMESLOT_UNIT units.
uint16_t mConnMaxInterval
Preferred maximum connection interval in OT_BLE_TIMESLOT_UNIT units.
uint16_t mConnSlaveLatency
Slave Latency in number of connection events.
uint16_t mConnSupervisionTimeout
Defines connection timeout parameter in OT_BLE_CONN_SUPERVISOR_UNIT units.

This structure represents BLE connection parameters.

Member Data Documentation

◆ mConnMaxInterval

uint16_t otPlatBleGapConnParams::mConnMaxInterval

Preferred maximum connection interval in OT_BLE_TIMESLOT_UNIT units.

Shall be in OT_BLE_CONN_INTERVAL_MIN and OT_BLE_CONN_INTERVAL_MAX range.

◆ mConnMinInterval

uint16_t otPlatBleGapConnParams::mConnMinInterval

Preferred minimum connection interval in OT_BLE_TIMESLOT_UNIT units.

Shall be in OT_BLE_CONN_INTERVAL_MIN and OT_BLE_CONN_INTERVAL_MAX range.

◆ mConnSlaveLatency

uint16_t otPlatBleGapConnParams::mConnSlaveLatency

Slave Latency in number of connection events.

Shall not exceed OT_BLE_CONN_SLAVE_LATENCY_MAX value.

◆ mConnSupervisionTimeout

uint16_t otPlatBleGapConnParams::mConnSupervisionTimeout

Defines connection timeout parameter in OT_BLE_CONN_SUPERVISOR_UNIT units.

Shall be in OT_BLE_CONN_SUPERVISOR_TIMEOUT_MIN and OT_BLE_CONN_SUPERVISOR_TIMEOUT_MIN range.


The documentation for this struct was generated from the following file:
  • include/openthread/platform/ ble.h