This structure represents link-specific information for messages received from the Thread radio.
#include <
include/openthread/link.h
>
Public Attributes | |
uint16_t | mPanId |
Source PAN ID. | |
uint8_t | mChannel |
802.15.4 Channel | |
int8_t | mRss |
Received Signal Strength in dBm. | |
uint8_t | mLqi |
Link Quality Indicator for a received message. | |
bool | mLinkSecurity |
Indicates whether or not link security is enabled. | |
uint8_t | mTimeSyncSeq |
The time sync sequence. | |
int64_t | mNetworkTimeOffset |
The time offset to the Thread network time, in microseconds. |
This structure represents link-specific information for messages received from the Thread radio.
The documentation for this struct was generated from the following file:
- include/openthread/
link.h