This module includes functions that control link-layer configuration.

Classes

struct otThreadLinkInfo
This structure represents link-specific information for messages received from the Thread radio.
struct otMacFilterEntry
This structure represents a Mac Filter entry.
struct otMacCounters
This structure represents the MAC layer counters.
struct otActiveScanResult
This structure represents a received IEEE 802.15.4 Beacon.
struct otEnergyScanResult
This structure represents an energy scan result.

Macros

#define OT_MAC_FILTER_FIXED_RSS_DISABLED 127
Used to indicate no fixed received signal strength was set.
#define OT_MAC_FILTER_ITERATOR_INIT 0
Initializer for otMacFilterIterator.

Typedefs

typedef struct otThreadLinkInfo otThreadLinkInfo
This structure represents link-specific information for messages received from the Thread radio.
typedef uint8_t otMacFilterIterator
Used to iterate through mac filter entries.
typedef enum otMacFilterAddressMode otMacFilterAddressMode
Defines address mode of the mac filter.
typedef struct otMacFilterEntry otMacFilterEntry
This structure represents a Mac Filter entry.
typedef struct otMacCounters otMacCounters
This structure represents the MAC layer counters.
typedef struct otActiveScanResult otActiveScanResult
This structure represents a received IEEE 802.15.4 Beacon.
typedef struct otEnergyScanResult otEnergyScanResult
This structure represents an energy scan result.
typedef void(* otHandleActiveScanResult ) ( otActiveScanResult *aResult, void *aContext)
This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.
typedef void(* otHandleEnergyScanResult ) ( otEnergyScanResult *aResult, void *aContext)
This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.
typedef void(* otLinkPcapCallback ) (const otRadioFrame *aFrame, bool aIsTx, void *aContext)
This function pointer is called when an IEEE 802.15.4 frame is received.

Enumerations

enum otMacFilterAddressMode {
OT_MAC_FILTER_ADDRESS_MODE_DISABLED ,
OT_MAC_FILTER_ADDRESS_MODE_WHITELIST ,
OT_MAC_FILTER_ADDRESS_MODE_BLACKLIST
}
Defines address mode of the mac filter.

Functions

otError otLinkActiveScan ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleActiveScanResult aCallback, void *aCallbackContext)
This function starts an IEEE 802.15.4 Active Scan.
bool otLinkIsActiveScanInProgress ( otInstance *aInstance)
This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.
otError otLinkEnergyScan ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleEnergyScanResult aCallback, void *aCallbackContext)
This function starts an IEEE 802.15.4 Energy Scan.
bool otLinkIsEnergyScanInProgress ( otInstance *aInstance)
This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.
otError otLinkSendDataRequest ( otInstance *aInstance)
This function enqueues an IEEE 802.15.4 Data Request message for transmission.
bool otLinkIsInTransmitState ( otInstance *aInstance)
This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.
otError otLinkOutOfBandTransmitRequest ( otInstance *aInstance, otRadioFrame *aOobFrame)
This function enqueues an IEEE 802.15.4 out of band Frame for transmission.
uint8_t otLinkGetChannel ( otInstance *aInstance)
Get the IEEE 802.15.4 channel.
otError otLinkSetChannel ( otInstance *aInstance, uint8_t aChannel)
Set the IEEE 802.15.4 channel.
uint32_t otLinkGetSupportedChannelMask ( otInstance *aInstance)
Get the supported channel mask of MAC layer.
otError otLinkSetSupportedChannelMask ( otInstance *aInstance, uint32_t aChannelMask)
Set the supported channel mask of MAC layer.
const otExtAddress * otLinkGetExtendedAddress ( otInstance *aInstance)
Get the IEEE 802.15.4 Extended Address.
otError otLinkSetExtendedAddress ( otInstance *aInstance, const otExtAddress *aExtAddress)
This function sets the IEEE 802.15.4 Extended Address.
void otLinkGetFactoryAssignedIeeeEui64 ( otInstance *aInstance, otExtAddress *aEui64)
Get the factory-assigned IEEE EUI-64.
otPanId otLinkGetPanId ( otInstance *aInstance)
Get the IEEE 802.15.4 PAN ID.
otError otLinkSetPanId ( otInstance *aInstance, otPanId aPanId)
Set the IEEE 802.15.4 PAN ID.
uint32_t otLinkGetPollPeriod ( otInstance *aInstance)
Get the data poll period of sleepy end device.
otError otLinkSetPollPeriod ( otInstance *aInstance, uint32_t aPollPeriod)
Set/clear user-specified/external data poll period for sleepy end device.
otShortAddress otLinkGetShortAddress ( otInstance *aInstance)
Get the IEEE 802.15.4 Short Address.
uint8_t otLinkGetMaxFrameRetriesDirect ( otInstance *aInstance)
This method returns the maximum number of frame retries during direct transmission.
void otLinkSetMaxFrameRetriesDirect ( otInstance *aInstance, uint8_t aMaxFrameRetriesDirect)
This method sets the maximum number of frame retries during direct transmission.
uint8_t otLinkGetMaxFrameRetriesIndirect ( otInstance *aInstance)
This method returns the maximum number of frame retries during indirect transmission.
void otLinkSetMaxFrameRetriesIndirect ( otInstance *aInstance, uint8_t aMaxFrameRetriesIndirect)
This method sets the maximum number of frame retries during indirect transmission.
otMacFilterAddressMode otLinkFilterGetAddressMode ( otInstance *aInstance)
This function gets the address mode of MAC filter.
otError otLinkFilterSetAddressMode ( otInstance *aInstance, otMacFilterAddressMode aMode)
This function sets the address mode of MAC filter.
otError otLinkFilterAddAddress ( otInstance *aInstance, const otExtAddress *aExtAddress)
This method adds an Extended Address to MAC filter.
otError otLinkFilterRemoveAddress ( otInstance *aInstance, const otExtAddress *aExtAddress)
This method removes an Extended Address from MAC filter.
void otLinkFilterClearAddresses ( otInstance *aInstance)
This method clears all the Extended Addresses from MAC filter.
otError otLinkFilterGetNextAddress ( otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry)
This method gets an in-use address filter entry.
otError otLinkFilterAddRssIn ( otInstance *aInstance, const otExtAddress *aExtAddress, int8_t aRss)
This method sets the received signal strength (in dBm) for the messages from the Extended Address.
otError otLinkFilterRemoveRssIn ( otInstance *aInstance, const otExtAddress *aExtAddress)
This method removes the received signal strength setting for the received messages from the Extended Address or removes the default received signal strength setting if no Extended Address is specified.
void otLinkFilterClearRssIn ( otInstance *aInstance)
This method clears all the received signal strength settings.
otError otLinkFilterGetNextRssIn ( otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry)
This method gets an in-use RssIn filter entry.
uint8_t otLinkConvertRssToLinkQuality ( otInstance *aInstance, int8_t aRss)
This method converts received signal strength to link quality.
int8_t otLinkConvertLinkQualityToRss ( otInstance *aInstance, uint8_t aLinkQuality)
This method converts link quality to typical received signal strength.
const uint32_t * otLinkGetTxDirectRetrySuccessHistogram ( otInstance *aInstance, uint8_t *aNumberOfEntries)
This method gets histogram of retries for a single direct packet until success.
const uint32_t * otLinkGetTxIndirectRetrySuccessHistogram ( otInstance *aInstance, uint8_t *aNumberOfEntries)
This method gets histogram of retries for a single indirect packet until success.
void otLinkResetTxRetrySuccessHistogram ( otInstance *aInstance)
This method clears histogram statistics for direct and indirect transmissions.
const otMacCounters * otLinkGetCounters ( otInstance *aInstance)
Get the MAC layer counters.
void otLinkResetCounters ( otInstance *aInstance)
Reset the MAC layer counters.
void otLinkSetPcapCallback ( otInstance *aInstance, otLinkPcapCallback aPcapCallback, void *aCallbackContext)
This function registers a callback to provide received raw IEEE 802.15.4 frames.
bool otLinkIsPromiscuous ( otInstance *aInstance)
This function indicates whether or not promiscuous mode is enabled at the link layer.
otError otLinkSetPromiscuous ( otInstance *aInstance, bool aPromiscuous)
This function enables or disables the link layer promiscuous mode.
uint16_t otLinkGetCcaFailureRate ( otInstance *aInstance)
This function returns the current CCA (Clear Channel Assessment) failure rate.
otError otLinkSetEnabled ( otInstance *aInstance, bool aEnable)
This function enables or disables the link layer.
bool otLinkIsEnabled ( otInstance *aInstance)
This function indicates whether or not the link layer is enabled.

Detailed Description

This module includes functions that control link-layer configuration.

Macro Definition Documentation

◆ OT_MAC_FILTER_FIXED_RSS_DISABLED

#define OT_MAC_FILTER_FIXED_RSS_DISABLED 127

Used to indicate no fixed received signal strength was set.

Typedef Documentation

◆ otHandleActiveScanResult

typedef void(* otHandleActiveScanResult) ( otActiveScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.

Parameters
[in] aResult A valid pointer to the beacon information or NULL when the active scan completes.
[in] aContext A pointer to application-specific context.

◆ otHandleEnergyScanResult

typedef void(* otHandleEnergyScanResult) ( otEnergyScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.

Parameters
[in] aResult A valid pointer to the energy scan result information or NULL when the energy scan completes.
[in] aContext A pointer to application-specific context.

◆ otLinkPcapCallback

typedef void(* otLinkPcapCallback) (const otRadioFrame *aFrame, bool aIsTx, void *aContext)

This function pointer is called when an IEEE 802.15.4 frame is received.

Note
This callback is called after FCS processing and aFrame may not contain the actual FCS that was received.
This callback is called before IEEE 802.15.4 security processing.
Parameters
[in] aFrame A pointer to the received IEEE 802.15.4 frame.
[in] aIsTx Whether this frame is transmitted, not received.
[in] aContext A pointer to application-specific context.

Enumeration Type Documentation

◆ otMacFilterAddressMode

Defines address mode of the mac filter.

Enumerator
OT_MAC_FILTER_ADDRESS_MODE_DISABLED

Address filter is disabled.

OT_MAC_FILTER_ADDRESS_MODE_WHITELIST

Whitelist address filter mode is enabled.

OT_MAC_FILTER_ADDRESS_MODE_BLACKLIST

Blacklist address filter mode is enabled.

Function Documentation

◆ otLinkActiveScan()

otError otLinkActiveScan ( otInstance * aInstance,
uint32_t aScanChannels,
uint16_t aScanDuration,
otHandleActiveScanResult aCallback,
void * aCallbackContext
)

This function starts an IEEE 802.15.4 Active Scan.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aScanChannels A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK).
[in] aScanDuration The time in milliseconds to spend scanning each channel.
[in] aCallback A pointer to a function called on receiving a beacon or scan completes.
[in] aCallbackContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Accepted the Active Scan request.
OT_ERROR_BUSY Already performing an Active Scan.

◆ otLinkConvertLinkQualityToRss()

int8_t otLinkConvertLinkQualityToRss ( otInstance * aInstance,
uint8_t aLinkQuality
)

This method converts link quality to typical received signal strength.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aLinkQuality LinkQuality value, should be in range [0,3].
Returns
Typical platform received signal strength mapping to aLinkQuality .

◆ otLinkConvertRssToLinkQuality()

uint8_t otLinkConvertRssToLinkQuality ( otInstance * aInstance,
int8_t aRss
)

This method converts received signal strength to link quality.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aRss The received signal strength value to be converted.
Returns
Link quality value mapping to aRss .

◆ otLinkEnergyScan()

otError otLinkEnergyScan ( otInstance * aInstance,
uint32_t aScanChannels,
uint16_t aScanDuration,
otHandleEnergyScanResult aCallback,
void * aCallbackContext
)

This function starts an IEEE 802.15.4 Energy Scan.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aScanChannels A bit vector indicating on which channels to perform energy scan.
[in] aScanDuration The time in milliseconds to spend scanning each channel.
[in] aCallback A pointer to a function called to pass on scan result on indicate scan completion.
[in] aCallbackContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Accepted the Energy Scan request.
OT_ERROR_BUSY Could not start the energy scan.

◆ otLinkFilterAddAddress()

otError otLinkFilterAddAddress ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This method adds an Extended Address to MAC filter.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A reference to the Extended Address.
Return values
OT_ERROR_NONE Successfully added aExtAddress to MAC filter.
OT_ERROR_ALREADY If aExtAddress was already in MAC filter.
OT_ERROR_INVALID_ARGS If aExtAddress is NULL.
OT_ERROR_NO_BUFS No available entry exists.
See also
otLinkFilterGetAddressMode
otLinkFilterSetAddressMode
otLinkFilterRemoveAddress
otLinkFilterClearAddresses
otLinkFilterGetNextAddress
otLinkFilterAddRssIn
otLinkFilterRemoveRssIn
otLinkFilterClearRssIn
otLinkFilterGetNextRssIn

◆ otLinkFilterAddRssIn()

otError otLinkFilterAddRssIn ( otInstance * aInstance,
const otExtAddress * aExtAddress,
int8_t aRss
)

This method sets the received signal strength (in dBm) for the messages from the Extended Address.

The default received signal strength for all received messages would be set if no Extended Address is specified.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the IEEE 802.15.4 Extended Address, or NULL to set the default received signal strength.
[in] aRss The received signal strength (in dBm) to set.
Return values
OT_ERROR_NONE Successfully set aRss for aExtAddress or set the default aRss for all received messages if aExtAddress is NULL.
OT_ERROR_NO_BUFS No available entry exists.
See also
otLinkFilterGetAddressMode
otLinkFilterSetAddressMode
otLinkFilterAddAddress
otLinkFilterRemoveAddress
otLinkFilterClearAddresses
otLinkFilterGetNextAddress
otLinkFilterRemoveRssIn
otLinkFilterClearRssIn
otLinkFilterGetNextRssIn

◆ otLinkFilterClearAddresses()

void otLinkFilterClearAddresses ( otInstance * aInstance )

◆ otLinkFilterClearRssIn()

void otLinkFilterClearRssIn ( otInstance * aInstance )

◆ otLinkFilterGetAddressMode()

otMacFilterAddressMode otLinkFilterGetAddressMode ( otInstance * aInstance )

◆ otLinkFilterGetNextAddress()

otError otLinkFilterGetNextAddress ( otInstance * aInstance,
otMacFilterIterator * aIterator,
otMacFilterEntry * aEntry
)

This method gets an in-use address filter entry.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the MAC filter iterator context. To get the first in-use address filter entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT.
[out] aEntry A pointer to where the information is placed.
Return values
OT_ERROR_NONE Successfully retrieved an in-use address filter entry.
OT_ERROR_INVALID_ARGS If aIterator or aEntry is NULL.
OT_ERROR_NOT_FOUND No subsequent entry exists.
See also
otLinkFilterGetAddressMode
otLinkFilterSetAddressMode
otLinkFilterAddAddress
otLinkFilterRemoveAddress
otLinkFilterClearAddresses
otLinkFilterAddRssIn
otLinkFilterRemoveRssIn
otLinkFilterClearRssIn
otLinkFilterGetNextRssIn

◆ otLinkFilterGetNextRssIn()

otError otLinkFilterGetNextRssIn ( otInstance * aInstance,
otMacFilterIterator * aIterator,
otMacFilterEntry * aEntry
)

This method gets an in-use RssIn filter entry.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A reference to the MAC filter iterator context. To get the first in-use RssIn Filter entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT.
[out] aEntry A reference to where the information is placed. The last entry would have the extended address as all 0xff to indicate the default received signal strength if it was set.
Return values
OT_ERROR_NONE Successfully retrieved an in-use RssIn Filter entry.
OT_ERROR_INVALID_ARGS If aIterator or aEntry is NULL.
OT_ERROR_NOT_FOUND No subsequent entry exists.
See also
otLinkFilterGetAddressMode
otLinkFilterSetAddressMode
otLinkFilterAddAddress
otLinkFilterRemoveAddress
otLinkFilterClearAddresses
otLinkFilterGetNextAddress
otLinkFilterAddRssIn
otLinkFilterRemoveRssIn
otLinkFilterClearRssIn

◆ otLinkFilterRemoveAddress()

otError otLinkFilterRemoveAddress ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This method removes an Extended Address from MAC filter.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A reference to the Extended Address.
Return values
OT_ERROR_NONE Successfully removed aExtAddress from MAC filter.
OT_ERROR_INVALID_ARGS If aExtAddress is NULL.
OT_ERROR_NOT_FOUND aExtAddress is not in MAC filter.
See also
otLinkFilterGetAddressMode
otLinkFilterSetAddressMode
otLinkFilterAddAddress
otLinkFilterClearAddresses
otLinkFilterGetNextAddress
otLinkFilterAddRssIn
otLinkFilterRemoveRssIn
otLinkFilterClearRssIn
otLinkFilterGetNextRssIn

◆ otLinkFilterRemoveRssIn()

otError otLinkFilterRemoveRssIn ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This method removes the received signal strength setting for the received messages from the Extended Address or removes the default received signal strength setting if no Extended Address is specified.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the IEEE 802.15.4 Extended Address, or NULL to reset the default received signal strength.
Return values
OT_ERROR_NONE Successfully removed received signal strength setting for aExtAddress or removed the default received signal strength setting if aExtAddress is NULL.
OT_ERROR_NOT_FOUND aExtAddress is not in MAC filter if it is not NULL.
See also
otLinkFilterGetAddressMode
otLinkFilterSetAddressMode
otLinkFilterAddAddress
otLinkFilterRemoveAddress
otLinkFilterClearAddresses
otLinkFilterGetNextAddress
otLinkFilterAddRssIn
otLinkFilterClearRssIn
otLinkFilterGetNextRssIn

◆ otLinkFilterSetAddressMode()

otError otLinkFilterSetAddressMode ( otInstance * aInstance,
otMacFilterAddressMode aMode
)

This function sets the address mode of MAC filter.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMode The address mode to set.
Return values
OT_ERROR_NONE Successfully set the address mode.
OT_ERROR_INVALID_ARGS aMode is not valid.
See also
otLinkFilterGetAddressMode
otLinkFilterAddAddress
otLinkFilterRemoveAddress
otLinkFilterClearAddresses
otLinkFilterGetNextAddress
otLinkFilterAddRssIn
otLinkFilterRemoveRssIn
otLinkFilterClearRssIn
otLinkFilterGetNextRssIn

◆ otLinkGetCcaFailureRate()

uint16_t otLinkGetCcaFailureRate ( otInstance * aInstance )

This function returns the current CCA (Clear Channel Assessment) failure rate.

The rate is maintained over a window of (roughly) last OPENTHREAD_CONFIG_CCA_FAILURE_RATE_AVERAGING_WINDOW frame transmissions.

Returns
The CCA failure rate with maximum value 0xffff corresponding to 100% failure rate.

◆ otLinkGetChannel()

uint8_t otLinkGetChannel ( otInstance * aInstance )

Get the IEEE 802.15.4 channel.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The IEEE 802.15.4 channel.
See also
otLinkSetChannel

◆ otLinkGetCounters()

const otMacCounters * otLinkGetCounters ( otInstance * aInstance )

Get the MAC layer counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the MAC layer counters.

◆ otLinkGetExtendedAddress()

const otExtAddress * otLinkGetExtendedAddress ( otInstance * aInstance )

Get the IEEE 802.15.4 Extended Address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the IEEE 802.15.4 Extended Address.

◆ otLinkGetFactoryAssignedIeeeEui64()

void otLinkGetFactoryAssignedIeeeEui64 ( otInstance * aInstance,
otExtAddress * aEui64
)

Get the factory-assigned IEEE EUI-64.

Parameters
[in] aInstance A pointer to the OpenThread instance.
[out] aEui64 A pointer to where the factory-assigned IEEE EUI-64 is placed.

◆ otLinkGetMaxFrameRetriesDirect()

uint8_t otLinkGetMaxFrameRetriesDirect ( otInstance * aInstance )

This method returns the maximum number of frame retries during direct transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The maximum number of retries during direct transmission.

◆ otLinkGetMaxFrameRetriesIndirect()

uint8_t otLinkGetMaxFrameRetriesIndirect ( otInstance * aInstance )

This method returns the maximum number of frame retries during indirect transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The maximum number of retries during indirect transmission.

◆ otLinkGetPanId()

otPanId otLinkGetPanId ( otInstance * aInstance )

Get the IEEE 802.15.4 PAN ID.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The IEEE 802.15.4 PAN ID.
See also
otLinkSetPanId

◆ otLinkGetPollPeriod()

uint32_t otLinkGetPollPeriod ( otInstance * aInstance )

Get the data poll period of sleepy end device.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The data poll period of sleepy end device in milliseconds.
See also
otLinkSetPollPeriod

◆ otLinkGetShortAddress()

otShortAddress otLinkGetShortAddress ( otInstance * aInstance )

Get the IEEE 802.15.4 Short Address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the IEEE 802.15.4 Short Address.

◆ otLinkGetSupportedChannelMask()

uint32_t otLinkGetSupportedChannelMask ( otInstance * aInstance )

Get the supported channel mask of MAC layer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The supported channel mask as uint32_t with bit 0 (lsb) mapping to channel 0, bit 1 to channel 1, so on.

◆ otLinkGetTxDirectRetrySuccessHistogram()

const uint32_t* otLinkGetTxDirectRetrySuccessHistogram ( otInstance * aInstance,
uint8_t * aNumberOfEntries
)

This method gets histogram of retries for a single direct packet until success.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aNumberOfEntries A pointer to where the size of returned histogram array is placed.
Returns
A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.

◆ otLinkGetTxIndirectRetrySuccessHistogram()

const uint32_t* otLinkGetTxIndirectRetrySuccessHistogram ( otInstance * aInstance,
uint8_t * aNumberOfEntries
)

This method gets histogram of retries for a single indirect packet until success.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aNumberOfEntries A pointer to where the size of returned histogram array is placed.
Returns
A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.

◆ otLinkIsActiveScanInProgress()

bool otLinkIsActiveScanInProgress ( otInstance * aInstance )

This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
true if an IEEE 802.15.4 Active Scan is in progress, false otherwise.

◆ otLinkIsEnabled()

bool otLinkIsEnabled ( otInstance * aInstance )

This function indicates whether or not the link layer is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
true Link layer is enabled.
false Link layer is not enabled.

◆ otLinkIsEnergyScanInProgress()

bool otLinkIsEnergyScanInProgress ( otInstance * aInstance )

This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
true if an IEEE 802.15.4 Energy Scan is in progress, false otherwise.

◆ otLinkIsInTransmitState()

bool otLinkIsInTransmitState ( otInstance * aInstance )

This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.

MAC module is in the transmit state during CSMA/CA procedure, CCA, Data, Beacon or Data Request frame transmission and receiving an ACK of a transmitted frame. MAC module is not in the transmit state during transmission of an ACK frame or a Beacon Request frame.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
true if an IEEE 802.15.4 MAC is in the transmit state, false otherwise.

◆ otLinkIsPromiscuous()

bool otLinkIsPromiscuous ( otInstance * aInstance )

This function indicates whether or not promiscuous mode is enabled at the link layer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
true Promiscuous mode is enabled.
false Promiscuous mode is not enabled.

◆ otLinkOutOfBandTransmitRequest()

otError otLinkOutOfBandTransmitRequest ( otInstance * aInstance,
otRadioFrame * aOobFrame
)

This function enqueues an IEEE 802.15.4 out of band Frame for transmission.

An Out of Band frame is one that was generated outside of OpenThread.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aOobFrame A pointer to the frame to transmit.
Return values
OT_ERROR_NONE Successfully scheduled the frame transmission.
OT_ERROR_ALREADY MAC layer is busy sending a previously requested frame.
OT_ERROR_INVALID_STATE The MAC layer is not enabled.
OT_ERROR_INVALID_ARGS The argument aOobFrame is NULL.

◆ otLinkResetCounters()

void otLinkResetCounters ( otInstance * aInstance )

Reset the MAC layer counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkResetTxRetrySuccessHistogram()

void otLinkResetTxRetrySuccessHistogram ( otInstance * aInstance )

This method clears histogram statistics for direct and indirect transmissions.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkSendDataRequest()

otError otLinkSendDataRequest ( otInstance * aInstance )

This function enqueues an IEEE 802.15.4 Data Request message for transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully enqueued an IEEE 802.15.4 Data Request message.
OT_ERROR_ALREADY An IEEE 802.15.4 Data Request message is already enqueued.
OT_ERROR_INVALID_STATE Device is not in rx-off-when-idle mode.
OT_ERROR_NO_BUFS Insufficient message buffers available.

◆ otLinkSetChannel()

otError otLinkSetChannel ( otInstance * aInstance,
uint8_t aChannel
)

Set the IEEE 802.15.4 channel.

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aChannel The IEEE 802.15.4 channel.
Return values
OT_ERROR_NONE Successfully set the channel.
OT_ERROR_INVALID_ARGS If aChannel is not in the range [11, 26] or is not in the supported channel mask.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otLinkGetChannel

◆ otLinkSetEnabled()

otError otLinkSetEnabled ( otInstance * aInstance,
bool aEnable
)

This function enables or disables the link layer.

Note
The link layer may only be enabled / disabled when the Thread Interface is disabled.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aEnable true to enable the link layer, or false otherwise.
Return values
OT_ERROR_NONE Successfully enabled / disabled the link layer.
OT_ERROR_INVALID_STATE Could not disable the link layer because the Thread interface is enabled.

◆ otLinkSetExtendedAddress()

otError otLinkSetExtendedAddress ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This function sets the IEEE 802.15.4 Extended Address.

This function succeeds only when Thread protocols are disabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the IEEE 802.15.4 Extended Address.
Return values
OT_ERROR_NONE Successfully set the IEEE 802.15.4 Extended Address.
OT_ERROR_INVALID_ARGS aExtAddress was NULL.
OT_ERROR_INVALID_STATE Thread protocols are enabled.

◆ otLinkSetMaxFrameRetriesDirect()

void otLinkSetMaxFrameRetriesDirect ( otInstance * aInstance,
uint8_t aMaxFrameRetriesDirect
)

This method sets the maximum number of frame retries during direct transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMaxFrameRetriesDirect The maximum number of retries during direct transmission.

◆ otLinkSetMaxFrameRetriesIndirect()

void otLinkSetMaxFrameRetriesIndirect ( otInstance * aInstance,
uint8_t aMaxFrameRetriesIndirect
)

This method sets the maximum number of frame retries during indirect transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMaxFrameRetriesIndirect The maximum number of retries during indirect transmission.

◆ otLinkSetPanId()

otError otLinkSetPanId ( otInstance * aInstance,
otPanId aPanId
)

Set the IEEE 802.15.4 PAN ID.

This function succeeds only when Thread protocols are disabled. A successful call to this function also invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPanId The IEEE 802.15.4 PAN ID.
Return values
OT_ERROR_NONE Successfully set the PAN ID.
OT_ERROR_INVALID_ARGS If aPanId is not in the range [0, 65534].
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otLinkGetPanId

◆ otLinkSetPcapCallback()

void otLinkSetPcapCallback ( otInstance * aInstance,
otLinkPcapCallback aPcapCallback,
void * aCallbackContext
)

This function registers a callback to provide received raw IEEE 802.15.4 frames.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPcapCallback A pointer to a function that is called when receiving an IEEE 802.15.4 link frame or NULL to disable the callback.
[in] aCallbackContext A pointer to application-specific context.

◆ otLinkSetPollPeriod()

otError otLinkSetPollPeriod ( otInstance * aInstance,
uint32_t aPollPeriod
)

Set/clear user-specified/external data poll period for sleepy end device.

Note
This function updates only poll period of sleepy end device. To update child timeout the function otThreadSetChildTimeout() shall be called.
Minimal non-zero value should be OPENTHREAD_CONFIG_MAC_MINIMUM_POLL_PERIOD (10ms). Or zero to clear user-specified poll period.
User-specified value should be no more than the maximal value 0x3FFFFFF ((1 << 26) - 1) allowed, otherwise it would be clipped by the maximal value.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPollPeriod data poll period in milliseconds.
Return values
OT_ERROR_NONE Successfully set/cleared user-specified poll period.
OT_ERROR_INVALID_ARGS If aPollPeriod is invalid.
See also
otLinkGetPollPeriod

◆ otLinkSetPromiscuous()

otError otLinkSetPromiscuous ( otInstance * aInstance,
bool aPromiscuous
)

This function enables or disables the link layer promiscuous mode.

Note
Promiscuous mode may only be enabled when the Thread interface is disabled.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPromiscuous true to enable promiscuous mode, or false otherwise.
Return values
OT_ERROR_NONE Successfully enabled promiscuous mode.
OT_ERROR_INVALID_STATE Could not enable promiscuous mode because the Thread interface is enabled.

◆ otLinkSetSupportedChannelMask()

otError otLinkSetSupportedChannelMask ( otInstance * aInstance,
uint32_t aChannelMask
)

Set the supported channel mask of MAC layer.

This function succeeds only when Thread protocols are disabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aChannelMask The supported channel mask (bit 0 or lsb mapping to channel 0, and so on).
Return values
OT_ERROR_NONE Successfully set the supported channel mask.
OT_ERROR_INVALID_STATE Thread protocols are enabled.