This structure represents the CoAP transmission parameters.
#include <
include/openthread/coap.h
>
Public Attributes |
|
| uint32_t | mAckTimeout |
|
Minimum spacing before first retransmission when ACK is not received, in milliseconds (RFC7252 default value is 2000ms).
|
|
| uint8_t | mAckRandomFactorNumerator |
|
Numerator of ACK_RANDOM_FACTOR used to calculate maximum spacing before first retransmission when ACK is not received (RFC7252 default value of ACK_RANDOM_FACTOR is 1.5; must not be decreased below 1).
|
|
| uint8_t | mAckRandomFactorDenominator |
|
Denominator of ACK_RANDOM_FACTOR used to calculate maximum spacing before first retransmission when ACK is not received (RFC7252 default value of ACK_RANDOM_FACTOR is 1.5; must not be decreased below 1).
|
|
| uint8_t | mMaxRetransmit |
|
Maximum number of retransmissions for CoAP Confirmable messages (RFC7252 default value is 4).
|
|
This structure represents the CoAP transmission parameters.
The documentation for this struct was generated from the following file:
-
include/openthread/
coap.h