This module includes functions that control the Thread stack's execution.
Functions | |
otError | otDiagProcessCmd (otInstance *aInstance, uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen) |
This function processes a factory diagnostics command line. | |
void | otDiagProcessCmdLine (otInstance *aInstance, const char *aString, char *aOutput, size_t aOutputMaxLen) |
This function processes a factory diagnostics command line. | |
bool | otDiagIsEnabled (otInstance *aInstance) |
This function indicates whether or not the factory diagnostics mode is enabled. |
Detailed Description
This module includes functions that control the Thread stack's execution.
Function Documentation
◆ otDiagIsEnabled()
bool otDiagIsEnabled | ( | otInstance * | aInstance | ) |
This function indicates whether or not the factory diagnostics mode is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
TRUE
if factory diagnostics mode is enabled FALSE
if factory diagnostics mode is disabled.
◆ otDiagProcessCmd()
otError otDiagProcessCmd | ( | otInstance * | aInstance, |
uint8_t | aArgsLength, |
||
char * | aArgs[], |
||
char * | aOutput, |
||
size_t | aOutputMaxLen |
||
) |
This function processes a factory diagnostics command line.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aArgsLength
The number of elements in aArgs
.[in] aArgs
An array of arguments. [out] aOutput
The diagnostics execution result. [in] aOutputMaxLen
The output buffer size.
- Return values
-
OT_ERROR_INVALID_ARGS
The command is supported but invalid arguments provided. OT_ERROR_NONE
The command is successfully process. OT_ERROR_NOT_IMPLEMENTED
The command is not supported.
◆ otDiagProcessCmdLine()
void otDiagProcessCmdLine | ( | otInstance * | aInstance, |
const char * | aString, |
||
char * | aOutput, |
||
size_t | aOutputMaxLen |
||
) |
This function processes a factory diagnostics command line.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aString
A NULL-terminated input string. [out] aOutput
The diagnostics execution result. [in] aOutputMaxLen
The output buffer size.