This structure represents a Service configuration.
#include <
include/openthread/netdata.h
>
Public Attributes | |
uint8_t | mServiceId |
Used to return Service ID when iterating over the partition's Network Data. | |
uint32_t | mEnterpriseNumber |
IANA Enterprise Number. | |
uint8_t | mServiceDataLength |
Length of service data. | |
uint8_t | mServiceData [OT_SERVICE_DATA_MAX_SIZE] |
Service data bytes. | |
otServerConfig | mServerConfig |
The Server configuration. |
This structure represents a Service configuration.
The documentation for this struct was generated from the following file:
- include/openthread/
netdata.h