otRadioIeInfo Struct Reference

This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame.

#include <include/openthread/platform/radio.h>

Public Attributes

int64_t mNetworkTimeOffset
 The time offset to the Thread network time.
 
uint8_t mTimeIeOffset
 The Time IE offset from the start of PSDU.
 
uint8_t mTimeSyncSeq
 The Time sync sequence.

This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame.


The documentation for this struct was generated from the following file:
  • include/openthread/platform/radio.h