This structure represents presence of different components in Active or Pending Operational Dataset.
#include <
include/openthread/dataset.h
>
Public Attributes | |
bool | mIsActiveTimestampPresent: 1 |
TRUE if Active Timestamp is present, FALSE otherwise. | |
bool | mIsPendingTimestampPresent: 1 |
TRUE if Pending Timestamp is present, FALSE otherwise. | |
bool | mIsMasterKeyPresent: 1 |
TRUE if Network Master Key is present, FALSE otherwise. | |
bool | mIsNetworkNamePresent: 1 |
TRUE if Network Name is present, FALSE otherwise. | |
bool | mIsExtendedPanIdPresent: 1 |
TRUE if Extended PAN ID is present, FALSE otherwise. | |
bool | mIsMeshLocalPrefixPresent: 1 |
TRUE if Mesh Local Prefix is present, FALSE otherwise. | |
bool | mIsDelayPresent: 1 |
TRUE if Delay Timer is present, FALSE otherwise. | |
bool | mIsPanIdPresent: 1 |
TRUE if PAN ID is present, FALSE otherwise. | |
bool | mIsChannelPresent: 1 |
TRUE if Channel is present, FALSE otherwise. | |
bool | mIsPskcPresent: 1 |
TRUE if PSKc is present, FALSE otherwise. | |
bool | mIsSecurityPolicyPresent: 1 |
TRUE if Security Policy is present, FALSE otherwise. | |
bool | mIsChannelMaskPresent: 1 |
TRUE if Channel Mask is present, FALSE otherwise. |
This structure represents presence of different components in Active or Pending Operational Dataset.
The documentation for this struct was generated from the following file:
- include/openthread/
dataset.h