This structure represents an External Route configuration.
#include <
include/openthread/netdata.h
>
Public Attributes | |
otIp6Prefix | mPrefix |
The prefix for the off-mesh route. | |
uint16_t | mRloc16 |
The Rloc associated with the external route entry. | |
signed int | mPreference: 2 |
A 2-bit signed integer indicating router preference as defined in RFC 4191. | |
bool | mStable: 1 |
TRUE, if this configuration is considered Stable Network Data. | |
bool | mNextHopIsThisDevice: 1 |
TRUE if the external route entry's next hop is this device itself (i.e., the route was added earlier by this device). |
This structure represents an External Route configuration.
Member Data Documentation
◆ mNextHopIsThisDevice
bool otExternalRouteConfig::mNextHopIsThisDevice |
TRUE if the external route entry's next hop is this device itself (i.e., the route was added earlier by this device).
FALSE otherwise.
This value is ignored when adding an external route. For any added route the next hop is this device.
◆ mRloc16
uint16_t otExternalRouteConfig::mRloc16 |
The Rloc associated with the external route entry.
This value is ignored when adding an external route. For any added route, the device's Rloc is used.
◆ mStable
bool otExternalRouteConfig::mStable |
TRUE, if this configuration is considered Stable Network Data.
FALSE, otherwise.
The documentation for this struct was generated from the following file:
- include/openthread/
netdata.h