Network#

The Network command set provides commands for interacting with the network. This includes building as well as sending ZigBee commands out on to the network.

Macros#

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_BROAD_PJOIN

network broad-pjoin [seconds:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_CHANNEL

network change-channel [channel:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_KEEP_ALIVE_MODE

network change-keep-alive-mode [keepAliveMode:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_EXTPANID

network extpanid [extPanId:-1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_JOINABLE

network find joinable

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_UNUSED

network find unused

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FORM

network form [channel:1] [power:1] [panId:2]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ID

network id

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_INIT

network init

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ISOPEN

network isopen

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_JOIN

network join [channel:1] [power:1] [panId:2]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_LEAVE

network leave

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_START

network multi-phy-start [page:1] [channel:1] [power:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_STOP

network multi-phy-stop

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_PJOIN

network pjoin [seconds:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN

network rejoin [haveCurrentNetworkKey:1] [channelMask:4]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN_DIFF_DEVICE_TYPE

network rejoin-diff-device-type [haveCurrentNetworkKey:1] [channelMask:4] [nodeType:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_SET

network set [networkIndex:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_TIMEOUT_OPTION_MASK

network timeout-option-mask [mask:2]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_DEFAULT

option apsretry default

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_OFF

option apsretry off

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_ON

option apsretry on

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_CLEAR

option binding-table clear

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_SET

option binding-table set [bindingTableIndex:1] [clusterId:2] [localEndpoint:1] [remoteEndpoint:1] [ieeeAddress:8]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_DISC

option disc [profileId:2] [clusterId:2]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_EDB

option edb [endpoint:1]