Plugin Commands: Slot Manager#

This plugin provides a set of CLI commands to interact with external SPI flash, particularly in a setup where slots are present to work with the common bootloader.

Macros#

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_BOOT_SLOT

plugin slot-manager boot-slot [slotId:4]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_ERASE_SLOT

plugin slot-manager erase-slot [slotId:4]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_EXT_FLASH_INFO

plugin slot-manager ext-flash-info

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_READ

plugin slot-manager read [address:4] [length:1]

#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_SLOTS_INFO

plugin slot-manager slots-info