Plugin Commands: Throughput#
The throughput commands allow you to test your application's network throughput
Macros#
plugin throughput clear-counters
plugin throughput print-counters
plugin throughput print-parameters
plugin throughput print-result
plugin throughput set-all [nodeId:2] [count:2] [interval:2] [packet:1] [inflight_count:1] [apsOptions:2] [timeout:4]
plugin throughput set-aps-ack-off
plugin throughput set-aps-ack-on
plugin throughput set-count [count:2]
plugin throughput set-destination [nodeId:2]
plugin throughput set-inflight [inflight_count:1]
plugin throughput set-interval [interval:2]
plugin throughput set-packet-size [packet:1]
plugin throughput set-timeout [timeout:4]
plugin throughput start
plugin throughput stop
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_CLEAR_COUNTERS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_CLEAR_COUNTERS
plugin throughput clear-counters
Clear all the stack counters
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_COUNTERS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_COUNTERS
plugin throughput print-counters
Print the stack counters
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_PARAMETERS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_PARAMETERS
plugin throughput print-parameters
Print all the test parameters
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_RESULT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_PRINT_RESULT
plugin throughput print-result
Show the results of the last test.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_ALL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_ALL
plugin throughput set-all [nodeId:2] [count:2] [interval:2] [packet:1] [inflight_count:1] [apsOptions:2] [timeout:4]
Set all parameters: Destination Count Interval packetLength maxInFlight testTimeout
nodeId - INT16U - Destination nodeId
count - INT16U - Packets to send
interval - INT16U - Interval in ms
packet - INT8U - Packet length in bytes
inflight_count - INT8U - Packets in flight
apsOptions - INT16U - APS Options
timeout - INT32U - Timeout in ms
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_OFF#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_OFF
plugin throughput set-aps-ack-off
Turn off APS acks
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_ON#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_APS_ACK_ON
plugin throughput set-aps-ack-on
Turn on APS acks
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_COUNT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_COUNT
plugin throughput set-count [count:2]
Set the number of packets to send
count - INT16U - Packets to send
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_DESTINATION#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_DESTINATION
plugin throughput set-destination [nodeId:2]
Set the destination nodeId
nodeId - INT16U - Destination nodeId
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INFLIGHT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INFLIGHT
plugin throughput set-inflight [inflight_count:1]
Set the number of packets in flight during the test.
inflight_count - INT8U - Packets in flight
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INTERVAL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_INTERVAL
plugin throughput set-interval [interval:2]
Set the interval
interval - INT16U - Interval in ms
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_PACKET_SIZE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_PACKET_SIZE
plugin throughput set-packet-size [packet:1]
Set the packet length
packet - INT8U - Packet length in bytes
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_TIMEOUT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_SET_TIMEOUT
plugin throughput set-timeout [timeout:4]
Set the test timeout
timeout - INT32U - Timeout in ms
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_START
plugin throughput start
Start the throughput test.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_PLUGIN_THROUGHPUT_STOP
plugin throughput stop
Abort the test while running.