Plugin Commands: Test Harness#

The test harness commands are used to test various unusual functionality or behavior of a remote device.

Macros#

#define

plugin test-harness add-child [ShortId:2] [EUI:-1] [nodeType:1]

#define
#define

plugin test-harness attr options [type:1] [timeout:2]

#define

plugin test-harness attr set-dest [addr:2] [endpoint:1]

#define

plugin test-harness attr start-test [clusterId:2] [attrStartId:2] [attrEndId:2] [clientToServer:1]

#define

plugin test-harness endpoint cluster-endpoint-index [endpoint:1] [clusterId:2] [mask:1]

#define
#define
#define

plugin test-harness key-establishment cert-mangle change-byte [byteIndex:1] [byteValue:1]

#define

plugin test-harness key-establishment cert-mangle corrupt [corruptionIndex:1]

#define

plugin test-harness key-establishment cert-mangle issuer [issuer:-1]

#define

plugin test-harness key-establishment cert-mangle length [lengthModifier:1]

#define

plugin test-harness key-establishment cert-mangle subject [subject:-1]

#define

plugin test-harness key-establishment delay-cbke [actualDelay:2] [advertisedDelay:2]

#define

plugin test-harness key-establishment key-mangle [lengthModifier:1]

#define

plugin test-harness key-establishment new-key-policy [allowKeyEstablishmentPolicy:1]

#define

plugin test-harness key-establishment out-of-sequence [commandId:1]

#define
#define
#define

plugin test-harness price send-new-fields [sendNewFields:1]

#define

plugin test-harness price send-se10-fields [sendNewFields:1]

#define
#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ADD_CHILD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ADD_CHILD

plugin test-harness add-child [ShortId:2] [EUI:-1] [nodeType:1]

  • Adds a child to the child table.

    • ShortId - INT16U - The shortId of the child device.

    • EUI - OCTET_STRING - The EUI64 of the child (big endian).

    • nodeType - INT8U - The node type of the child device.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_APS_SEC_FOR_CLUSTER_OFF#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_APS_SEC_FOR_CLUSTER_OFF

plugin test-harness aps-sec-for-cluster off

  • Turns off automatic APS security for the previously specified cluster.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_APS_SEC_FOR_CLUSTER_ON#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_APS_SEC_FOR_CLUSTER_ON

plugin test-harness aps-sec-for-cluster on [clusterId:2]

  • Turns on automatic APS security for the specified cluster.

    • clusterId - INT16U - The cluster ID to add APS security to automatically.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ATTR_OPTIONS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ATTR_OPTIONS

plugin test-harness attr options [type:1] [timeout:2]

  • Set the options for the attributes tests.

    • type - INT8U

    • timeout - INT16U


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ATTR_SET_DEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ATTR_SET_DEST

plugin test-harness attr set-dest [addr:2] [endpoint:1]

  • Set the destination for the attributes tests.

    • addr - INT16U

    • endpoint - INT8U


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ATTR_START_TEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ATTR_START_TEST

plugin test-harness attr start-test [clusterId:2] [attrStartId:2] [attrEndId:2] [clientToServer:1]

  • Start the attributes test.

    • clusterId - INT16U

    • attrStartId - INT16U

    • attrEndId - INT16U

    • clientToServer - BOOLEAN


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_CONCENTRATOR_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_CONCENTRATOR_START

plugin test-harness concentrator start

  • Starts the concentrator's periodic broadcasts.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_CONCENTRATOR_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_CONCENTRATOR_STOP

plugin test-harness concentrator stop

  • Starts the concentrator's periodic broadcasts.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_CLUSTER_ENDPOINT_INDEX#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_CLUSTER_ENDPOINT_INDEX

plugin test-harness endpoint cluster-endpoint-index [endpoint:1] [clusterId:2] [mask:1]

  • Get cluster endpoint index

    • endpoint - INT8U - The local endpoint of the cluster.

    • clusterId - INT16U - The cluster whose index is needed.

    • mask - INT8U - 0 for client-side attributes or 1 for server-side attributes.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_DISABLE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_DISABLE

plugin test-harness endpoint disable [endpoint:1]

  • Disables the endpont to receive messages and be discovered

    • endpoint - INT8U - The endpoint number.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_ENABLE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_ENABLE

plugin test-harness endpoint enable [endpoint:1]

  • Enables the endpont to receive messages and be discovered

    • endpoint - INT8U - The endpoint number.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_STATUS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_ENDPOINT_STATUS

plugin test-harness endpoint status

  • Disables the endpont to receive messages and be discovered


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_HASH_THE_FLASH#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_HASH_THE_FLASH

plugin test-harness hash-the-flash

  • Runs the AES-CCM algorithm over the contents of the software image to calcalute the image stamp.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_ADV_APS_FC#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_ADV_APS_FC

plugin test-harness key-establishment adv-aps-fc

  • Advances the local device's outgoing APS FC by 4096.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_CHANGE_BYTE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_CHANGE_BYTE

plugin test-harness key-establishment cert-mangle change-byte [byteIndex:1] [byteValue:1]

  • Changes a single byte in the cert

    • byteIndex - INT8U - The index of the certificate byte to change

    • byteValue - INT8U - The new value of the certificate byte


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_CORRUPT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_CORRUPT

plugin test-harness key-establishment cert-mangle corrupt [corruptionIndex:1]

  • Corrupts a single byte in the cert

    • corruptionIndex - INT8U - The index of the certificate byte to corrupt


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_ISSUER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_ISSUER

plugin test-harness key-establishment cert-mangle issuer [issuer:-1]

  • Changes the issuer in the certificate.

    • issuer - OCTET_STRING - The EUI64 of the issuer (big endian).


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_LENGTH#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_LENGTH

plugin test-harness key-establishment cert-mangle length [lengthModifier:1]

  • Mangles the length of the certificate

    • lengthModifier - INT8S - The positive or negative change in length.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_SUBJECT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_CERT_MANGLE_SUBJECT

plugin test-harness key-establishment cert-mangle subject [subject:-1]

  • Changes the subject (EUI64) of the cert

    • subject - OCTET_STRING - The EUI64 of the subject (big endian).


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_DEFAULT_RESP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_DEFAULT_RESP

plugin test-harness key-establishment default-resp

  • Sends a default response error message in response to initate KE.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_DELAY_CBKE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_DELAY_CBKE

plugin test-harness key-establishment delay-cbke [actualDelay:2] [advertisedDelay:2]

  • Changes the advertised delays by the local device for CBKE.

    • actualDelay - INT16U - Set the actual delay that occurs.

    • advertisedDelay - INT16U - Sets the advertised delay sent to the partner of key establishment


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_KEY_MANGLE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_KEY_MANGLE

plugin test-harness key-establishment key-mangle [lengthModifier:1]

  • Mangles the length of the empheral key.

    • lengthModifier - INT8S - The positive or negative change in length.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_NEW_KEY_POLICY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_NEW_KEY_POLICY

plugin test-harness key-establishment new-key-policy [allowKeyEstablishmentPolicy:1]

  • Sets the policy of whether the TC allows new KE requests.

    • allowKeyEstablishmentPolicy - INT8U - Allows / disallows new key establishment requests.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_NO_RESOURCES#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_NO_RESOURCES

plugin test-harness key-establishment no-resources

  • All received KE requests will be responded with 'no resources'.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_NORMAL_MODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_NORMAL_MODE

plugin test-harness key-establishment normal-mode

  • Sets the key establishment mode to normal.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_OUT_OF_SEQUENCE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_OUT_OF_SEQUENCE

plugin test-harness key-establishment out-of-sequence [commandId:1]

  • All received KE requests will be responded with 'no resources'.

    • commandId - INT8U - The out-of-sequence command ID to send.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_RESET_APS_FC#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_RESET_APS_FC

plugin test-harness key-establishment reset-aps-fc

  • Forces the local device to reset its outgoing APS FC.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_SET_AVAILABLE_SUITE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_SET_AVAILABLE_SUITE

plugin test-harness key-establishment set-available-suite [suite:2]

  • Selects between the CBKE 163k1 and 283k1 suites.

    • suite - INT16U - This field holds the type of key establishment suite. It can be EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1, EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1, or EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_SUITE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_SUITE

plugin test-harness key-establishment suite [suite:2]

  • Selects between the CBKE 163k1 and 283k1 suites.

    • suite - INT16U - This field holds the type of key establishment suite. It can be EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1, EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1, or EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_TIMEOUT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_ESTABLISHMENT_TIMEOUT

plugin test-harness key-establishment timeout

  • Artificially creates a timeout by delaying an outgoing message.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_UPDATE_BROADCAST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_UPDATE_BROADCAST

plugin test-harness key-update broadcast

  • Changes TC NWK key update mechanism to broadcast.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_UPDATE_NOW#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_UPDATE_NOW

plugin test-harness key-update now

  • Starts a TC NWK key update now


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_UPDATE_UNICAST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_KEY_UPDATE_UNICAST

plugin test-harness key-update unicast

  • Changes TC NWK key update mechanism to unicast with APS security.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_OTA_IMAGE_MANGLE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_OTA_IMAGE_MANGLE

plugin test-harness ota image-mangle [index:2]

  • Mangles the Simple Storage RAM OTA image.

    • index - INT16U - The byte index into the OTA image that will be mangled.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_PRICE_SEND_NEW_FIELDS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_PRICE_SEND_NEW_FIELDS

plugin test-harness price send-new-fields [sendNewFields:1]

  • Controls whether the new SE 1.1 price fields are included.

    • sendNewFields - INT8U - Boolean indicating whether to send new fields.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_PRICE_SEND_SE10_FIELDS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_PRICE_SEND_SE10_FIELDS

plugin test-harness price send-se10-fields [sendNewFields:1]

  • Controls whether the new SE 1.1 price fields are included.

    • sendNewFields - INT8U - Boolean indicating whether to send new fields.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_RADIO_OFF#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_RADIO_OFF

plugin test-harness radio off

  • Turns off the radio so that no messages are sent.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_RADIO_ON#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_RADIO_ON

plugin test-harness radio on

  • Turns on the radio if it was previously turned off


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_REGISTRATION_OFF#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_REGISTRATION_OFF

plugin test-harness registration off

  • Turns off automatic SE registration.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_REGISTRATION_ON#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_REGISTRATION_ON

plugin test-harness registration on

  • Turns on automatic SE registration.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_SET_COMPLIANCE_REVISION#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_SET_COMPLIANCE_REVISION

plugin test-harness set-compliance-revision [version:1]

  • Setting a compliance revision for a device such that the device can act as pre-R21 or R21+ for testing purposes. The reason for doing this is because the end device may send a node descriptor request and the hub will respond with the node descriptor response which will include the hub's compliance revision. If the compliance revision of the hub is R21+, only then will the TC link key request be made by the end device.

    • version - INT8U - The compliance version


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_SET_MAX_CHILDREN#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_SET_MAX_CHILDREN

plugin test-harness set-max-children [version:1]

  • Sets the maximum children supported by the local node.

    • version - INT8U - The maximum number of children to support


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_SET_RADIO_POWER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_SET_RADIO_POWER

plugin test-harness set-radio-power [power:1]

  • Sets the radio power.

    • power - INT8U - The radio power to set.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_STACK_LIMIT_BEACONS_OFF#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_STACK_LIMIT_BEACONS_OFF

plugin test-harness stack limit-beacons off

  • Disables a limit to the max number of outgoing beacons.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_STACK_LIMIT_BEACONS_ON#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_STACK_LIMIT_BEACONS_ON

plugin test-harness stack limit-beacons on

  • Enables a limit to the max number of outgoing beacons.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_STATUS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_STATUS

plugin test-harness status

  • Display the current status of the test harness.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_TC_KEEPALIVE_SEND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_TC_KEEPALIVE_SEND

plugin test-harness tc-keepalive send

  • Sends a Trust Center Keepalive.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_TC_KEEPALIVE_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_TC_KEEPALIVE_START

plugin test-harness tc-keepalive start

  • Starts the TC keepalive state machine.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_TC_KEEPALIVE_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TEST_HARNESS_PLUGIN_TEST_HARNESS_TC_KEEPALIVE_STOP

plugin test-harness tc-keepalive stop

  • Stops the TC keepalive state machine.