ACMP_Init_TypeDef Struct Reference

ACMP initialization structure.

#include <em_acmp.h>

Data Fields

bool fullBias
Full-bias current.
uint32_t biasProg
Bias current.
bool interruptOnFallingEdge
Enable setting the interrupt flag on the falling edge.
bool interruptOnRisingEdge
Enable setting the interrupt flag on the rising edge.
ACMP_InputRange_TypeDef inputRange
Input range.
ACMP_Accuracy_TypeDef accuracy
ACMP accuracy mode.
ACMP_PowerSource_TypeDef powerSource
Select the power source for the ACMP.
ACMP_HysteresisLevel_TypeDef hysteresisLevel_0
Hysteresis when ACMP output is 0.
ACMP_HysteresisLevel_TypeDef hysteresisLevel_1
Hysteresis when ACMP output is 1.
ACMP_VLPInput_Typedef vlpInput
VLP Input source.
bool