CMU_HFXOInit_TypeDef Struct Reference
HFXO initialization structure.
#include <em_cmu.h>
Data Fields |
|
bool | lowPowerMode |
Enable low-power mode.
|
|
bool | autoStartEm01 |
bool | autoSelEm01 |
bool | autoStartSelOnRacWakeup |
uint16_t | ctuneStartup |
Startup phase CTUNE (load capacitance) value.
|
|
uint16_t | ctuneSteadyState |
Steady-state phase CTUNE (load capacitance) value.
|
|
uint8_t | regIshSteadyState |
Shunt steady-state current.
|
|
uint8_t | xoCoreBiasTrimStartup |
Startup XO core bias current trim.
|
|
uint8_t | xoCoreBiasTrimSteadyState |
Steady-state XO core bias current trim.
|
|
uint8_t | thresholdPeakDetect |
Peak detection threshold.
|
|
uint8_t | timeoutShuntOptimization |
Timeout - shunt optimization.
|
|
uint8_t | timeoutPeakDetect |
Timeout - peak detection.
|
|
uint8_t |