PCNT_Init_TypeDef Struct Reference

Initialization structure.

#include <em_pcnt.h>

Data Fields

PCNT_Mode_TypeDef mode
Mode to operate in.
uint32_t counter
Initial counter value (refer to reference manual for max value allowed).
uint32_t top
Initial top value (refer to reference manual for max value allowed).
bool negEdge
Polarity of incoming edge.
bool countDown
Counting direction, only applicable for pcntModeOvsSingle and pcntModeExtSingle modes.
bool filter
Enable filter, only available in pcntModeOvsSingle * mode.
bool hyst
Set to true to enable hysteresis.
bool s1CntDir
Set to true to enable S1 to determine the direction of counting in OVSSINGLE or EXTCLKSINGLE modes.
PCNT_CntEvent_TypeDef cntEvent
Selects whether the regular counter responds to up-count events, down-count events, both, or none.
PCNT_CntEvent_TypeDef auxCntEvent