ACMP_VAConfig_TypeDef Struct Reference

VA Configuration structure.

#include <em_acmp.h>

Data Fields

ACMP_VAInput_TypeDef input
VA voltage input source.
uint32_t div0
A divider for VA voltage input source when ACMP output is 0.
uint32_t div1
A divider for VA voltage input source when ACMP output is 1.

VA Configuration structure.

This structure is used to configure the VA voltage input source and its dividers.

Field Documentation

input

ACMP_VAInput_TypeDef ACMP_VAConfig_TypeDef::input

VA voltage input source.

div0

uint32_t ACMP_VAConfig_TypeDef::div0

A divider for VA voltage input source when ACMP output is 0.

This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.

VA divided = VA input * (div0 + 1) / 64

div1

uint32_t ACMP_VAConfig_TypeDef::div1

A divider for VA voltage input source when ACMP output is 1.

This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.

VA divided = VA input * (div1 + 1) / 64