TIMER_InitDTI_TypeDef Struct Reference
TIMER Dead Time Insertion (DTI) initialization structure.
#include <em_timer.h>
Data Fields |
|
bool | enable |
Enable DTI or leave it disabled until
TIMER_EnableDTI()
is called.
|
|
bool | activeLowOut |
DTI Output Polarity.
|
|
bool | invertComplementaryOut |
DTI Complementary Output Invert.
|
|
bool | autoRestart |
Enable Automatic Start-up functionality (when debugger exits).
|
|
bool | enablePrsSource |
Enable/disable PRS as DTI input.
|
|
TIMER_PRSSEL_TypeDef | prsSel |
Select which PRS channel as DTI input.
|
|
TIMER_Prescale_TypeDef | prescale |
DTI prescaling factor, if HFPER / HFPERB clock used.
|
|
unsigned int | riseTime |
DTI Rise Time.
|
|
unsigned int | fallTime |
DTI Fall Time.
|
|
uint32_t | outputsEnableMask |
DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2.
|
|
bool | enableFaultSourceCoreLockup |