CRYOTIMER_Init_TypeDef Struct Reference

CRYOTIMER initialization structure.

#include <em_cryotimer.h>

Data Fields

bool enable
Enable/disable counting when initialization is complete.
bool debugRun
Enable/disable timer counting during debug halt.
bool em4Wakeup
Enable/disable EM4 Wakeup.
CRYOTIMER_Osc_TypeDef osc
Select the oscillator for the CRYOTIMER.
CRYOTIMER_Presc_TypeDef presc
Prescaler.
CRYOTIMER_Period_TypeDef period
A period between a wakeup event/interrupt.

CRYOTIMER initialization structure.

Field Documentation

enable

bool CRYOTIMER_Init_TypeDef::enable

Enable/disable counting when initialization is complete.

debugRun

bool CRYOTIMER_Init_TypeDef::debugRun

Enable/disable timer counting during debug halt.

em4Wakeup

bool CRYOTIMER_Init_TypeDef::em4Wakeup

Enable/disable EM4 Wakeup.

osc

CRYOTIMER_Osc_TypeDef CRYOTIMER_Init_TypeDef::osc

Select the oscillator for the CRYOTIMER.

presc