LDMA_Descriptor_t Union Reference

DMA descriptor.

#include <em_ldma.h>

Data Fields

struct {
uint32_t structType : 2
Set to 0 to select XFER descriptor type.
uint32_t reserved0 : 1
Reserved

uint32_t structReq : 1
DMA transfer trigger during LINKLOAD.
uint32_t xferCnt : 11
Transfer count minus one.
uint32_t byteSwap : 1
Enable byte swapping transfers.
uint32_t blockSize : 4
Number of unit transfers per arbitration cycle.
uint32_t doneIfs : 1
Generate interrupt when done.
uint32_t reqMode : 1
Block or cycle transfer selector.
uint32_t decLoopCnt : 1
Enable looped transfers.
uint32_t ignoreSrec : 1
Ignore single requests.
uint32_t srcInc : 2
Source address increment unit size.
uint32_t size : 2
DMA transfer unit size.
uint32_t dstInc : 2
Destination address increment unit size.
uint32_t