RTCC_Init_TypeDef Struct Reference

RTCC initialization structure.

#include <em_rtcc.h>

Data Fields

bool enable
Enable/disable counting when initialization is completed.
bool debugRun
Enable/disable timer counting during debug halt.
bool precntWrapOnCCV0
Enable/disable pre-counter wrap on ch.
bool cntWrapOnCCV1
Enable/disable counter wrap on ch.
RTCC_CntPresc_TypeDef presc
Counter prescaler.
RTCC_PrescMode_TypeDef prescMode
Prescaler mode.
bool enaOSCFailDetect
Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.
RTCC_CntMode_TypeDef cntMode
Select operational mode of the counter.
bool disLeapYearCorr
Disable leap year correction for calendar mode.

RTCC initialization structure.

Field Documentation

◆ enable

bool RTCC_Init_TypeDef::enable

Enable/disable counting when initialization is completed.

◆ debugRun

bool RTCC_Init_TypeDef::debugRun

Enable/disable timer counting during debug halt.

◆ precntWrapOnCCV0

bool RTCC_Init_TypeDef::precntWrapOnCCV0

Enable/disable pre-counter wrap on ch.

0 CCV value.

◆ cntWrapOnCCV1

bool RTCC_Init_TypeDef::cntWrapOnCCV1

Enable/disable counter wrap on ch.

1 CCV value.

◆ presc

RTCC_CntPresc_TypeDef RTCC_Init_TypeDef::presc

Counter prescaler.

◆ prescMode

RTCC_PrescMode_TypeDef RTCC_Init_TypeDef::prescMode

Prescaler mode.

◆ enaOSCFailDetect

bool RTCC_Init_TypeDef::enaOSCFailDetect

Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.

◆ cntMode

RTCC_CntMode_TypeDef RTCC_Init_TypeDef::cntMode

Select operational mode of the counter.

◆ disLeapYearCorr

bool RTCC_Init_TypeDef::disLeapYearCorr

Disable leap year correction for calendar mode.

When this parameter is set to false, February has 29 days if (year % 4 == 0). If set to true, February always has 28 days.