LESENSEEMLIB
Detailed Description
Low Energy Sensor (LESENSE) Peripheral API.
This module contains functions to control the LESENSE peripheral of Silicon Labs 32-bit MCUs and SoCs. LESENSE is a low energy sensor interface capable of autonomously collecting and processing data from multiple sensors even when in EM2.
Data Structures |
|
struct | LESENSE_AltExDesc_TypeDef |
struct | LESENSE_ChAll_TypeDef |
struct | LESENSE_ChDesc_TypeDef |
struct | LESENSE_ConfAltEx_TypeDef |
struct | LESENSE_CoreCtrlDesc_TypeDef |
struct | LESENSE_DecCtrlDesc_TypeDef |
struct | LESENSE_DecStAll_TypeDef |
struct | LESENSE_DecStCond_TypeDef |
struct | LESENSE_DecStDesc_TypeDef |
struct | LESENSE_Init_TypeDef |
struct | LESENSE_PerCtrlDesc_TypeDef |
struct | LESENSE_TimeCtrlDesc_TypeDef |
Macros |
|
#define | LESENSE_ALTEX_CH_CONF_DEFAULT |
#define | LESENSE_ALTEX_CONF_DEFAULT |
#define | LESENSE_CH_CONF_DEFAULT |
#define | LESENSE_CORECTRL_DESC_DEFAULT |
#define | LESENSE_DECCTRL_DESC_DEFAULT |
#define | LESENSE_DECODER_CONF_DEFAULT |
#define | LESENSE_INIT_DEFAULT |
#define | LESENSE_NUM_CHANNELS 16 |
#define | LESENSE_NUM_DECODER_STATES ( _LESENSE_DECSTATE_DECSTATE_MASK + 1) |
#define | LESENSE_PERCTRL_DESC_DEFAULT |
#define | LESENSE_SCAN_CONF_DEFAULT |
#define | LESENSE_ST_CONF_DEFAULT |
#define | LESENSE_TIMECTRL_DESC_DEFAULT |
Enumerations |
|
enum |
LESENSE_AltExMap_TypeDef
{
lesenseAltExMapALTEX = _LESENSE_CTRL_ALTEXMAP_ALTEX, lesenseAltExMapACMP = _LESENSE_CTRL_ALTEXMAP_ACMP } |
enum |
LESENSE_AltExPinIdle_TypeDef
{
lesenseAltExPinIdleDis = _LESENSE_ALTEXCONF_IDLECONF0_DISABLE, lesenseAltExPinIdleHigh = _LESENSE_ALTEXCONF_IDLECONF0_HIGH, lesenseAltExPinIdleLow = _LESENSE_ALTEXCONF_IDLECONF0_LOW } |
enum |
LESENSE_BiasMode_TypeDef
{
lesenseBiasModeDutyCycle = LESENSE_BIASCTRL_BIASMODE_DUTYCYCLE, lesenseBiasModeHighAcc = LESENSE_BIASCTRL_BIASMODE_HIGHACC, lesenseBiasModeDontTouch = LESENSE_BIASCTRL_BIASMODE_DONTTOUCH } |
enum |
LESENSE_BufTrigLevel_TypeDef
{
lesenseBufTrigHalf = LESENSE_CTRL_BUFIDL_HALFFULL, lesenseBufTrigFull = LESENSE_CTRL_BUFIDL_FULL } |
enum |
LESENSE_ChClk_TypeDef
{
lesenseClkLF = _LESENSE_CH_INTERACT_EXCLK_LFACLK, lesenseClkHF = _LESENSE_CH_INTERACT_EXCLK_AUXHFRCO } |
enum |
LESENSE_ChCompMode_TypeDef
{
lesenseCompModeLess = LESENSE_CH_EVAL_COMP_LESS, lesenseCompModeGreaterOrEq = LESENSE_CH_EVAL_COMP_GE } |
enum |
LESENSE_ChIntMode_TypeDef
{
lesenseSetIntNone = LESENSE_CH_INTERACT_SETIF_NONE, lesenseSetIntLevel = LESENSE_CH_INTERACT_SETIF_LEVEL, lesenseSetIntPosEdge = LESENSE_CH_INTERACT_SETIF_POSEDGE, lesenseSetIntNegEdge = LESENSE_CH_INTERACT_SETIF_NEGEDGE } |
enum |
LESENSE_ChPinExMode_TypeDef
{
lesenseChPinExDis = LESENSE_CH_INTERACT_EXMODE_DISABLE, lesenseChPinExHigh = LESENSE_CH_INTERACT_EXMODE_HIGH, lesenseChPinExLow = LESENSE_CH_INTERACT_EXMODE_LOW, lesenseChPinExDACOut = LESENSE_CH_INTERACT_EXMODE_DACOUT } |
enum |
LESENSE_ChPinIdleMode_TypeDef
{
lesenseChPinIdleDis = _LESENSE_IDLECONF_CH0_DISABLE, lesenseChPinIdleHigh = _LESENSE_IDLECONF_CH0_HIGH, lesenseChPinIdleLow = _LESENSE_IDLECONF_CH0_LOW, lesenseChPinIdleDACCh0 = _LESENSE_IDLECONF_CH0_DACCH0, lesenseChPinIdleDACCh1 = _LESENSE_IDLECONF_CH12_DACCH1 } |
enum |
LESENSE_ChSampleMode_TypeDef
{
lesenseSampleModeCounter = 0x0 << _LESENSE_CH_INTERACT_SAMPLE_SHIFT, lesenseSampleModeACMP = LESENSE_CH_INTERACT_SAMPLE_ACMP } |
enum |
LESENSE_ClkPresc_TypeDef
{
lesenseClkDiv_1 = 0, lesenseClkDiv_2 = 1, lesenseClkDiv_4 = 2, lesenseClkDiv_8 = 3, lesenseClkDiv_16 = 4, lesenseClkDiv_32 = 5, lesenseClkDiv_64 = 6, lesenseClkDiv_128 = 7 } |
enum |
LESENSE_ControlACMP_TypeDef
{
lesenseACMPModeDisable = _LESENSE_PERCTRL_ACMP0MODE_DISABLE, lesenseACMPModeMux = _LESENSE_PERCTRL_ACMP0MODE_MUX, lesenseACMPModeMuxThres = _LESENSE_PERCTRL_ACMP0MODE_MUXTHRES } |
enum |
LESENSE_ControlDACConv_TypeDef
{
lesenseDACConvModeDisable = _LESENSE_PERCTRL_DACCH0CONV_DISABLE, lesenseDACConvModeContinuous = _LESENSE_PERCTRL_DACCH0CONV_CONTINUOUS, lesenseDACConvModeSampleHold = _LESENSE_PERCTRL_DACCH0CONV_SAMPLEHOLD, lesenseDACConvModeSampleOff = _LESENSE_PERCTRL_DACCH0CONV_SAMPLEOFF } |
enum |
LESENSE_ControlDACData_TypeDef
{
lesenseDACIfData = _LESENSE_PERCTRL_DACCH0DATA_DACDATA, lesenseACMPThres = _LESENSE_PERCTRL_DACCH0DATA_ACMPTHRES } |
enum |
LESENSE_ControlDACOut_TypeDef
{
lesenseDACOutModeDisable = _LESENSE_PERCTRL_DACCH0OUT_DISABLE, lesenseDACOutModePin = _LESENSE_PERCTRL_DACCH0OUT_PIN, lesenseDACOutModeADCACMP = _LESENSE_PERCTRL_DACCH0OUT_ADCACMP, lesenseDACOutModePinADCACMP = _LESENSE_PERCTRL_DACCH0OUT_PINADCACMP } |
enum |
LESENSE_DACRef_TypeDef
{
lesenseDACRefVdd = LESENSE_PERCTRL_DACREF_VDD, lesenseDACRefBandGap = LESENSE_PERCTRL_DACREF_BANDGAP } |
enum |
LESENSE_DecInput_TypeDef
{
lesenseDecInputSensorSt = LESENSE_DECCTRL_INPUT_SENSORSTATE, lesenseDecInputPRS = LESENSE_DECCTRL_INPUT_PRS } |
enum |
LESENSE_DMAWakeUp_TypeDef
{
lesenseDMAWakeUpDisable = LESENSE_CTRL_DMAWU_DISABLE, lesenseDMAWakeUpBufValid = LESENSE_CTRL_DMAWU_BUFDATAV, lesenseDMAWakeUpBufLevel = LESENSE_CTRL_DMAWU_BUFLEVEL } |
enum |
LESENSE_PRSSel_TypeDef
{
lesensePRSCh0 = 0, lesensePRSCh1 = 1, lesensePRSCh2 = 2, lesensePRSCh3 = 3, lesensePRSCh4 = 4, lesensePRSCh5 = 5, lesensePRSCh6 = 6, lesensePRSCh7 = 7, lesensePRSCh8 = 8, lesensePRSCh9 = 9, lesensePRSCh10 = 10, lesensePRSCh11 = 11 } |
enum |
LESENSE_ScanConfSel_TypeDef
{
lesenseScanConfDirMap = LESENSE_CTRL_SCANCONF_DIRMAP, lesenseScanConfInvMap = LESENSE_CTRL_SCANCONF_INVMAP, lesenseScanConfToggle = LESENSE_CTRL_SCANCONF_TOGGLE, lesenseScanConfDecDef = LESENSE_CTRL_SCANCONF_DECDEF } |
enum |
LESENSE_ScanMode_TypeDef
{
lesenseScanStartPeriodic = LESENSE_CTRL_SCANMODE_PERIODIC, lesenseScanStartOneShot = LESENSE_CTRL_SCANMODE_ONESHOT, lesenseScanStartPRS = LESENSE_CTRL_SCANMODE_PRS } |
enum |
LESENSE_StTransAct_TypeDef
{
lesenseTransActNone = LESENSE_ST_TCONFA_PRSACT_NONE, lesenseTransActPRS0 = LESENSE_ST_TCONFA_PRSACT_PRS0, lesenseTransActPRS1 = LESENSE_ST_TCONFA_PRSACT_PRS1, lesenseTransActPRS01 = LESENSE_ST_TCONFA_PRSACT_PRS01, lesenseTransActPRS2 = LESENSE_ST_TCONFA_PRSACT_PRS2, lesenseTransActPRS02 = LESENSE_ST_TCONFA_PRSACT_PRS02, lesenseTransActPRS12 = LESENSE_ST_TCONFA_PRSACT_PRS12, lesenseTransActPRS012 = LESENSE_ST_TCONFA_PRSACT_PRS012, lesenseTransActUp = LESENSE_ST_TCONFA_PRSACT_UP, lesenseTransActDown = LESENSE_ST_TCONFA_PRSACT_DOWN, lesenseTransActUpAndPRS2 = LESENSE_ST_TCONFA_PRSACT_UPANDPRS2, lesenseTransActDownAndPRS2 = LESENSE_ST_TCONFA_PRSACT_DOWNANDPRS2 } |
enum |
LESENSE_WarmupMode_TypeDef
{
lesenseWarmupModeNormal = LESENSE_PERCTRL_WARMUPMODE_NORMAL, lesenseWarmupModeACMP = LESENSE_PERCTRL_WARMUPMODE_KEEPACMPWARM, lesenseWarmupModeDAC = LESENSE_PERCTRL_WARMUPMODE_KEEPDACWARM, lesenseWarmupModeKeepWarm = LESENSE_PERCTRL_WARMUPMODE_KEEPACMPDACWARM } |
Functions |
|
void | LESENSE_AltExConfig (const LESENSE_ConfAltEx_TypeDef *confAltEx) |
Configure the LESENSE alternate excitation modes.
|
|
__STATIC_INLINE uint32_t | LESENSE_ChannelActiveGet (void) |
Get the currently active channel index.
|
|
void | LESENSE_ChannelAllConfig (const LESENSE_ChAll_TypeDef *confChAll) |
Configure all (16) LESENSE sensor channels.
|
|
void | LESENSE_ChannelConfig (const LESENSE_ChDesc_TypeDef *confCh, uint32_t chIdx) |
Configure a single LESENSE sensor channel.
|
|
void | LESENSE_ChannelEnable (uint8_t chIdx, bool enaScanCh, bool enaPin) |
Enable/disable LESENSE scan channel and the pin assigned to it.
|
|
void | LESENSE_ChannelEnableMask (uint16_t chMask, uint16_t pinMask) |
Enable/disable LESENSE scan channel and the pin assigned to it.
|
|
void | LESENSE_ChannelThresSet (uint8_t chIdx, uint16_t acmpThres, uint16_t cntThres) |
Set LESENSE channel threshold parameters.
|
|
void | LESENSE_ChannelTimingSet (uint8_t chIdx, uint8_t exTime, uint8_t sampleDelay, uint16_t measDelay) |
Set LESENSE channel timing parameters.
|
|
void | LESENSE_ClkDivSet ( LESENSE_ChClk_TypeDef clk, LESENSE_ClkPresc_TypeDef clkDiv) |
Set clock division for LESENSE timers.
|
|
void | LESENSE_DecoderStart (void) |
Start LESENSE decoder.
|
|
void | LESENSE_DecoderStateAllConfig (const LESENSE_DecStAll_TypeDef *confDecStAll) |
Configure all LESENSE decoder states.
|
|
void | LESENSE_DecoderStateConfig (const LESENSE_DecStDesc_TypeDef *confDecSt, uint32_t decSt) |
Configure a single LESENSE decoder state.
|
|
uint32_t | LESENSE_DecoderStateGet (void) |
Get the current state of the LESENSE decoder.
|
|
void | LESENSE_DecoderStateSet (uint32_t decSt) |
Set LESENSE decoder state.
|
|
__STATIC_INLINE void | LESENSE_DecoderStop (void) |
Stop LESENSE decoder.
|
|
void | LESENSE_Init (const LESENSE_Init_TypeDef *init, bool reqReset) |
Initialize the LESENSE module.
|
|
__STATIC_INLINE void | LESENSE_IntClear (uint32_t flags) |
Clear one or more pending LESENSE interrupts.
|
|
__STATIC_INLINE void | LESENSE_IntDisable (uint32_t flags) |
Disable one or more LESENSE interrupts.
|
|
__STATIC_INLINE void | LESENSE_IntEnable (uint32_t flags) |
Enable one or more LESENSE interrupts.
|
|
__STATIC_INLINE uint32_t | LESENSE_IntGet (void) |
Get pending LESENSE interrupt flags.
|
|
__STATIC_INLINE uint32_t | LESENSE_IntGetEnabled (void) |
Get enabled and pending LESENSE interrupt flags.
|
|
__STATIC_INLINE void | LESENSE_IntSet (uint32_t flags) |
Set one or more pending LESENSE interrupts from SW.
|
|
__STATIC_INLINE void | LESENSE_RAMPowerDown (void) |
Shut off power to the LESENSE RAM, disables LESENSE.
|
|
void | LESENSE_Reset (void) |
Reset the LESENSE module.
|
|
void | LESENSE_ResultBufferClear (void) |
Clear result buffer.
|
|
uint32_t | LESENSE_ScanFreqSet (uint32_t refFreq, uint32_t scanFreq) |
Set scan frequency for periodic scanning.
|
|
void | LESENSE_ScanModeSet ( LESENSE_ScanMode_TypeDef scanMode, bool start) |
Set scan mode of the LESENSE channels.
|
|
__STATIC_INLINE uint32_t | LESENSE_ScanResultDataBufferGet (uint32_t idx) |
Get data from the result data buffer.
|
|
__STATIC_INLINE uint32_t | LESENSE_ScanResultDataGet (void) |
Get the oldest unread data from the result buffer.
|
|
__STATIC_INLINE uint32_t | LESENSE_ScanResultGet (void) |
Get the latest scan comparison result (1 bit / channel).
|
|
void | LESENSE_ScanStart (void) |
Start scanning of sensors.
|
|
void | LESENSE_ScanStop (void) |
Stop scanning of sensors.
|
|
__STATIC_INLINE uint32_t | LESENSE_SensorStateGet (void) |
Get the current state of the LESENSE sensor.
|
|
void | LESENSE_StartDelaySet (uint8_t startDelay) |
Set start delay of sensor interaction on each channel.
|
|
__STATIC_INLINE uint32_t | LESENSE_StatusGet (void) |
Get the current status of LESENSE.
|
|
__STATIC_INLINE void | LESENSE_StatusWait (uint32_t flag) |
Wait until the status of LESENSE is equal to what requested.
|
|
Macro Definition Documentation
#define LESENSE_ALTEX_CH_CONF_DEFAULT |
Default configuration for alternate excitation channel.
Definition at line
965
of file
em_lesense.h
.
#define LESENSE_ALTEX_CONF_DEFAULT |
Default configuration for all alternate excitation channels.
Definition at line
974
of file
em_lesense.h
.
#define LESENSE_CH_CONF_DEFAULT |
Default configuration for scan channel.
Definition at line
877
of file
em_lesense.h
.
#define LESENSE_CORECTRL_DESC_DEFAULT |
Default configuration for LESENSE_CtrlDesc_TypeDef structure.
Definition at line
531
of file
em_lesense.h
.
#define LESENSE_DECCTRL_DESC_DEFAULT |
Default configuration for LESENSE_PerCtrl_TypeDef structure.
Definition at line
720
of file
em_lesense.h
.
#define LESENSE_DECODER_CONF_DEFAULT |
Default configuration for all decoder states.
Definition at line
1077
of file
em_lesense.h
.
#define LESENSE_INIT_DEFAULT |
Default configuration for LESENSE_Init_TypeDef structure.
Definition at line
753
of file
em_lesense.h
.
#define LESENSE_NUM_CHANNELSÂ Â Â 16 |
Number of LESENSE channels.
Definition at line
60
of file
em_lesense.h
.
Referenced by LESENSE_ChannelAllConfig() , LESENSE_ChannelConfig() , LESENSE_ChannelThresSet() , and LESENSE_Reset() .
#define LESENSE_NUM_DECODER_STATESÂ Â Â ( _LESENSE_DECSTATE_DECSTATE_MASK + 1) |
Number of decoder states supported by current device.
Definition at line
57
of file
em_lesense.h
.
Referenced by LESENSE_DecoderStateAllConfig() , LESENSE_DecoderStateConfig() , and LESENSE_Reset() .
#define LESENSE_PERCTRL_DESC_DEFAULT |
Default configuration for LESENSE_PerCtrl_TypeDef structure.
Definition at line
641
of file
em_lesense.h
.
#define LESENSE_SCAN_CONF_DEFAULT |
Default configuration for all sensor channels.
Definition at line
902
of file
em_lesense.h
.
#define LESENSE_ST_CONF_DEFAULT |
Default configuration for decoder state condition.
Definition at line
1045
of file
em_lesense.h
.
#define LESENSE_TIMECTRL_DESC_DEFAULT |
Default configuration for LESENSE_TimeCtrlDesc_TypeDef structure.
Definition at line
561
of file
em_lesense.h
.
Enumeration Type Documentation
Idle phase configuration of alternate excitation channels.
Definition at line
431
of file
em_lesense.h
.
Bias modes.
Definition at line
168
of file
em_lesense.h
.
Compare modes for counter comparison.
Definition at line
395
of file
em_lesense.h
.
Interrupt generation setup for CHx interrupt flag.
Definition at line
327
of file
em_lesense.h
.
Channel pin mode for the excitation phase of the scan sequence.
Definition at line
342
of file
em_lesense.h
.
Channel pin mode for the idle phase of the scan sequence.
Definition at line
357
of file
em_lesense.h
.
Clock divisors for controlling the prescaling factor of the period counter. Note: these enumeration values are being used for different clock division related configuration parameters (hfPresc, lfPresc, pcPresc).
Definition at line
70
of file
em_lesense.h
.
ACMPx control configuration.
Definition at line
271
of file
em_lesense.h
.
DAC channel x conversion mode configuration.
Definition at line
219
of file
em_lesense.h
.
DAC CHx data control configuration.
Definition at line
199
of file
em_lesense.h
.
DAC channel x output mode configuration.
Definition at line
240
of file
em_lesense.h
.
Modes of operation for DMA wakeup from EM2.
Definition at line
154
of file
em_lesense.h
.
PRS sources. Note: these enumeration values are being used for different PRS related configuration parameters.
Definition at line
96
of file
em_lesense.h
.
Scan configuration.
Definition at line
180
of file
em_lesense.h
.
Scan modes.
Enumerator | |
---|---|
lesenseScanStartPeriodic |
New scan is started each time the period counter overflows. |
lesenseScanStartOneShot |
Single scan is performed when LESENSE_ScanStart() is called. |
lesenseScanStartPRS |
New scan is triggered by pulse on PRS channel. |
Definition at line
82
of file
em_lesense.h
.
Transition action modes.
Definition at line
446
of file
em_lesense.h
.
Warm up modes. ACMP and DAC duty cycle mode configuration.
Definition at line
286
of file
em_lesense.h
.
Function Documentation
void LESENSE_AltExConfig | ( | const LESENSE_ConfAltEx_TypeDef * |
confAltEx
|
) |
Configure the LESENSE alternate excitation modes.
This function configures the alternate excitation channels of the LESENSE interface. Please refer to the configuration parameter type definition ( LESENSE_ConfAltEx_TypeDef ) for more details.
- Note
-
Parameter
useAltEx
must be true in the channel configuration structrure ( LESENSE_ChDesc_TypeDef ) in order to use alternate excitation pins on the channel.
- Parameters
-
[in] confAltEx
Configuration structure for LESENSE alternate excitation pins.
Definition at line
605
of file
em_lesense.c
.
References _LESENSE_CTRL_ALTEXMAP_SHIFT , LESENSE_ConfAltEx_TypeDef::AltEx , LESENSE_ConfAltEx_TypeDef::altExMap , LESENSE_AltExDesc_TypeDef::alwaysEx , BUS_RegBitWrite() , LESENSE_AltExDesc_TypeDef::enablePin , LESENSE_AltExDesc_TypeDef::idleConf , LESENSE , lesenseAltExMapACMP , and lesenseAltExMapALTEX .
__STATIC_INLINE uint32_t LESENSE_ChannelActiveGet | ( | void |
|
) |
Get the currently active channel index.
- Returns
- This function returns the value of LESENSE_CHINDEX register that contains the index of the currently active channel (0-15).
Definition at line
1258
of file
em_lesense.h
.
References LESENSE .
void LESENSE_ChannelAllConfig | ( | const LESENSE_ChAll_TypeDef * |
confChAll
|
) |
Configure all (16) LESENSE sensor channels.
This function configures all the sensor channels of LESENSE interface. Please refer to the configuration parameter type definition ( LESENSE_ChAll_TypeDef ) for more details.
- Note
- Channels can be configured individually using LESENSE_ChannelConfig() function. Notice that pins used by the LESENSE module must be properly configured by the user explicitly, in order for the LESENSE to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] confChAll
Configuration structure for all (16) LESENSE sensor channels.
Definition at line
466
of file
em_lesense.c
.
References LESENSE_ChAll_TypeDef::Ch , LESENSE_ChannelConfig() , and LESENSE_NUM_CHANNELS .
Referenced by CAPLESENSE_setupLESENSE() .
void LESENSE_ChannelConfig | ( | const LESENSE_ChDesc_TypeDef * |
confCh,
|
uint32_t |
chIdx
|
||
) |
Configure a single LESENSE sensor channel.
This function configures a single sensor channel of the LESENSE interface. Please refer to the configuration parameter type definition ( LESENSE_ChDesc_TypeDef ) for more details.
- Note
-
This function has been designed to minimize the effects of sensor channel reconfiguration while LESENSE is in operation, however one shall be aware of these effects and the right timing of calling this function. Parameter
useAltEx
must be true in the channel configuration in order to use alternate excitation pins.
- Parameters
-
[in] confCh
Configuration structure for a single LESENSE sensor channel. [in] chIdx
Channel index to configure (0-15).
Definition at line
499
of file
em_lesense.c
.
References _LESENSE_CH_EVAL_DECODE_SHIFT , _LESENSE_CH_EVAL_SCANRESINV_SHIFT , _LESENSE_CH_EVAL_STRSAMPLE_SHIFT , _LESENSE_CH_INTERACT_ALTEX_SHIFT , _LESENSE_CH_INTERACT_EXCLK_SHIFT , _LESENSE_CH_INTERACT_SAMPLECLK_SHIFT , _LESENSE_CH_TIMING_EXTIME_MASK , _LESENSE_CH_TIMING_EXTIME_SHIFT , _LESENSE_CH_TIMING_MEASUREDLY_MASK , _LESENSE_CH_TIMING_MEASUREDLY_SHIFT , _LESENSE_CH_TIMING_SAMPLEDLY_MASK , _LESENSE_CH_TIMING_SAMPLEDLY_SHIFT , LESENSE_ChDesc_TypeDef::acmpThres , BUS_RegBitWrite() , LESENSE_ChDesc_TypeDef::chPinExMode , LESENSE_ChDesc_TypeDef::chPinIdleMode , LESENSE_ChDesc_TypeDef::cntThres , LESENSE_ChDesc_TypeDef::compMode , LESENSE_ChDesc_TypeDef::enaInt , LESENSE_ChDesc_TypeDef::enaPin , LESENSE_ChDesc_TypeDef::enaScanCh , LESENSE_ChDesc_TypeDef::exClk , LESENSE_ChDesc_TypeDef::exTime , LESENSE_ChDesc_TypeDef::intMode , LESENSE_ChDesc_TypeDef::invRes , LESENSE , LESENSE_ChannelThresSet() , LESENSE_ChannelTimingSet() , LESENSE_NUM_CHANNELS , lesenseChPinExDACOut , lesenseChPinIdleDACCh0 , lesenseChPinIdleDACCh1 , LESENSE_ChDesc_TypeDef::measDelay , LESENSE_ChDesc_TypeDef::sampleClk , LESENSE_ChDesc_TypeDef::sampleDelay , LESENSE_ChDesc_TypeDef::sampleMode , LESENSE_ChDesc_TypeDef::shiftRes , LESENSE_ChDesc_TypeDef::storeCntRes , and LESENSE_ChDesc_TypeDef::useAltEx .
Referenced by LESENSE_ChannelAllConfig() .
void LESENSE_ChannelEnable | ( | uint8_t |
chIdx,
|
bool |
enaScanCh,
|
||
bool |
enaPin
|
||
) |
Enable/disable LESENSE scan channel and the pin assigned to it.
Use this function to enable/disable a selected LESENSE scan channel and the pin assigned to.
- Note
- Users can enable/disable scan channels and the channel pin by LESENSE_ChannelConfig() function, but only with a significant overhead. This simple function serves the purpose of controlling these parameters after the channel has been configured.
- Parameters
-
[in] chIdx
Identifier of the scan channel. Valid range: 0-15. [in] enaScanCh
Enable/disable the selected scan channel by setting this parameter to true/false respectively. [in] enaPin
Enable/disable the pin assigned to the channel selected by chIdx
.
Definition at line
688
of file
em_lesense.c
.
References BUS_RegBitWrite() , and LESENSE .
void LESENSE_ChannelEnableMask | ( | uint16_t |
chMask,
|
uint16_t |
pinMask
|
||
) |
Enable/disable LESENSE scan channel and the pin assigned to it.
Use this function to enable/disable LESENSE scan channels and the pins assigned to them using a mask.
- Note
- Users can enable/disable scan channels and channel pins by using LESENSE_ChannelAllConfig() function, but only with a significant overhead. This simple function serves the purpose of controlling these parameters after the channel has been configured.
- Parameters
-
[in] chMask
Set the corresponding bit to 1 to enable, 0 to disable the selected scan channel. [in] pinMask
Set the corresponding bit to 1 to enable, 0 to disable the pin on selected channel.
Definition at line
724
of file
em_lesense.c
.
References LESENSE .
void LESENSE_ChannelThresSet | ( | uint8_t |
chIdx,
|
uint16_t |
acmpThres,
|
||
uint16_t |
cntThres
|
||
) |
Set LESENSE channel threshold parameters.
Use this function to set threshold parameters on a selected LESENSE channel.
- Note
- Users can configure the channel threshold parameters by LESENSE_ChannelConfig() function, but only with a significant overhead. This simple function serves the purpose of controlling these parameters after the channel has been configured.
- Parameters
-
[in] chIdx
Identifier of the scan channel. Valid range: 0-15. [in] acmpThres
ACMP threshold. - If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseDACIfData , acmpThres defines the 12-bit DAC data in the corresponding data register of the DAC interface (DACn_CH0DATA and DACn_CH1DATA). In this case, the valid range is: 0-4095 (12 bits).
- If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseACMPThres , acmpThres defines the 6-bit Vdd scaling factor of ACMP negative input (VDDLEVEL in ACMP_INPUTSEL register). In this case, the valid range is: 0-63 (6 bits).
[in] cntThres
Decision threshold for counter comparison. Valid range: 0-65535 (16 bits).
Definition at line
814
of file
em_lesense.c
.
References _LESENSE_CH_EVAL_COMPTHRES_MASK , _LESENSE_CH_EVAL_COMPTHRES_SHIFT , LESENSE , and LESENSE_NUM_CHANNELS .
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_ChannelConfig() .
void LESENSE_ChannelTimingSet | ( | uint8_t |
chIdx,
|
uint8_t |
exTime,
|
||
uint8_t |
sampleDelay,
|
||
uint16_t |
measDelay
|
||
) |
Set LESENSE channel timing parameters.
Use this function to set timing parameters on a selected LESENSE channel.
- Note
- Users can configure the channel timing parameters by LESENSE_ChannelConfig() function, but only with a significant overhead. This simple function serves the purpose of controlling these parameters after the channel has been configured.
- Parameters
-
[in] chIdx
Identifier of the scan channel. Valid range: 0-15. [in] exTime
Excitation time on chIdx. Excitation will last exTime+1 excitation clock cycles. Valid range: 0-63 (6 bits). [in] sampleDelay
Sample delay on chIdx. Sampling will occur after sampleDelay+1 sample clock cycles. Valid range: 0-127 (7 bits). [in] measDelay
Measure delay on chIdx. Sensor measuring is delayed for measDelay+1 excitation clock cycles. Valid range: 0-127 (7 bits).
Definition at line
760
of file
em_lesense.c
.
References _LESENSE_CH_TIMING_EXTIME_MASK , _LESENSE_CH_TIMING_EXTIME_SHIFT , _LESENSE_CH_TIMING_MEASUREDLY_MASK , _LESENSE_CH_TIMING_MEASUREDLY_SHIFT , _LESENSE_CH_TIMING_SAMPLEDLY_MASK , _LESENSE_CH_TIMING_SAMPLEDLY_SHIFT , and LESENSE .
Referenced by LESENSE_ChannelConfig() .
void LESENSE_ClkDivSet | ( | LESENSE_ChClk_TypeDef |
clk,
|
LESENSE_ClkPresc_TypeDef |
clkDiv
|
||
) |
Set clock division for LESENSE timers.
Use this function to configure the clock division for the LESENSE timers used for excitation timing. The division setting is global, but the clock source can be selected for each channel using LESENSE_ChannelConfig() function, please refer to the documentation of it for more details.
- Note
- If AUXHFRCO is used for excitation timing, LFACLK can not exceed 500kHz. LFACLK can not exceed 50kHz if the ACMP threshold level (ACMPTHRES) is not equal for all channels.
- Parameters
-
[in] clk
Select clock to prescale. - lesenseClkHF - set AUXHFRCO clock divisor for HF timer.
- lesenseClkLF - set LFACLKles clock divisor for LF timer.
[in] clkDiv
Clock divisor value. Valid range depends on the clk
value.
Definition at line
407
of file
em_lesense.c
.
References _LESENSE_TIMCTRL_AUXPRESC_MASK , _LESENSE_TIMCTRL_AUXPRESC_SHIFT , _LESENSE_TIMCTRL_LFPRESC_MASK , _LESENSE_TIMCTRL_LFPRESC_SHIFT , LESENSE , lesenseClkDiv_8 , lesenseClkHF , and lesenseClkLF .
Referenced by CAPLESENSE_setupLESENSE() .
void LESENSE_DecoderStart | ( | void |
|
) |
Start LESENSE decoder.
- Note
- This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so the user should expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation in order to optimize an application.
Definition at line
1169
of file
em_lesense.c
.
References LESENSE , LESENSE_CMD_DECODE , and LESENSE_SYNCBUSY_CMD .
void LESENSE_DecoderStateAllConfig | ( | const LESENSE_DecStAll_TypeDef * |
confDecStAll
|
) |
Configure all LESENSE decoder states.
This function configures all the decoder states of the LESENSE interface. Please refer to the configuration parameter type definition ( LESENSE_DecStAll_TypeDef ) for more details.
- Note
- Decoder states can be configured individually using LESENSE_DecoderStateConfig() function.
- Parameters
-
[in] confDecStAll
Configuration structure for all (16 or 32) LESENSE decoder states.
Definition at line
975
of file
em_lesense.c
.
References LESENSE_DecoderStateConfig() , LESENSE_NUM_DECODER_STATES , and LESENSE_DecStAll_TypeDef::St .
void LESENSE_DecoderStateConfig | ( | const LESENSE_DecStDesc_TypeDef * |
confDecSt,
|
uint32_t |
decSt
|
||
) |
Configure a single LESENSE decoder state.
This function configures a single decoder state of the LESENSE interface. Please refer to the configuration parameter type definition ( LESENSE_DecStDesc_TypeDef ) for more details.
- Parameters
-
[in] confDecSt
Configuration structure for a single LESENSE decoder state. [in] decSt
Decoder state index to configure (0-15) or (0-31) depending on device.
Definition at line
1001
of file
em_lesense.c
.
References _LESENSE_ST_TCONFA_CHAIN_SHIFT , _LESENSE_ST_TCONFA_COMP_SHIFT , _LESENSE_ST_TCONFA_MASK_SHIFT , _LESENSE_ST_TCONFA_NEXTSTATE_SHIFT , _LESENSE_ST_TCONFA_SETIF_SHIFT , _LESENSE_ST_TCONFB_COMP_SHIFT , _LESENSE_ST_TCONFB_MASK_SHIFT , _LESENSE_ST_TCONFB_NEXTSTATE_SHIFT , _LESENSE_ST_TCONFB_SETIF_SHIFT , LESENSE_DecStDesc_TypeDef::chainDesc , LESENSE_DecStCond_TypeDef::compMask , LESENSE_DecStCond_TypeDef::compVal , LESENSE_DecStDesc_TypeDef::confA , LESENSE_DecStDesc_TypeDef::confB , LESENSE , LESENSE_NUM_DECODER_STATES , LESENSE_DecStCond_TypeDef::nextState , LESENSE_DecStCond_TypeDef::prsAct , and LESENSE_DecStCond_TypeDef::setInt .
Referenced by LESENSE_DecoderStateAllConfig() .
uint32_t LESENSE_DecoderStateGet | ( | void |
|
) |
Get the current state of the LESENSE decoder.
- Returns
- This function returns the value of LESENSE_DECSTATE register that represents the current state of the LESENSE decoder.
Definition at line
1067
of file
em_lesense.c
.
References _LESENSE_DECSTATE_DECSTATE_MASK , and LESENSE .
void LESENSE_DecoderStateSet | ( | uint32_t |
decSt
|
) |
Set LESENSE decoder state.
This function can be used for setting the initial state of the LESENSE decoder.
- Note
- Make sure the LESENSE decoder state is initialized by this function before enabling the decoder!
- Parameters
-
[in] decSt
Decoder state to set as current state. Valid range: 0-15 or 0-31 depending on device.
Definition at line
1052
of file
em_lesense.c
.
References _LESENSE_DECSTATE_DECSTATE_MASK , and LESENSE .
Referenced by LESENSE_Init() .
__STATIC_INLINE void LESENSE_DecoderStop | ( | void |
|
) |
Stop LESENSE decoder.
This function disables the LESENSE decoder by setting the command to the LESENSE_DECCTRL register.
Definition at line
1199
of file
em_lesense.h
.
References LESENSE , and LESENSE_DECCTRL_DISABLE .
void LESENSE_Init | ( | const LESENSE_Init_TypeDef * |
init,
|
bool |
reqReset
|
||
) |
Initialize the LESENSE module.
This function configures the main parameters of the LESENSE interface. Please refer to the initialization parameter type definition ( LESENSE_Init_TypeDef ) for more details.
- Note
-
LESENSE_Init()
has been designed for initializing LESENSE once in an operation cycle. Be aware of the effects of reconfiguration if using this function from multiple sources in your code. This function has not been designed to be re-entrant. Requesting reset by setting
reqReset
to true is required in each reset or power-on cycle in order to configure the default values of the RAM mapped LESENSE registers. Notice that GPIO pins used by the LESENSE module must be properly configured by the user explicitly, in order for the LESENSE to work as intended. (When configuring pins, one should remember to consider the sequence of configuration, in order to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] init
LESENSE initialization structure. [in] reqReset
Request to call LESENSE_Reset() first in order to initialize all LESENSE registers with the default value.
Definition at line
117
of file
em_lesense.c
.
References _LESENSE_CTRL_ACMP0INV_MASK , _LESENSE_CTRL_ACMP0INV_SHIFT , _LESENSE_CTRL_ACMP1INV_SHIFT , _LESENSE_CTRL_BUFOW_SHIFT , _LESENSE_CTRL_DEBUGRUN_SHIFT , _LESENSE_CTRL_DUALSAMPLE_SHIFT , _LESENSE_CTRL_PRSSEL_SHIFT , _LESENSE_CTRL_STRSCANRES_SHIFT , _LESENSE_DECCTRL_ERRCHK_SHIFT , _LESENSE_DECCTRL_HYSTIRQ_SHIFT , _LESENSE_DECCTRL_HYSTPRS0_SHIFT , _LESENSE_DECCTRL_HYSTPRS1_SHIFT , _LESENSE_DECCTRL_HYSTPRS2_SHIFT , _LESENSE_DECCTRL_INTMAP_SHIFT , _LESENSE_DECCTRL_PRSCNT_SHIFT , _LESENSE_DECCTRL_PRSSEL0_SHIFT , _LESENSE_DECCTRL_PRSSEL1_SHIFT , _LESENSE_DECCTRL_PRSSEL2_SHIFT , _LESENSE_DECCTRL_PRSSEL3_SHIFT , _LESENSE_PERCTRL_ACMP0MODE_SHIFT , _LESENSE_PERCTRL_ACMP1MODE_SHIFT , _LESENSE_PERCTRL_DACCH0CONV_SHIFT , _LESENSE_PERCTRL_DACCH0DATA_SHIFT , _LESENSE_PERCTRL_DACCH0OUT_SHIFT , _LESENSE_PERCTRL_DACCH1CONV_SHIFT , _LESENSE_PERCTRL_DACCH1DATA_SHIFT , _LESENSE_PERCTRL_DACCH1OUT_SHIFT , _LESENSE_PERCTRL_DACPRESC_SHIFT , LESENSE_PerCtrlDesc_TypeDef::acmp0Mode , LESENSE_PerCtrlDesc_TypeDef::acmp1Mode , LESENSE_CoreCtrlDesc_TypeDef::biasMode , LESENSE_CoreCtrlDesc_TypeDef::bufOverWr , LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel , LESENSE_DecCtrlDesc_TypeDef::chkState , LESENSE_Init_TypeDef::coreCtrl , LESENSE_PerCtrlDesc_TypeDef::dacCh0ConvMode , LESENSE_PerCtrlDesc_TypeDef::dacCh0Data , LESENSE_PerCtrlDesc_TypeDef::dacCh0OutMode , LESENSE_PerCtrlDesc_TypeDef::dacCh1ConvMode , LESENSE_PerCtrlDesc_TypeDef::dacCh1Data , LESENSE_PerCtrlDesc_TypeDef::dacCh1OutMode , LESENSE_PerCtrlDesc_TypeDef::dacPresc , LESENSE_PerCtrlDesc_TypeDef::dacRef , LESENSE_CoreCtrlDesc_TypeDef::debugRun , LESENSE_Init_TypeDef::decCtrl , LESENSE_DecCtrlDesc_TypeDef::decInput , LESENSE_TimeCtrlDesc_TypeDef::delayAuxStartup , LESENSE_CoreCtrlDesc_TypeDef::dualSample , LESENSE_DecCtrlDesc_TypeDef::hystIRQ , LESENSE_DecCtrlDesc_TypeDef::hystPRS0 , LESENSE_DecCtrlDesc_TypeDef::hystPRS1 , LESENSE_DecCtrlDesc_TypeDef::hystPRS2 , LESENSE_DecCtrlDesc_TypeDef::initState , LESENSE_DecCtrlDesc_TypeDef::intMap , LESENSE_CoreCtrlDesc_TypeDef::invACMP0 , LESENSE_CoreCtrlDesc_TypeDef::invACMP1 , LESENSE , LESENSE_DecoderStateSet() , LESENSE_Reset() , LESENSE_ScanModeSet() , LESENSE_StartDelaySet() , LESENSE_Init_TypeDef::perCtrl , LESENSE_DecCtrlDesc_TypeDef::prsChSel0 , LESENSE_DecCtrlDesc_TypeDef::prsChSel1 , LESENSE_DecCtrlDesc_TypeDef::prsChSel2 , LESENSE_DecCtrlDesc_TypeDef::prsChSel3 , LESENSE_DecCtrlDesc_TypeDef::prsCount , LESENSE_CoreCtrlDesc_TypeDef::prsSel , LESENSE_CoreCtrlDesc_TypeDef::scanConfSel , LESENSE_CoreCtrlDesc_TypeDef::scanStart , LESENSE_TimeCtrlDesc_TypeDef::startDelay , LESENSE_CoreCtrlDesc_TypeDef::storeScanRes , LESENSE_Init_TypeDef::timeCtrl , LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA , and LESENSE_PerCtrlDesc_TypeDef::warmupMode .
Referenced by CAPLESENSE_setupLESENSE() .
__STATIC_INLINE void LESENSE_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending LESENSE interrupts.
- Parameters
-
[in] flags
Pending LESENSE interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources of the LESENSE module (LESENSE_IF_nnn).
Definition at line
1360
of file
em_lesense.h
.
References LESENSE .
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_IRQHandler() .
__STATIC_INLINE void LESENSE_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more LESENSE interrupts.
- Parameters
-
[in] flags
LESENSE interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources of the LESENSE module (LESENSE_IF_nnn).
Definition at line
1388
of file
em_lesense.h
.
References LESENSE .
Referenced by CAPLESENSE_setupLESENSE() .
__STATIC_INLINE void LESENSE_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more LESENSE interrupts.
- Parameters
-
[in] flags
LESENSE interrupt sources to enable. Use a set of interrupt flags OR-ed together to enable multiple interrupt sources of the LESENSE module (LESENSE_IF_nnn).
Definition at line
1374
of file
em_lesense.h
.
References LESENSE .
Referenced by CAPLESENSE_setupLESENSE() .
__STATIC_INLINE uint32_t LESENSE_IntGet | ( | void |
|
) |
Get pending LESENSE interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending LESENSE interrupt sources. The OR combination of valid interrupt flags of the LESENSE module (LESENSE_IF_nnn).
Definition at line
1418
of file
em_lesense.h
.
References LESENSE .
__STATIC_INLINE uint32_t LESENSE_IntGetEnabled | ( | void |
|
) |
Get enabled and pending LESENSE interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- The event bits are not cleared by the use of this function.
- Returns
-
Pending and enabled LESENSE interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in LESENSE_IEN_nnn register (LESENSE_IEN_nnn) and
- the OR combination of valid interrupt flags of the LESENSE module (LESENSE_IF_nnn).
Definition at line
1441
of file
em_lesense.h
.
References LESENSE .
Referenced by LESENSE_IRQHandler() .
__STATIC_INLINE void LESENSE_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending LESENSE interrupts from SW.
- Parameters
-
[in] flags
LESENSE interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources of the LESENSE module (LESENSE_IFS_nnn).
Definition at line
1402
of file
em_lesense.h
.
References LESENSE .
__STATIC_INLINE void LESENSE_RAMPowerDown | ( | void |
|
) |
Shut off power to the LESENSE RAM, disables LESENSE.
This function shuts off the LESENSE RAM in order to decrease the leakage current of the mcu if LESENSE is not used in your application.
- Note
- Warning! Once the LESENSE RAM is powered down, it cannot be powered up again.
Definition at line
1344
of file
em_lesense.h
.
References LESENSE , and LESENSE_POWERDOWN_RAM .
void LESENSE_Reset | ( | void |
|
) |
Reset the LESENSE module.
Use this function to reset the LESENSE registers.
- Note
-
Resetting LESENSE registers is required in each reset or power-on cycle in order to configure the default values of the RAM mapped LESENSE registers.
LESENSE_Reset()
can be called on initialization by setting the
reqReset
parameter to true in LESENSE_Init() .
Definition at line
1226
of file
em_lesense.c
.
References _LESENSE_ALTEXCONF_RESETVALUE , _LESENSE_BIASCTRL_RESETVALUE , _LESENSE_CH_EVAL_RESETVALUE , _LESENSE_CH_INTERACT_RESETVALUE , _LESENSE_CH_TIMING_RESETVALUE , _LESENSE_CHEN_RESETVALUE , _LESENSE_CTRL_RESETVALUE , _LESENSE_DECCTRL_RESETVALUE , _LESENSE_IDLECONF_RESETVALUE , _LESENSE_IEN_RESETVALUE , _LESENSE_IFC_MASK , _LESENSE_PERCTRL_RESETVALUE , _LESENSE_ROUTE_RESETVALUE , _LESENSE_ST_TCONFA_RESETVALUE , _LESENSE_ST_TCONFB_RESETVALUE , LESENSE , LESENSE_CMD_CLEARBUF , LESENSE_CMD_STOP , LESENSE_DECCTRL_DISABLE , LESENSE_NUM_CHANNELS , LESENSE_NUM_DECODER_STATES , and LESENSE_SYNCBUSY_CMD .
Referenced by LESENSE_Init() .
void LESENSE_ResultBufferClear | ( | void |
|
) |
Clear result buffer.
- Note
- This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so the user should expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation in order to optimize an application.
Definition at line
1198
of file
em_lesense.c
.
References LESENSE , LESENSE_CMD_CLEARBUF , and LESENSE_SYNCBUSY_CMD .
Referenced by CAPLESENSE_setupLESENSE() .
uint32_t LESENSE_ScanFreqSet | ( | uint32_t |
refFreq,
|
uint32_t |
scanFreq
|
||
) |
Set scan frequency for periodic scanning.
This function only applies to LESENSE if period counter is being used as a trigger for scan start. The calculation is based on the following formula: Fscan = LFACLKles / ((1+PCTOP)*2^PCPRESC)
- Note
- Note that the calculation does not necessarily result in the requested scan frequency due to integer division. Check the return value for the resulted scan frequency.
- Parameters
-
[in] refFreq
Select reference LFACLK clock frequency in Hz. If set to 0, the current clock frequency is being used as a reference. [in] scanFreq
Set the desired scan frequency in Hz.
- Returns
- Frequency in Hz calculated and set by this function. Users can use this to compare the requested and set values.
Definition at line
249
of file
em_lesense.c
.
References _LESENSE_TIMCTRL_PCPRESC_MASK , _LESENSE_TIMCTRL_PCPRESC_SHIFT , _LESENSE_TIMCTRL_PCTOP_MASK , _LESENSE_TIMCTRL_PCTOP_SHIFT , CMU_ClockFreqGet() , cmuClock_LESENSE , LESENSE , and lesenseClkDiv_128 .
Referenced by CAPLESENSE_setupLESENSE() .
void LESENSE_ScanModeSet | ( | LESENSE_ScanMode_TypeDef |
scanMode,
|
bool |
start
|
||
) |
Set scan mode of the LESENSE channels.
This function configures how the scan start is being triggered. It can be used for re-configuring the scan mode while running the application but it is also used by LESENSE_Init() for initialization.
- Note
- Users can configure the scan mode by LESENSE_Init() function, but only with a significant overhead. This simple function serves the purpose of controlling this parameter after the channel has been configured. Please be aware the effects of the non-atomic Read-Modify-Write cycle!
- Parameters
-
[in] scanMode
Select where to map LESENSE alternate excitation channels. - lesenseScanStartPeriodic - New scan is started each time the period counter overflows.
- lesenseScanStartOneShot - Single scan is performed when LESENSE_ScanStart() is called.
- lesenseScanStartPRS - New scan is triggered by pulse on PRS channel.
[in] start
If true, LESENSE_ScanStart() is immediately issued after configuration.
Definition at line
327
of file
em_lesense.c
.
References _LESENSE_CTRL_SCANMODE_MASK , LESENSE , and LESENSE_ScanStart() .
Referenced by LESENSE_Init() .
__STATIC_INLINE uint32_t LESENSE_ScanResultDataBufferGet | ( | uint32_t |
idx
|
) |
Get data from the result data buffer.
- Note
- Make sure that the STORERES bit is set in LESENSE_CHx_EVAL, or STRSCANRES bit is set in LESENSE_CTRL, otherwise this function will return undefined value.
- Parameters
-
[in] idx
Result data buffer index. Valid range: 0-15.
- Returns
- This function returns the selected word from the result data buffer.
Definition at line
1312
of file
em_lesense.h
.
References LESENSE .
Referenced by CAPLESENSE_setupLESENSE() .
__STATIC_INLINE uint32_t LESENSE_ScanResultDataGet | ( | void |
|
) |
Get the oldest unread data from the result buffer.
- Note
- Make sure that the STORERES bit is set in LESENSE_CHx_EVAL, or STRSCANRES bit is set in LESENSE_CTRL, otherwise this function will return undefined value.
- Returns
- This function returns the value of LESENSE_RESDATA register that contains the oldest unread counter result from the result buffer.
Definition at line
1292
of file
em_lesense.h
.
References LESENSE .
Referenced by LESENSE_IRQHandler() .
__STATIC_INLINE uint32_t LESENSE_ScanResultGet | ( | void |
|
) |
Get the latest scan comparison result (1 bit / channel).
- Returns
- This function returns the value of LESENSE_SCANRES register that contains the comparison result of the last scan on all channels. Bit x is set if a comparison triggered on channel x, which means that the LESENSE counter met the comparison criteria set in LESENSE_CHx_EVAL by COMPMODE and CNTTHRES.
Definition at line
1274
of file
em_lesense.h
.
References _LESENSE_SCANRES_SCANRES_MASK , and LESENSE .
void LESENSE_ScanStart | ( | void |
|
) |
Start scanning of sensors.
- Note
- This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so the user should expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation in order to optimize an application.
Definition at line
1108
of file
em_lesense.c
.
References LESENSE , LESENSE_CMD_START , and LESENSE_SYNCBUSY_CMD .
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_ScanModeSet() .
void LESENSE_ScanStop | ( | void |
|
) |
Stop scanning of sensors.
- Note
- This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so the user should expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation in order to optimize an application.
- If issued during a scan, the command takes effect after scan completion.
Definition at line
1140
of file
em_lesense.c
.
References LESENSE , LESENSE_CMD_STOP , and LESENSE_SYNCBUSY_CMD .
Referenced by CAPLESENSE_setupLESENSE() .
__STATIC_INLINE uint32_t LESENSE_SensorStateGet | ( | void |
|
) |
Get the current state of the LESENSE sensor.
- Returns
- This function returns the value of LESENSE_SENSORSTATE register that represents the current state of the LESENSE sensor.
Definition at line
1326
of file
em_lesense.h
.
References LESENSE .
void LESENSE_StartDelaySet | ( | uint8_t |
startDelay
|
) |
Set start delay of sensor interaction on each channel.
This function sets start delay of sensor interaction on each channel. It can be used for adjusting the start delay while running the application but it is also used by LESENSE_Init() for initialization.
- Note
- Users can configure the start delay by LESENSE_Init() function, but only with a significant overhead. This simple function serves the purpose of controlling this parameter after the channel has been configured. Please be aware the effects of the non-atomic Read-Modify-Write cycle!
- Parameters
-
[in] startDelay
Number of LFACLK cycles to delay. Valid range: 0-3 (2 bit).
Definition at line
366
of file
em_lesense.c
.
References _LESENSE_TIMCTRL_STARTDLY_MASK , _LESENSE_TIMCTRL_STARTDLY_SHIFT , and LESENSE .
Referenced by LESENSE_Init() .
__STATIC_INLINE uint32_t LESENSE_StatusGet | ( | void |
|
) |
Get the current status of LESENSE.
- Returns
-
This function returns the value of LESENSE_STATUS register that contains the OR combination of the following status bits:
- LESENSE_STATUS_RESV - Result data valid. Set when data is available in the result buffer. Cleared when the buffer is empty.
- LESENSE_STATUS_RESFULL - Result buffer full. Set when the result buffer is full.
- LESENSE_STATUS_RUNNING - LESENSE is active.
- LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.
Definition at line
1219
of file
em_lesense.h
.
References LESENSE .
Referenced by CAPLESENSE_setupLESENSE() .
__STATIC_INLINE void LESENSE_StatusWait | ( | uint32_t |
flag
|
) |
Wait until the status of LESENSE is equal to what requested.
This function is polling the LESENSE_STATUS register and waits until the requested combination of flags are set.
- Parameters
-
[in] flag
The OR combination of the following status bits: - LESENSE_STATUS_BUFDATAV - Result data valid. Set when data is available in the result buffer. Cleared when the buffer is empty.
- LESENSE_STATUS_BUFHALFFULL - Result buffer half full. Set when the result buffer is half full.
- LESENSE_STATUS_BUFFULL - Result buffer full. Set when the result buffer is full.
- LESENSE_STATUS_RUNNING - LESENSE is active.
- LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.
- LESENSE_STATUS_DACACTIVE - The DAC interface is currently active.
Definition at line
1244
of file
em_lesense.h
.
References LESENSE .