ACMP_CapsenseInit_TypeDef Struct ReferenceEMLIB > ACMP
Capsense initialization structure.
Definition at line 525
of file em_acmp.h
.
#include <
em_acmp.h
>
Data Fields | |
uint32_t | biasProg |
bool | enable |
bool | fullBias |
bool | halfBias |
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
bool | lowPowerReferenceEnabled |
ACMP_CapsenseResistor_TypeDef | resistor |
uint32_t | vddLevel |
ACMP_WarmTime_TypeDef | warmTime |
Field Documentation
uint32_t ACMP_CapsenseInit_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line 538
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
bool ACMP_CapsenseInit_TypeDef::enable |
If true, ACMP is being enabled after configuration.
Definition at line 592
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
bool ACMP_CapsenseInit_TypeDef::fullBias |
Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line 528
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit(), and CAPLESENSE_setupACMP().
bool ACMP_CapsenseInit_TypeDef::halfBias |
Half bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line 533
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel |
bool ACMP_CapsenseInit_TypeDef::lowPowerReferenceEnabled |
Low power reference enabled. This setting, if enabled, reduces the power used by the VDD and bandgap references.
Definition at line 564
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor |
Resistor used in the capacative sensing circuit. For values see your device datasheet.
Definition at line 559
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
uint32_t ACMP_CapsenseInit_TypeDef::vddLevel |
Vdd reference value. VDD_SCALED = (Vdd * VDDLEVEL) / 63. Valid values are in the range 0-63.
Definition at line 570
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
ACMP_WarmTime_TypeDef ACMP_CapsenseInit_TypeDef::warmTime |
Warmup time. This is measured in HFPERCLK cycles and should be about 10us in wall clock time.
Definition at line 543
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_acmp.h