RMU_TypeDef Struct ReferenceDevices > EFM32LG_RMU

Definition at line 48 of file efm32lg_rmu.h .

Data Fields

__OM uint32_t CMD
__IOM uint32_t CTRL
__IM uint32_t RSTCAUSE

Field Documentation

__OM uint32_t RMU_TypeDef::CMD

Command Register

Definition at line 51 of file efm32lg_rmu.h .

__IOM uint32_t RMU_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32lg_rmu.h .

__IM uint32_t RMU_TypeDef::RSTCAUSE

Reset Cause Register

Definition at line 50 of file efm32lg_rmu.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_rmu.h