MSDSCSI_Inquiry_TypeDef Struct ReferenceKit Drivers > Msd

SCSI Inquiry Command Descriptor Block (CDB) typedef.

Definition at line 56 of file msdscsi.h .

#include < msdscsi.h >

Data Fields

struct {
uint8_t Evpd : 1
uint8_t Obsolete : 1
uint8_t Reserved : 6
};
uint16_t AllocationLength
uint8_t Control
uint8_t OpCode
uint8_t PageCode

Field Documentation

uint16_t MSDSCSI_Inquiry_TypeDef::AllocationLength

Number of inquiry data bytes requested.

Definition at line 64 of file msdscsi.h .

uint8_t MSDSCSI_Inquiry_TypeDef::Control

Control byte.

Definition at line 65 of file msdscsi.h .

uint8_t MSDSCSI_Inquiry_TypeDef::Evpd

Enable Vital Product data.

Definition at line 59 of file msdscsi.h .

uint8_t MSDSCSI_Inquiry_TypeDef::Obsolete

Obsolete, expect any value.

Definition at line 60 of file msdscsi.h .

uint8_t MSDSCSI_Inquiry_TypeDef::OpCode

Command opcode.

Definition at line 57 of file msdscsi.h .

uint8_t MSDSCSI_Inquiry_TypeDef::PageCode

Pagecode.

Definition at line 63 of file msdscsi.h .

uint8_t MSDSCSI_Inquiry_TypeDef::Reserved

Reserved, expect 0.

Definition at line 61 of file msdscsi.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/ msdscsi.h