WDOG_TypeDef Struct ReferenceDevices > EFM32LG_WDOG

Definition at line 48 of file efm32lg_wdog.h .

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CTRL
__IM uint32_t SYNCBUSY

Field Documentation

__IOM uint32_t WDOG_TypeDef::CMD

Command Register

Definition at line 50 of file efm32lg_wdog.h .

Referenced by WDOGn_Feed() .

__IOM uint32_t WDOG_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32lg_wdog.h .

Referenced by WDOGn_Enable() , WDOGn_Feed() , WDOGn_Init() , and WDOGn_Lock() .

__IM uint32_t WDOG_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 52 of file efm32lg_wdog.h .

Referenced by WDOGn_Enable() , WDOGn_Feed() , WDOGn_Init() , and WDOGn_Lock() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_wdog.h