AES_TypeDef Struct ReferenceDevices > EFM32LG_AES

Definition at line 48 of file efm32lg_aes.h .

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CTRL
__IOM uint32_t DATA
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t KEYHA
__IOM uint32_t KEYHB
__IOM uint32_t KEYHC
__IOM uint32_t KEYHD
__IOM uint32_t KEYLA
__IOM uint32_t KEYLB
__IOM uint32_t KEYLC
__IOM uint32_t KEYLD
uint32_t RESERVED0 [3]
__IM uint32_t STATUS
__IOM uint32_t XORDATA

Field Documentation

__IOM uint32_t AES_TypeDef::CMD

Command Register

Definition at line 50 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::DATA

DATA Register

Definition at line 56 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::IEN

Interrupt Enable Register

Definition at line 52 of file efm32lg_aes.h .

__IM uint32_t AES_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYHA

KEY High Register

Definition at line 63 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYHB

KEY High Register

Definition at line 64 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYHC

KEY High Register

Definition at line 65 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYHD

KEY High Register

Definition at line 66 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYLA

KEY Low Register

Definition at line 59 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYLB

KEY Low Register

Definition at line 60 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYLC

KEY Low Register

Definition at line 61 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::KEYLD

KEY Low Register

Definition at line 62 of file efm32lg_aes.h .

uint32_t AES_TypeDef::RESERVED0[3]

Reserved for future use

Definition at line 58 of file efm32lg_aes.h .

__IM uint32_t AES_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32lg_aes.h .

__IOM uint32_t AES_TypeDef::XORDATA

XORDATA Register

Definition at line 57 of file efm32lg_aes.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_aes.h