LETIMER_TypeDef Struct ReferenceDevices > EFM32LG_LETIMER

Definition at line 48 of file efm32lg_letimer.h .

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CNT
__IOM uint32_t COMP0
__IOM uint32_t COMP1
__IOM uint32_t CTRL
__IOM uint32_t FREEZE
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t REP0
__IOM uint32_t REP1
uint32_t RESERVED0 [2]
__IOM uint32_t ROUTE
__IM uint32_t STATUS
__IM uint32_t SYNCBUSY

Field Documentation

__IOM uint32_t LETIMER_TypeDef::CMD

Command Register

Definition at line 50 of file efm32lg_letimer.h .

Referenced by LETIMER_Enable() , LETIMER_Init() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::CNT

Counter Value Register

Definition at line 52 of file efm32lg_letimer.h .

Referenced by LETIMER_CounterGet() .

__IOM uint32_t LETIMER_TypeDef::COMP0

Compare Value Register 0

Definition at line 53 of file efm32lg_letimer.h .

Referenced by LETIMER_CompareGet() , LETIMER_CompareSet() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::COMP1

Compare Value Register 1

Definition at line 54 of file efm32lg_letimer.h .

Referenced by LETIMER_CompareGet() , LETIMER_CompareSet() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32lg_letimer.h .

Referenced by LETIMER_Init() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::FREEZE

Freeze Register

Definition at line 62 of file efm32lg_letimer.h .

Referenced by LETIMER_FreezeEnable() .

__IOM uint32_t LETIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 60 of file efm32lg_letimer.h .

Referenced by LETIMER_IntDisable() , LETIMER_IntEnable() , LETIMER_IntGetEnabled() , and LETIMER_Reset() .

__IM uint32_t LETIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 57 of file efm32lg_letimer.h .

Referenced by LETIMER_IntGet() , and LETIMER_IntGetEnabled() .

__IOM uint32_t LETIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 59 of file efm32lg_letimer.h .

Referenced by LETIMER_IntClear() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 58 of file efm32lg_letimer.h .

Referenced by LETIMER_IntSet() .

__IOM uint32_t LETIMER_TypeDef::REP0

Repeat Counter Register 0

Definition at line 55 of file efm32lg_letimer.h .

Referenced by LETIMER_RepeatGet() , LETIMER_RepeatSet() , and LETIMER_Reset() .

__IOM uint32_t LETIMER_TypeDef::REP1

Repeat Counter Register 1

Definition at line 56 of file efm32lg_letimer.h .

Referenced by LETIMER_RepeatGet() , LETIMER_RepeatSet() , and LETIMER_Reset() .

uint32_t LETIMER_TypeDef::RESERVED0[2]

Reserved for future use

Definition at line 65 of file efm32lg_letimer.h .

__IOM uint32_t LETIMER_TypeDef::ROUTE

I/O Routing Register

Definition at line 66 of file efm32lg_letimer.h .

__IM uint32_t LETIMER_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32lg_letimer.h .

Referenced by LETIMER_Init() .

__IM uint32_t LETIMER_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 63 of file efm32lg_letimer.h .

Referenced by LETIMER_FreezeEnable() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_letimer.h