GPIO_TypeDef Struct ReferenceDevices > EFM32LG_GPIO

Definition at line 48 of file efm32lg_gpio.h .

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CTRL
__IM uint32_t EM4WUCAUSE
__IOM uint32_t EM4WUEN
__IOM uint32_t EM4WUPOL
__IOM uint32_t EXTIFALL
__IOM uint32_t EXTIPSELH
__IOM uint32_t EXTIPSELL
__IOM uint32_t EXTIRISE
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t INSENSE
__IOM uint32_t LOCK
GPIO_P_TypeDef P [6]
uint32_t RESERVED0 [10]
__IOM uint32_t ROUTE

Field Documentation

__IOM uint32_t GPIO_TypeDef::CMD

GPIO Command Register

Definition at line 65 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::CTRL

GPIO Control Register

Definition at line 64 of file efm32lg_gpio.h .

__IM uint32_t GPIO_TypeDef::EM4WUCAUSE

EM4 Wake-up Cause Register

Definition at line 68 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::EM4WUEN

EM4 Wake-up Enable Register

Definition at line 66 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::EM4WUPOL

EM4 Wake-up Polarity Register

Definition at line 67 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::EXTIFALL

External Interrupt Falling Edge Trigger Register

Definition at line 55 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::EXTIPSELH

External Interrupt Port Select High Register

Definition at line 53 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::EXTIPSELL

External Interrupt Port Select Low Register

Definition at line 52 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::EXTIRISE

External Interrupt Rising Edge Trigger Register

Definition at line 54 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::IEN

Interrupt Enable Register

Definition at line 56 of file efm32lg_gpio.h .

__IM uint32_t GPIO_TypeDef::IF

Interrupt Flag Register

Definition at line 57 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 59 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 58 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::INSENSE

Input Sense Register

Definition at line 62 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::LOCK

Configuration Lock Register

Definition at line 63 of file efm32lg_gpio.h .

GPIO_P_TypeDef GPIO_TypeDef::P[6]

Port configuration bits

Definition at line 49 of file efm32lg_gpio.h .

uint32_t GPIO_TypeDef::RESERVED0[10]

Reserved for future use

Definition at line 51 of file efm32lg_gpio.h .

__IOM uint32_t GPIO_TypeDef::ROUTE

I/O Routing Register

Definition at line 61 of file efm32lg_gpio.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_gpio.h