USB_DOEP_TypeDef Struct ReferenceDevices

USB_DOEP EFM32LG USB DOEP.

Definition at line 46 of file efm32lg_usb_doep.h .

#include < efm32lg_usb_doep.h >

Data Fields

__IOM uint32_t CTL
__IOM uint32_t DMAADDR
__IOM uint32_t INT
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [1]
uint32_t RESERVED2 [2]
__IOM uint32_t TSIZ

Field Documentation

__IOM uint32_t USB_DOEP_TypeDef::CTL

Device OUT Endpoint x+1 Control Register

Definition at line 47 of file efm32lg_usb_doep.h .

__IOM uint32_t USB_DOEP_TypeDef::DMAADDR

Device OUT Endpoint x+1 DMA Address Register

Definition at line 52 of file efm32lg_usb_doep.h .

__IOM uint32_t USB_DOEP_TypeDef::INT

Device OUT Endpoint x+1 Interrupt Register

Definition at line 49 of file efm32lg_usb_doep.h .

uint32_t USB_DOEP_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 48 of file efm32lg_usb_doep.h .

uint32_t USB_DOEP_TypeDef::RESERVED1[1]

Reserved for future use

Definition at line 50 of file efm32lg_usb_doep.h .

uint32_t USB_DOEP_TypeDef::RESERVED2[2]

Reserved future

Definition at line 53 of file efm32lg_usb_doep.h .

__IOM uint32_t USB_DOEP_TypeDef::TSIZ

Device OUT Endpoint x+1 Transfer Size Register

Definition at line 51 of file efm32lg_usb_doep.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_usb_doep.h