USART_TypeDef Struct ReferenceDevices > EFM32LG_USART
Definition at line 48
of file efm32lg_usart.h
.
Data Fields | |
__IOM uint32_t | CLKDIV |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | FRAME |
__IOM uint32_t | I2SCTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INPUT |
__IOM uint32_t | IRCTRL |
__IOM uint32_t | ROUTE |
__IM uint32_t | RXDATA |
__IM uint32_t | RXDATAX |
__IM uint32_t | RXDATAXP |
__IM uint32_t | RXDOUBLE |
__IM uint32_t | RXDOUBLEX |
__IM uint32_t | RXDOUBLEXP |
__IM uint32_t | STATUS |
__IOM uint32_t | TRIGCTRL |
__IOM uint32_t | TXDATA |
__IOM uint32_t | TXDATAX |
__IOM uint32_t | TXDOUBLE |
__IOM uint32_t | TXDOUBLEX |
Field Documentation
__IOM uint32_t USART_TypeDef::CLKDIV |
Clock Control Register
Definition at line 54
of file efm32lg_usart.h
.
Referenced by USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_BaudrateSyncSet(), and USART_Reset().
__IOM uint32_t USART_TypeDef::CMD |
Command Register
Definition at line 52
of file efm32lg_usart.h
.
Referenced by UARTDRV_InitUart(), USART_Enable(), USART_InitAsync(), USART_InitSync(), and USART_Reset().
__IOM uint32_t USART_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32lg_usart.h
.
Referenced by SPIDRV_Init(), USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_InitAsync(), USART_InitSync(), USART_Reset(), and USARTn_InitIrDA().
__IOM uint32_t USART_TypeDef::FRAME |
USART Frame Format Register
Definition at line 50
of file efm32lg_usart.h
.
Referenced by USART_InitAsync(), USART_InitSync(), and USART_Reset().
__IOM uint32_t USART_TypeDef::I2SCTRL |
I2S Control Register
Definition at line 72
of file efm32lg_usart.h
.
Referenced by USART_InitI2s(), and USART_Reset().
__IOM uint32_t USART_TypeDef::IEN |
Interrupt Enable Register
Definition at line 68
of file efm32lg_usart.h
.
Referenced by USART_IntDisable(), USART_IntEnable(), USART_IntGetEnabled(), and USART_Reset().
__IM uint32_t USART_TypeDef::IF |
Interrupt Flag Register
Definition at line 65
of file efm32lg_usart.h
.
Referenced by USART_IntGet(), and USART_IntGetEnabled().
__IOM uint32_t USART_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 67
of file efm32lg_usart.h
.
Referenced by USART_IntClear(), and USART_Reset().
__IOM uint32_t USART_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 66
of file efm32lg_usart.h
.
Referenced by USART_IntSet().
__IOM uint32_t USART_TypeDef::INPUT |
USART Input Register
Definition at line 71
of file efm32lg_usart.h
.
Referenced by USART_InitAsync(), USART_InitSync(), and USART_Reset().
__IOM uint32_t USART_TypeDef::IRCTRL |
IrDA Control Register
Definition at line 69
of file efm32lg_usart.h
.
Referenced by USART_Reset(), and USARTn_InitIrDA().
__IOM uint32_t USART_TypeDef::ROUTE |
I/O Routing Register
Definition at line 70
of file efm32lg_usart.h
.
Referenced by RETARGET_SerialInit(), SPIDRV_Init(), UARTDRV_InitUart(), and USART_Reset().
__IM uint32_t USART_TypeDef::RXDATA |
RX Buffer Data Register
Definition at line 56
of file efm32lg_usart.h
.
Referenced by USART_Rx(), USART_RxDataGet(), and USART_SpiTransfer().
__IM uint32_t USART_TypeDef::RXDATAX |
RX Buffer Data Extended Register
Definition at line 55
of file efm32lg_usart.h
.
Referenced by USART_RxDataXGet(), and USART_RxExt().
__IM uint32_t USART_TypeDef::RXDATAXP |
RX Buffer Data Extended Peek Register
Definition at line 59
of file efm32lg_usart.h
.
__IM uint32_t USART_TypeDef::RXDOUBLE |
RX FIFO Double Data Register
Definition at line 58
of file efm32lg_usart.h
.
Referenced by USART_RxDouble(), and USART_RxDoubleGet().
__IM uint32_t USART_TypeDef::RXDOUBLEX |
RX Buffer Double Data Extended Register
Definition at line 57
of file efm32lg_usart.h
.
Referenced by USART_RxDoubleExt(), and USART_RxDoubleXGet().
__IM uint32_t USART_TypeDef::RXDOUBLEXP |
RX Buffer Double Data Extended Peek Register
Definition at line 60
of file efm32lg_usart.h
.
__IM uint32_t USART_TypeDef::STATUS |
USART Status Register
Definition at line 53
of file efm32lg_usart.h
.
Referenced by USART_Rx(), USART_RxDouble(), USART_RxDoubleExt(), USART_RxExt(), USART_SpiTransfer(), USART_StatusGet(), USART_Tx(), USART_TxDouble(), USART_TxDoubleExt(), and USART_TxExt().
__IOM uint32_t USART_TypeDef::TRIGCTRL |
USART Trigger Control register
Definition at line 51
of file efm32lg_usart.h
.
Referenced by USART_InitPrsTrigger(), and USART_Reset().
__IOM uint32_t USART_TypeDef::TXDATA |
TX Buffer Data Register
Definition at line 62
of file efm32lg_usart.h
.
Referenced by USART_SpiTransfer(), and USART_Tx().
__IOM uint32_t USART_TypeDef::TXDATAX |
TX Buffer Data Extended Register
Definition at line 61
of file efm32lg_usart.h
.
Referenced by USART_TxExt().
__IOM uint32_t USART_TypeDef::TXDOUBLE |
TX Buffer Double Data Register
Definition at line 64
of file efm32lg_usart.h
.
Referenced by USART_TxDouble().
__IOM uint32_t USART_TypeDef::TXDOUBLEX |
TX Buffer Double Data Extended Register
Definition at line 63
of file efm32lg_usart.h
.
Referenced by USART_TxDoubleExt().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/
efm32lg_usart.h