DMA_DESCRIPTOR_TypeDef Struct ReferenceDevices > EFM32LG_DMA_DESCRIPTOR
Definition at line 47
of file efm32lg_dma_descriptor.h
.
Data Fields | |
__IOM uint32_t | CTRL |
__IOM void *__IOM | DSTEND |
__IOM void *__IOM | SRCEND |
__IOM uint32_t | USER |
Field Documentation
__IOM uint32_t DMA_DESCRIPTOR_TypeDef::CTRL |
DMA control register
Definition at line 52
of file efm32lg_dma_descriptor.h
.
Referenced by DMA_ActivateScatterGather(), DMA_CfgDescr(), DMA_CfgDescrScatterGather(), and DMA_RefreshPingPong().
__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::DSTEND |
DMA destination address end
Definition at line 51
of file efm32lg_dma_descriptor.h
.
Referenced by DMA_ActivateScatterGather(), DMA_CfgDescrScatterGather(), and DMA_RefreshPingPong().
__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::SRCEND |
DMA source address end
Definition at line 50
of file efm32lg_dma_descriptor.h
.
Referenced by DMA_ActivateScatterGather(), DMA_CfgDescrScatterGather(), and DMA_RefreshPingPong().
__IOM uint32_t DMA_DESCRIPTOR_TypeDef::USER |
DMA padding register, available for user
Definition at line 53
of file efm32lg_dma_descriptor.h
.
Referenced by DMA_ActivateScatterGather(), DMA_CfgChannel(), and DMA_CfgDescrScatterGather().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/
efm32lg_dma_descriptor.h