ADC_InitScanInput_TypeDef Struct ReferenceEMLIB > ADC

Scan input configuration

Definition at line 850 of file em_adc.h.

#include <em_adc.h>

Data Fields

uint32_t scanInputEn
 
uint32_t scanInputSel
 
uint32_t scanNegSel
 

Field Documentation

uint32_t ADC_InitScanInput_TypeDef::scanInputEn

Input enable mask

Definition at line 855 of file em_adc.h.

uint32_t ADC_InitScanInput_TypeDef::scanInputSel

Input range select to be applied to ADC_SCANINPUTSEL.

Definition at line 852 of file em_adc.h.

uint32_t ADC_InitScanInput_TypeDef::scanNegSel

Alternative negative input

Definition at line 858 of file em_adc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_adc.h