IDACEMLIB
Detailed Description
Current Digital-to-Analog Converter (IDAC) Peripheral API.
The current digital-to-analog converter (IDAC) can source or sink a configurable constant current, which can be output on, or sinked from pin or ADC. The current is configurable with several ranges of various step sizes. The IDAC can be used with PRS and it can operate down to EM3.
The following steps are necessary for basic operation:
Clock enable:
Initialize the peripheral with default settings and modify selected fields such as output select:
Set output:
Data Structures |
|
struct | IDAC_Init_TypeDef |
Macros |
|
#define | IDAC_INIT_DEFAULT |
Enumerations |
|
enum |
IDAC_OutMode_TypeDef
{
idacOutputAPORT1XCH0 = IDAC_CTRL_APORTOUTSEL_APORT1XCH0, idacOutputAPORT1YCH1 = IDAC_CTRL_APORTOUTSEL_APORT1YCH1, idacOutputAPORT1XCH2 = IDAC_CTRL_APORTOUTSEL_APORT1XCH2, idacOutputAPORT1YCH3 = IDAC_CTRL_APORTOUTSEL_APORT1YCH3, idacOutputAPORT1XCH4 = IDAC_CTRL_APORTOUTSEL_APORT1XCH4, idacOutputAPORT1YCH5 = IDAC_CTRL_APORTOUTSEL_APORT1YCH5, idacOutputAPORT1XCH6 = IDAC_CTRL_APORTOUTSEL_APORT1XCH6, idacOutputAPORT1YCH7 = IDAC_CTRL_APORTOUTSEL_APORT1YCH7, idacOutputAPORT1XCH8 = IDAC_CTRL_APORTOUTSEL_APORT1XCH8, idacOutputAPORT1YCH9 = IDAC_CTRL_APORTOUTSEL_APORT1YCH9, idacOutputAPORT1XCH10 = IDAC_CTRL_APORTOUTSEL_APORT1XCH10, idacOutputAPORT1YCH11 = IDAC_CTRL_APORTOUTSEL_APORT1YCH11, idacOutputAPORT1XCH12 = IDAC_CTRL_APORTOUTSEL_APORT1XCH12, idacOutputAPORT1YCH13 = IDAC_CTRL_APORTOUTSEL_APORT1YCH13, idacOutputAPORT1XCH14 = IDAC_CTRL_APORTOUTSEL_APORT1XCH14, idacOutputAPORT1YCH15 = IDAC_CTRL_APORTOUTSEL_APORT1YCH15, idacOutputAPORT1XCH16 = IDAC_CTRL_APORTOUTSEL_APORT1XCH16, idacOutputAPORT1YCH17 = IDAC_CTRL_APORTOUTSEL_APORT1YCH17, idacOutputAPORT1XCH18 = IDAC_CTRL_APORTOUTSEL_APORT1XCH18, idacOutputAPORT1YCH19 = IDAC_CTRL_APORTOUTSEL_APORT1YCH19, idacOutputAPORT1XCH20 = IDAC_CTRL_APORTOUTSEL_APORT1XCH20, idacOutputAPORT1YCH21 = IDAC_CTRL_APORTOUTSEL_APORT1YCH21, idacOutputAPORT1XCH22 = IDAC_CTRL_APORTOUTSEL_APORT1XCH22, idacOutputAPORT1YCH23 = IDAC_CTRL_APORTOUTSEL_APORT1YCH23, idacOutputAPORT1XCH24 = IDAC_CTRL_APORTOUTSEL_APORT1XCH24, idacOutputAPORT1YCH25 = IDAC_CTRL_APORTOUTSEL_APORT1YCH25, idacOutputAPORT1XCH26 = IDAC_CTRL_APORTOUTSEL_APORT1XCH26, idacOutputAPORT1YCH27 = IDAC_CTRL_APORTOUTSEL_APORT1YCH27, idacOutputAPORT1XCH28 = IDAC_CTRL_APORTOUTSEL_APORT1XCH28, idacOutputAPORT1YCH29 = IDAC_CTRL_APORTOUTSEL_APORT1YCH29, idacOutputAPORT1XCH30 = IDAC_CTRL_APORTOUTSEL_APORT1XCH30, idacOutputAPORT1YCH31 = IDAC_CTRL_APORTOUTSEL_APORT1YCH31 } |
enum |
IDAC_PRSSEL_TypeDef
{
idacPRSSELCh0 = IDAC_CTRL_PRSSEL_PRSCH0, idacPRSSELCh1 = IDAC_CTRL_PRSSEL_PRSCH1, idacPRSSELCh2 = IDAC_CTRL_PRSSEL_PRSCH2, idacPRSSELCh3 = IDAC_CTRL_PRSSEL_PRSCH3, idacPRSSELCh4 = IDAC_CTRL_PRSSEL_PRSCH4, idacPRSSELCh5 = IDAC_CTRL_PRSSEL_PRSCH5, idacPRSSELCh6 = IDAC_CTRL_PRSSEL_PRSCH6, idacPRSSELCh7 = IDAC_CTRL_PRSSEL_PRSCH7, idacPRSSELCh8 = IDAC_CTRL_PRSSEL_PRSCH8, idacPRSSELCh9 = IDAC_CTRL_PRSSEL_PRSCH9, idacPRSSELCh10 = IDAC_CTRL_PRSSEL_PRSCH10, idacPRSSELCh11 = IDAC_CTRL_PRSSEL_PRSCH11 } |
enum |
IDAC_Range_TypeDef
{
idacCurrentRange0 = IDAC_CURPROG_RANGESEL_RANGE0, idacCurrentRange1 = IDAC_CURPROG_RANGESEL_RANGE1, idacCurrentRange2 = IDAC_CURPROG_RANGESEL_RANGE2, idacCurrentRange3 = IDAC_CURPROG_RANGESEL_RANGE3 } |
Functions |
|
void | IDAC_Enable ( IDAC_TypeDef *idac, bool enable) |
Enable/disable IDAC.
|
|
void | IDAC_Init ( IDAC_TypeDef *idac, const IDAC_Init_TypeDef *init) |
Initialize IDAC.
|
|
__STATIC_INLINE void | IDAC_IntClear ( IDAC_TypeDef *idac, uint32_t flags) |
Clear one or more pending IDAC interrupts.
|
|
__STATIC_INLINE void | IDAC_IntDisable ( IDAC_TypeDef *idac, uint32_t flags) |
Disable one or more IDAC interrupts.
|
|
__STATIC_INLINE void | IDAC_IntEnable ( IDAC_TypeDef *idac, uint32_t flags) |
Enable one or more IDAC interrupts.
|
|
__STATIC_INLINE uint32_t | IDAC_IntGet ( IDAC_TypeDef *idac) |
Get pending IDAC interrupt flags.
|
|
__STATIC_INLINE uint32_t | IDAC_IntGetEnabled ( IDAC_TypeDef *idac) |
Get enabled and pending IDAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
__STATIC_INLINE void | IDAC_IntSet ( IDAC_TypeDef *idac, uint32_t flags) |
Set one or more pending IDAC interrupts from SW.
|
|
void | IDAC_MinimalOutputTransitionMode ( IDAC_TypeDef *idac, bool enable) |
Enable/disable Minimal Output Transition mode.
|
|
void | IDAC_OutEnable ( IDAC_TypeDef *idac, bool enable) |
Enable/disable the IDAC OUT pin.
|
|
void | IDAC_RangeSet ( IDAC_TypeDef *idac, const IDAC_Range_TypeDef range) |
Set the current range of the IDAC output.
|
|
void | IDAC_Reset ( IDAC_TypeDef *idac) |
Reset IDAC to same state as after a HW reset.
|
|
void | IDAC_StepSet ( IDAC_TypeDef *idac, const uint32_t step) |
Set the current step of the IDAC output.
|
|
Macro Definition Documentation
#define IDAC_INIT_DEFAULT |
Default config for IDAC init structure.
Definition at line
202
of file
em_idac.h
.
Enumeration Type Documentation
enum IDAC_OutMode_TypeDef |
Output mode.
Definition at line
93
of file
em_idac.h
.
enum IDAC_PRSSEL_TypeDef |
Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control the IDAC output.
Definition at line
135
of file
em_idac.h
.
enum IDAC_Range_TypeDef |
Function Documentation
void IDAC_Enable | ( | IDAC_TypeDef * |
idac,
|
bool |
enable
|
||
) |
Enable/disable IDAC.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] enable
true to enable IDAC, false to disable.
Definition at line
115
of file
em_idac.c
.
References _IDAC_CTRL_EN_SHIFT , BUS_RegBitWrite() , and IDAC_TypeDef::CTRL .
void IDAC_Init | ( | IDAC_TypeDef * |
idac,
|
const IDAC_Init_TypeDef * |
init
|
||
) |
Initialize IDAC.
Initializes IDAC according to the initialization structure parameter, and sets the default calibration value stored in the DEVINFO structure.
- Note
- This function will disable the IDAC prior to configuration.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] init
Pointer to IDAC initialization structure.
Definition at line
78
of file
em_idac.c
.
References IDAC_TypeDef::CTRL , IDAC_Init_TypeDef::enable , IDAC_CTRL_APORTOUTENPRS , IDAC_CTRL_CURSINK , IDAC_CTRL_EN , IDAC_Init_TypeDef::outMode , IDAC_Init_TypeDef::prsEnable , IDAC_Init_TypeDef::prsSel , and IDAC_Init_TypeDef::sinkEnable .
__STATIC_INLINE void IDAC_IntClear | ( | IDAC_TypeDef * |
idac,
|
uint32_t |
flags
|
||
) |
Clear one or more pending IDAC interrupts.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] flags
Pending IDAC interrupt source(s) to clear. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
236
of file
em_idac.h
.
References IDAC_TypeDef::IFC .
__STATIC_INLINE void IDAC_IntDisable | ( | IDAC_TypeDef * |
idac,
|
uint32_t |
flags
|
||
) |
Disable one or more IDAC interrupts.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] flags
IDAC interrupt source(s) to disable. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
252
of file
em_idac.h
.
References IDAC_TypeDef::IEN .
__STATIC_INLINE void IDAC_IntEnable | ( | IDAC_TypeDef * |
idac,
|
uint32_t |
flags
|
||
) |
Enable one or more IDAC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using IDAC_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] flags
IDAC interrupt source(s) to enable. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
273
of file
em_idac.h
.
References IDAC_TypeDef::IEN .
__STATIC_INLINE uint32_t IDAC_IntGet | ( | IDAC_TypeDef * |
idac
|
) |
Get pending IDAC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block.
- Returns
- IDAC interrupt source(s) pending. Returns one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
292
of file
em_idac.h
.
References IDAC_TypeDef::IF .
__STATIC_INLINE uint32_t IDAC_IntGetEnabled | ( | IDAC_TypeDef * |
idac
|
) |
Get enabled and pending IDAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled IDAC interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in IDACx_IEN_nnn register (IDACx_IEN_nnn) and
- the OR combination of valid interrupt flags of the IDAC module (IDACx_IF_nnn).
Definition at line
316
of file
em_idac.h
.
References IDAC_TypeDef::IEN , and IDAC_TypeDef::IF .
__STATIC_INLINE void IDAC_IntSet | ( | IDAC_TypeDef * |
idac,
|
uint32_t |
flags
|
||
) |
Set one or more pending IDAC interrupts from SW.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] flags
IDAC interrupt source(s) to set to pending. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.
Definition at line
339
of file
em_idac.h
.
References IDAC_TypeDef::IFS .
void IDAC_MinimalOutputTransitionMode | ( | IDAC_TypeDef * |
idac,
|
bool |
enable
|
||
) |
Enable/disable Minimal Output Transition mode.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] enable
true to enable Minimal Output Transition mode, false to disable.
Definition at line
166
of file
em_idac.c
.
References _IDAC_CTRL_MINOUTTRANS_SHIFT , BUS_RegBitWrite() , and IDAC_TypeDef::CTRL .
void IDAC_OutEnable | ( | IDAC_TypeDef * |
idac,
|
bool |
enable
|
||
) |
Enable/disable the IDAC OUT pin.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] enable
true to enable the IDAC OUT pin, false to disable.
Definition at line
331
of file
em_idac.c
.
References _IDAC_CTRL_APORTOUTEN_SHIFT , BUS_RegBitWrite() , and IDAC_TypeDef::CTRL .
void IDAC_RangeSet | ( | IDAC_TypeDef * |
idac,
|
const IDAC_Range_TypeDef |
range
|
||
) |
Set the current range of the IDAC output.
This function sets the current range of the IDAC output. The function also updates the IDAC calibration register (IDAC_CAL) with the default calibration value from DEVINFO (factory calibration) corresponding to the specified range.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] range
Current range value.
Definition at line
188
of file
em_idac.c
.
References _DEVINFO_IDAC0CAL0_SOURCERANGE0TUNING_MASK , _DEVINFO_IDAC0CAL0_SOURCERANGE0TUNING_SHIFT , _DEVINFO_IDAC0CAL0_SOURCERANGE1TUNING_MASK , _DEVINFO_IDAC0CAL0_SOURCERANGE1TUNING_SHIFT , _DEVINFO_IDAC0CAL0_SOURCERANGE2TUNING_MASK , _DEVINFO_IDAC0CAL0_SOURCERANGE2TUNING_SHIFT , _DEVINFO_IDAC0CAL0_SOURCERANGE3TUNING_MASK , _DEVINFO_IDAC0CAL0_SOURCERANGE3TUNING_SHIFT , _DEVINFO_IDAC0CAL1_SINKRANGE0TUNING_MASK , _DEVINFO_IDAC0CAL1_SINKRANGE0TUNING_SHIFT , _DEVINFO_IDAC0CAL1_SINKRANGE1TUNING_MASK , _DEVINFO_IDAC0CAL1_SINKRANGE1TUNING_SHIFT , _DEVINFO_IDAC0CAL1_SINKRANGE2TUNING_MASK , _DEVINFO_IDAC0CAL1_SINKRANGE2TUNING_SHIFT , _DEVINFO_IDAC0CAL1_SINKRANGE3TUNING_MASK , _DEVINFO_IDAC0CAL1_SINKRANGE3TUNING_SHIFT , _IDAC_CURPROG_RANGESEL_MASK , _IDAC_CURPROG_RANGESEL_SHIFT , _IDAC_CURPROG_TUNING_MASK , _IDAC_CURPROG_TUNING_SHIFT , IDAC_TypeDef::CTRL , IDAC_TypeDef::CURPROG , DEVINFO , IDAC0 , IDAC_CTRL_CURSINK , idacCurrentRange0 , idacCurrentRange1 , idacCurrentRange2 , and idacCurrentRange3 .
void IDAC_Reset | ( | IDAC_TypeDef * |
idac
|
) |
Reset IDAC to same state as after a HW reset.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block.
Definition at line
128
of file
em_idac.c
.
References _IDAC_CTRL_RESETVALUE , _IDAC_CURPROG_RESETVALUE , _IDAC_CURPROG_STEPSEL_SHIFT , _IDAC_DUTYCONFIG_RESETVALUE , IDAC_TypeDef::CTRL , IDAC_TypeDef::CURPROG , IDAC_TypeDef::DUTYCONFIG , IDAC_CTRL_EN , and IDAC_CURPROG_RANGESEL_RANGE0 .
void IDAC_StepSet | ( | IDAC_TypeDef * |
idac,
|
const uint32_t |
step
|
||
) |
Set the current step of the IDAC output.
- Parameters
-
[in] idac
Pointer to IDAC peripheral register block. [in] step
Step value for IDAC output. Valid range is 0-31.
Definition at line
308
of file
em_idac.c
.
References _IDAC_CURPROG_STEPSEL_MASK , _IDAC_CURPROG_STEPSEL_SHIFT , and IDAC_TypeDef::CURPROG .