TIMEREMLIB

Detailed Description

Timer/Counter (TIMER) Peripheral API.

The timer module consists of three main parts:

  • General timer config and enable control.
  • Compare/capture control.
  • Dead time insertion control (may not be available for all timers).

Data Structures

struct TIMER_Init_TypeDef
struct TIMER_InitCC_TypeDef
struct TIMER_InitDTI_TypeDef

Macros

#define TIMER_INIT_DEFAULT
#define TIMER_INITCC_DEFAULT
#define TIMER_INITDTI_DEFAULT

Enumerations

enum TIMER_CCMode_TypeDef {
timerCCModeOff = _TIMER_CC_CTRL_MODE_OFF,
timerCCModeCapture = _TIMER_CC_CTRL_MODE_INPUTCAPTURE,
timerCCModeCompare = _TIMER_CC_CTRL_MODE_OUTPUTCOMPARE,
timerCCModePWM = _TIMER_CC_CTRL_MODE_PWM
}
enum TIMER_ClkSel_TypeDef {
timerClkSelHFPerClk = _TIMER_CTRL_CLKSEL_PRESCHFPERCLK,
timerClkSelCC1 = _TIMER_CTRL_CLKSEL_CC1,
timerClkSelCascade = _TIMER_CTRL_CLKSEL_TIMEROUF
}
enum TIMER_DtiFaultAction_TypeDef {
timerDtiFaultActionNone = _TIMER_DTFC_DTFA_NONE,
timerDtiFaultActionInactive = _TIMER_DTFC_DTFA_INACTIVE,
timerDtiFaultActionClear = _TIMER_DTFC_DTFA_CLEAR,
timerDtiFaultActionTristate = _TIMER_DTFC_DTFA_TRISTATE
}
enum TIMER_Edge_TypeDef {
timerEdgeRising = _TIMER_CC_CTRL_ICEDGE_RISING,
timerEdgeFalling = _TIMER_CC_CTRL_ICEDGE_FALLING,
timerEdgeBoth = _TIMER_CC_CTRL_ICEDGE_BOTH,
timerEdgeNone = _TIMER_CC_CTRL_ICEDGE_NONE
}
enum TIMER_Event_TypeDef {
timerEventEveryEdge = _TIMER_CC_CTRL_ICEVCTRL_EVERYEDGE,
timerEventEvery2ndEdge = _TIMER_CC_CTRL_ICEVCTRL_EVERYSECONDEDGE,
timerEventRising = _TIMER_CC_CTRL_ICEVCTRL_RISING,
timerEventFalling = _TIMER_CC_CTRL_ICEVCTRL_FALLING
}
enum TIMER_InputAction_TypeDef {
timerInputActionNone = _TIMER_CTRL_FALLA_NONE,
timerInputActionStart = _TIMER_CTRL_FALLA_START,
timerInputActionStop = _TIMER_CTRL_FALLA_STOP,
timerInputActionReloadStart = _TIMER_CTRL_FALLA_RELOADSTART
}
enum TIMER_Mode_TypeDef {
timerModeUp = _TIMER_CTRL_MODE_UP,
timerModeDown = _TIMER_CTRL_MODE_DOWN,
timerModeUpDown = _TIMER_CTRL_MODE_UPDOWN,
timerModeQDec = _TIMER_CTRL_MODE_QDEC
}
enum TIMER_OutputAction_TypeDef {
timerOutputActionNone = _TIMER_CC_CTRL_CUFOA_NONE,
timerOutputActionToggle = _TIMER_CC_CTRL_CUFOA_TOGGLE,
timerOutputActionClear = _TIMER_CC_CTRL_CUFOA_CLEAR,
timerOutputActionSet = _TIMER_CC_CTRL_CUFOA_SET
}
enum TIMER_Prescale_TypeDef {
timerPrescale1 = _TIMER_CTRL_PRESC_DIV1,
timerPrescale2 = _TIMER_CTRL_PRESC_DIV2,
timerPrescale4 = _TIMER_CTRL_PRESC_DIV4,
timerPrescale8 = _TIMER_CTRL_PRESC_DIV8,
timerPrescale16 = _TIMER_CTRL_PRESC_DIV16,
timerPrescale32 = _TIMER_CTRL_PRESC_DIV32,
timerPrescale64 = _TIMER_CTRL_PRESC_DIV64,
timerPrescale128 = _TIMER_CTRL_PRESC_DIV128,
timerPrescale256 = _TIMER_CTRL_PRESC_DIV256,
timerPrescale512 = _TIMER_CTRL_PRESC_DIV512,
timerPrescale1024 = _TIMER_CTRL_PRESC_DIV1024
}
enum TIMER_PRSSEL_TypeDef {
timerPRSSELCh0 = _TIMER_CC_CTRL_PRSSEL_PRSCH0,
timerPRSSELCh1 = _TIMER_CC_CTRL_PRSSEL_PRSCH1,
timerPRSSELCh2 = _TIMER_CC_CTRL_PRSSEL_PRSCH2,
timerPRSSELCh3 = _TIMER_CC_CTRL_PRSSEL_PRSCH3,
timerPRSSELCh4 = _TIMER_CC_CTRL_PRSSEL_PRSCH4,
timerPRSSELCh5 = _TIMER_CC_CTRL_PRSSEL_PRSCH5,
timerPRSSELCh6 = _TIMER_CC_CTRL_PRSSEL_PRSCH6,
timerPRSSELCh7 = _TIMER_CC_CTRL_PRSSEL_PRSCH7,
timerPRSSELCh8 = _TIMER_CC_CTRL_PRSSEL_PRSCH8,
timerPRSSELCh9 = _TIMER_CC_CTRL_PRSSEL_PRSCH9,
timerPRSSELCh10 = _TIMER_CC_CTRL_PRSSEL_PRSCH10,
timerPRSSELCh11 = _TIMER_CC_CTRL_PRSSEL_PRSCH11
}

Functions

__STATIC_INLINE uint32_t TIMER_CaptureGet ( TIMER_TypeDef *timer, unsigned int ch)
Get capture value for compare/capture channel when operating in capture mode.
__STATIC_INLINE void TIMER_ClearDTIFault ( TIMER_TypeDef *timer, uint32_t flags)
Clear DTI fault source flags.
__STATIC_INLINE void TIMER_CompareBufSet ( TIMER_TypeDef *timer, unsigned int ch, uint32_t val)
Set compare value buffer for compare/capture channel when operating in compare or PWM mode.
__STATIC_INLINE void TIMER_CompareSet ( TIMER_TypeDef *timer, unsigned int ch, uint32_t val)
Set compare value for compare/capture channel when operating in compare or PWM mode.
__STATIC_INLINE uint32_t TIMER_CounterGet ( TIMER_TypeDef *timer)
Get TIMER counter value.
__STATIC_INLINE void TIMER_CounterSet ( TIMER_TypeDef *timer, uint32_t val)
Set TIMER counter value.
__STATIC_INLINE void TIMER_Enable ( TIMER_TypeDef *timer, bool enable)
Start/stop TIMER.
__STATIC_INLINE void TIMER_EnableDTI ( TIMER_TypeDef *timer, bool enable)
Enable or disable DTI unit.
__STATIC_INLINE uint32_t TIMER_GetDTIFault ( TIMER_TypeDef *timer)
Get DTI fault source flags status.
void TIMER_Init ( TIMER_TypeDef *timer, const TIMER_Init_TypeDef *init)
Initialize TIMER.
void TIMER_InitCC ( TIMER_TypeDef *timer, unsigned int ch, const TIMER_InitCC_TypeDef *init)
Initialize TIMER compare/capture channel.
void TIMER_InitDTI ( TIMER_TypeDef *timer, const TIMER_InitDTI_TypeDef *init)
Initialize the TIMER DTI unit.
__STATIC_INLINE void TIMER_IntClear ( TIMER_TypeDef *timer, uint32_t flags)
Clear one or more pending TIMER interrupts.
__STATIC_INLINE void TIMER_IntDisable ( TIMER_TypeDef *timer, uint32_t flags)
Disable one or more TIMER interrupts.
__STATIC_INLINE void TIMER_IntEnable ( TIMER_TypeDef *timer, uint32_t flags)
Enable one or more TIMER interrupts.
__STATIC_INLINE uint32_t TIMER_IntGet ( TIMER_TypeDef *timer)
Get pending TIMER interrupt flags.
__STATIC_INLINE uint32_t TIMER_IntGetEnabled ( TIMER_TypeDef *timer)
Get enabled and pending TIMER interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
__STATIC_INLINE void TIMER_IntSet ( TIMER_TypeDef *timer, uint32_t flags)
Set one or more pending TIMER interrupts from SW.
__STATIC_INLINE void TIMER_Lock ( TIMER_TypeDef *timer)
Lock some of the TIMER registers in order to protect them from being modified.
__STATIC_INLINE uint32_t TIMER_MaxCount (const TIMER_TypeDef *ref)
Get the Max count of the timer.
void TIMER_Reset ( TIMER_TypeDef *timer)
Reset TIMER to same state as after a HW reset.
__STATIC_INLINE void TIMER_TopBufSet ( TIMER_TypeDef *timer, uint32_t val)
Set top value buffer for timer.
__STATIC_INLINE uint32_t TIMER_TopGet ( TIMER_TypeDef *timer)
Get top value setting for timer.
__STATIC_INLINE void TIMER_TopSet ( TIMER_TypeDef *timer, uint32_t val)
Set top value for timer.
__STATIC_INLINE void TIMER_Unlock ( TIMER_TypeDef *timer)
Unlock the TIMER so that writing to locked registers again is possible.
__STATIC_INLINE bool TIMER_Valid (const TIMER_TypeDef *ref)
Validate the TIMER register block pointer.

Macro Definition Documentation

#define TIMER_INIT_DEFAULT
Value:
{ \
true, /* Enable timer when init complete. */ \
false, /* Stop counter during debug halt. */ \
timerPrescale1, /* No prescaling. */ \
timerClkSelHFPerClk, /* Select HFPER clock. */ \
false, /* Not 2x count mode. */ \
false, /* No ATI. */ \
timerInputActionNone, /* No action on falling input edge. */ \
timerInputActionNone, /* No action on rising input edge. */ \
timerModeUp, /* Up-counting. */ \
false, /* Do not clear DMA requests when DMA channel is active. */ \
false, /* Select X2 quadrature decode mode (if used). */ \
false, /* Disable one shot. */ \
false /* Not started/stopped/reloaded by other timers. */ \
}

Default config for TIMER init structure.

Definition at line 282 of file em_timer.h .

Referenced by BOARD_init() , and USTIMER_Init() .

#define TIMER_INITCC_DEFAULT
Value:
{ \
timerEventEveryEdge, /* Event on every capture. */ \
timerEdgeRising, /* Input capture edge on rising edge. */ \
timerPRSSELCh0, /* Not used by default, select PRS channel 0. */ \
timerOutputActionNone, /* No action on underflow. */ \
timerOutputActionNone, /* No action on overflow. */ \
timerOutputActionNone, /* No action on match. */ \
timerCCModeOff, /* Disable compare/capture channel. */ \
false, /* Disable filter. */ \
false, /* Select TIMERnCCx input. */ \
false, /* Clear output when counter disabled. */ \
false /* Do not invert output. */ \
}

Default config for TIMER compare/capture init structure.

Definition at line 361 of file em_timer.h .

Referenced by BOARD_init() , and USTIMER_Init() .

#define TIMER_INITDTI_DEFAULT
Value:
{ \
true, /* Enable the DTI. */ \
false, /* CC[0|1|2] outputs are active high. */ \
false, /* CDTI[0|1|2] outputs are not inverted. */ \
false, /* No auto restart when debugger exits. */ \
false, /* No PRS source selected. */ \
timerPRSSELCh0, /* Not used by default, select PRS channel 0. */ \
timerPrescale1, /* No prescaling. */ \
0, /* No rise time. */ \
0, /* No fall time. */ \
TIMER_DTOGEN_DTOGCC0EN | TIMER_DTOGEN_DTOGCDTI0EN , /* Enable CC0 and CDTI0 */ \
true, /* Enable core lockup as fault source */ \
true, /* Enable debugger as fault source */ \
false, /* Disable PRS fault source 0 */ \
timerPRSSELCh0, /* Not used by default, select PRS channel 0. */ \
false, /* Disable PRS fault source 1 */ \
timerPRSSELCh0, /* Not used by default, select PRS channel 0. */ \
timerDtiFaultActionInactive, /* No fault action. */ \
}
#define TIMER_DTOGEN_DTOGCDTI0EN
Definition: efr32mg12p_timer.h:1502

Default config for TIMER DTI init structure.

Definition at line 436 of file em_timer.h .

Enumeration Type Documentation

Timer compare/capture mode.

Enumerator
timerCCModeOff

Channel turned off.

timerCCModeCapture

Input capture.

timerCCModeCompare

Output compare.

timerCCModePWM

Pulse-Width modulation.

Definition at line 81 of file em_timer.h .

Clock select.

Enumerator
timerClkSelHFPerClk

Prescaled HFPER clock.

timerClkSelCC1

Compare/Capture Channel 1 Input.

timerClkSelCascade

Cascaded, clocked by underflow (down-counting) or overflow (up-counting) by lower numbered timer.

Definition at line 89 of file em_timer.h .

DT (Dead Time) Fault Actions.

Enumerator
timerDtiFaultActionNone

No action on fault.

timerDtiFaultActionInactive

Set outputs inactive.

timerDtiFaultActionClear

Clear outputs.

timerDtiFaultActionTristate

Tristate outputs.

Definition at line 223 of file em_timer.h .

Input capture edge select.

Enumerator
timerEdgeRising

Rising edges detected.

timerEdgeFalling

Falling edges detected.

timerEdgeBoth

Both edges detected.

timerEdgeNone

No edge detection, leave signal as is.

Definition at line 104 of file em_timer.h .

Input capture event control.

Enumerator
timerEventEveryEdge

PRS output pulse, interrupt flag and DMA request set on every capture.

timerEventEvery2ndEdge

PRS output pulse, interrupt flag and DMA request set on every second capture.

timerEventRising

PRS output pulse, interrupt flag and DMA request set on rising edge (if input capture edge = BOTH).

timerEventFalling

PRS output pulse, interrupt flag and DMA request set on falling edge (if input capture edge = BOTH).

Definition at line 119 of file em_timer.h .

Input edge action.

Enumerator
timerInputActionNone

No action taken.

timerInputActionStart

Start counter without reload.

timerInputActionStop

Stop counter without reload.

timerInputActionReloadStart

Reload and start counter.

Definition at line 137 of file em_timer.h .

Timer mode.

Enumerator
timerModeUp

Up-counting.

timerModeDown

Down-counting.

timerModeUpDown

Up/down-counting.

timerModeQDec

Quadrature decoder.

Definition at line 152 of file em_timer.h .

Compare/capture output action.

Enumerator
timerOutputActionNone

No action.

timerOutputActionToggle

Toggle on event.

timerOutputActionClear

Clear on event.

timerOutputActionSet

Set on event.

Definition at line 160 of file em_timer.h .

Prescaler.

Enumerator
timerPrescale1

Divide by 1.

timerPrescale2

Divide by 2.

timerPrescale4

Divide by 4.

timerPrescale8

Divide by 8.

timerPrescale16

Divide by 16.

timerPrescale32

Divide by 32.

timerPrescale64

Divide by 64.

timerPrescale128

Divide by 128.

timerPrescale256

Divide by 256.

timerPrescale512

Divide by 512.

timerPrescale1024

Divide by 1024.

Definition at line 175 of file em_timer.h .

Peripheral Reflex System signal.

Enumerator
timerPRSSELCh0

PRS channel 0.

timerPRSSELCh1

PRS channel 1.

timerPRSSELCh2

PRS channel 2.

timerPRSSELCh3

PRS channel 3.

timerPRSSELCh4

PRS channel 4.

timerPRSSELCh5

PRS channel 5.

timerPRSSELCh6

PRS channel 6.

timerPRSSELCh7

PRS channel 7.

timerPRSSELCh8

PRS channel 8.

timerPRSSELCh9

PRS channel 9.

timerPRSSELCh10

PRS channel 10.

timerPRSSELCh11

PRS channel 11.

Definition at line 190 of file em_timer.h .

Function Documentation

__STATIC_INLINE uint32_t TIMER_CaptureGet ( TIMER_TypeDef * timer,
unsigned int ch
)

Get capture value for compare/capture channel when operating in capture mode.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] ch Compare/capture channel to access.
Returns
Current capture value.

Definition at line 555 of file em_timer.h .

References TIMER_TypeDef::CC , and TIMER_CC_TypeDef::CCV .

__STATIC_INLINE void TIMER_ClearDTIFault ( TIMER_TypeDef * timer,
uint32_t flags
)

Clear DTI fault source flags.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] flags DTI fault source(s) to clear. Use one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.

Definition at line 721 of file em_timer.h .

References TIMER_TypeDef::DTFAULTC , and TIMER0 .

Referenced by TIMER_InitDTI() .

__STATIC_INLINE void TIMER_CompareBufSet ( TIMER_TypeDef * timer,
unsigned int ch,
uint32_t val
)

Set compare value buffer for compare/capture channel when operating in compare or PWM mode.

The compare value buffer holds the value which will be written to TIMERn_CCx_CCV on an update event if the buffer has been updated since the last event.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] ch Compare/capture channel to access.
[in] val Value to set in compare value buffer register.

Definition at line 579 of file em_timer.h .

References TIMER_TypeDef::CC , TIMER_CC_TypeDef::CCVB , and TIMER_MaxCount() .

Referenced by BOARD_rgbledSetRawColor() .

__STATIC_INLINE void TIMER_CompareSet ( TIMER_TypeDef * timer,
unsigned int ch,
uint32_t val
)

Set compare value for compare/capture channel when operating in compare or PWM mode.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] ch Compare/capture channel to access.
[in] val Value to set in compare value register.

Definition at line 601 of file em_timer.h .

References TIMER_TypeDef::CC , TIMER_CC_TypeDef::CCV , and TIMER_MaxCount() .

__STATIC_INLINE uint32_t TIMER_CounterGet ( TIMER_TypeDef * timer )

Get TIMER counter value.

Parameters
[in] timer Pointer to TIMER peripheral register block.
Returns
Current TIMER counter value.

Definition at line 619 of file em_timer.h .

References TIMER_TypeDef::CNT .

__STATIC_INLINE void TIMER_CounterSet ( TIMER_TypeDef * timer,
uint32_t val
)

Set TIMER counter value.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] val Value to set counter to.

Definition at line 634 of file em_timer.h .

References TIMER_TypeDef::CNT , and TIMER_MaxCount() .

__STATIC_INLINE void TIMER_Enable ( TIMER_TypeDef * timer,
bool enable
)

Start/stop TIMER.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] enable true to enable counting, false to disable.

Definition at line 650 of file em_timer.h .

References TIMER_TypeDef::CMD , TIMER_CMD_START , and TIMER_CMD_STOP .

Referenced by BOARD_rgbledSetRawColor() , and USTIMER_DeInit() .

__STATIC_INLINE void TIMER_EnableDTI ( TIMER_TypeDef * timer,
bool enable
)

Enable or disable DTI unit.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] enable true to enable DTI unit, false to disable.

Definition at line 679 of file em_timer.h .

References TIMER_TypeDef::DTCTRL , TIMER0 , and TIMER_DTCTRL_DTEN .

Referenced by TIMER_InitDTI() .

__STATIC_INLINE uint32_t TIMER_GetDTIFault ( TIMER_TypeDef * timer )

Get DTI fault source flags status.

Note
The event bits are not cleared by the use of this function.
Parameters
[in] timer Pointer to TIMER peripheral register block.
Returns
Status of the DTI fault source flags. Returns one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.

Definition at line 704 of file em_timer.h .

References TIMER_TypeDef::DTFAULT , and TIMER0 .

Referenced by TIMER_InitDTI() .

void TIMER_Init ( TIMER_TypeDef * timer,
const TIMER_Init_TypeDef * init
)

Initialize TIMER.

Notice that counter top must be configured separately with for instance TIMER_TopSet() . In addition, compare/capture and dead-time insertion init must be initialized separately if used. That should probably be done prior to the use of this function if configuring the TIMER to start when initialization is completed.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] init Pointer to TIMER initialization structure.

Definition at line 75 of file em_timer.c .

References _TIMER_CNT_RESETVALUE , _TIMER_CTRL_CLKSEL_SHIFT , _TIMER_CTRL_FALLA_SHIFT , _TIMER_CTRL_MODE_SHIFT , _TIMER_CTRL_PRESC_SHIFT , _TIMER_CTRL_RISEA_SHIFT , TIMER_Init_TypeDef::ati , TIMER_Init_TypeDef::clkSel , TIMER_TypeDef::CMD , TIMER_TypeDef::CNT , TIMER_Init_TypeDef::count2x , TIMER_TypeDef::CTRL , TIMER_Init_TypeDef::debugRun , TIMER_Init_TypeDef::dmaClrAct , TIMER_Init_TypeDef::enable , TIMER_Init_TypeDef::fallAction , TIMER_Init_TypeDef::mode , TIMER_Init_TypeDef::oneShot , TIMER_Init_TypeDef::prescale , TIMER_Init_TypeDef::quadModeX4 , TIMER_Init_TypeDef::riseAction , TIMER_Init_TypeDef::sync , TIMER_CMD_START , TIMER_CMD_STOP , TIMER_CTRL_ATI , TIMER_CTRL_DEBUGRUN , TIMER_CTRL_DMACLRACT , TIMER_CTRL_OSMEN , TIMER_CTRL_QDM_X4 , TIMER_CTRL_SYNC , and TIMER_CTRL_X2CNT .

Referenced by BOARD_init() , and USTIMER_Init() .

void TIMER_InitDTI ( TIMER_TypeDef * timer,
const TIMER_InitDTI_TypeDef * init
)
__STATIC_INLINE void TIMER_IntClear ( TIMER_TypeDef * timer,
uint32_t flags
)

Clear one or more pending TIMER interrupts.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] flags Pending TIMER interrupt source(s) to clear. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Definition at line 740 of file em_timer.h .

References TIMER_TypeDef::IFC .

Referenced by USTIMER_DeInit() .

__STATIC_INLINE void TIMER_IntDisable ( TIMER_TypeDef * timer,
uint32_t flags
)

Disable one or more TIMER interrupts.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] flags TIMER interrupt source(s) to disable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Definition at line 756 of file em_timer.h .

References TIMER_TypeDef::IEN .

Referenced by USTIMER_DeInit() , and USTIMER_Init() .

__STATIC_INLINE void TIMER_IntEnable ( TIMER_TypeDef * timer,
uint32_t flags
)

Enable one or more TIMER interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using TIMER_IntClear() prior to enabling if such a pending interrupt should be ignored.
Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] flags TIMER interrupt source(s) to enable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Definition at line 777 of file em_timer.h .

References TIMER_TypeDef::IEN .

__STATIC_INLINE uint32_t TIMER_IntGet ( TIMER_TypeDef * timer )

Get pending TIMER interrupt flags.

Note
The event bits are not cleared by the use of this function.
Parameters
[in] timer Pointer to TIMER peripheral register block.
Returns
TIMER interrupt source(s) pending. Returns one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Definition at line 796 of file em_timer.h .

References TIMER_TypeDef::IF .

__STATIC_INLINE uint32_t TIMER_IntGetEnabled ( TIMER_TypeDef * timer )

Get enabled and pending TIMER interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.

Parameters
[in] timer Pointer to TIMER peripheral register block.
Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled TIMER interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in TIMERx_IEN_nnn register (TIMERx_IEN_nnn) and
  • the OR combination of valid interrupt flags of the TIMER module (TIMERx_IF_nnn).

Definition at line 820 of file em_timer.h .

References TIMER_TypeDef::IEN , and TIMER_TypeDef::IF .

__STATIC_INLINE void TIMER_IntSet ( TIMER_TypeDef * timer,
uint32_t flags
)

Set one or more pending TIMER interrupts from SW.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] flags TIMER interrupt source(s) to set to pending. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Definition at line 843 of file em_timer.h .

References TIMER_TypeDef::IFS .

__STATIC_INLINE void TIMER_Lock ( TIMER_TypeDef * timer )

Lock some of the TIMER registers in order to protect them from being modified.

Please refer to the reference manual for TIMER registers that will be locked.

Note
If locking the TIMER registers, they must be unlocked prior to using any TIMER API functions modifying TIMER registers protected by the lock.
Parameters
[in] timer Pointer to TIMER peripheral register block.

Definition at line 865 of file em_timer.h .

References TIMER_TypeDef::DTLOCK , TIMER0 , and TIMER_DTLOCK_LOCKKEY_LOCK .

__STATIC_INLINE uint32_t TIMER_MaxCount ( const TIMER_TypeDef * ref )

Get the Max count of the timer.

Parameters
[in] timer Pointer to TIMER peripheral register block.
Returns
The max count value of the timer. This is 0xFFFF for 16 bit timers and 0xFFFFFFFF for 32 bit timers.

Definition at line 519 of file em_timer.h .

References WTIMER0 , and WTIMER1 .

Referenced by TIMER_CompareBufSet() , TIMER_CompareSet() , TIMER_CounterSet() , TIMER_TopBufSet() , and TIMER_TopSet() .

__STATIC_INLINE void TIMER_TopBufSet ( TIMER_TypeDef * timer,
uint32_t val
)

Set top value buffer for timer.

When the top value buffer register is updated, the value is loaded into the top value register at the next wrap around. This feature is useful in order to update the top value safely when the timer is running.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] val Value to set in top value buffer register.

Definition at line 890 of file em_timer.h .

References TIMER_MaxCount() , and TIMER_TypeDef::TOPB .

__STATIC_INLINE uint32_t TIMER_TopGet ( TIMER_TypeDef * timer )

Get top value setting for timer.

Parameters
[in] timer Pointer to TIMER peripheral register block.
Returns
Current top value.

Definition at line 906 of file em_timer.h .

References TIMER_TypeDef::TOP .

__STATIC_INLINE void TIMER_TopSet ( TIMER_TypeDef * timer,
uint32_t val
)

Set top value for timer.

Parameters
[in] timer Pointer to TIMER peripheral register block.
[in] val Value to set in top value register.

Definition at line 921 of file em_timer.h .

References TIMER_MaxCount() , and TIMER_TypeDef::TOP .

Referenced by BOARD_init() , and USTIMER_Init() .

__STATIC_INLINE void TIMER_Unlock ( TIMER_TypeDef * timer )

Unlock the TIMER so that writing to locked registers again is possible.

Parameters
[in] timer Pointer to TIMER peripheral register block.

Definition at line 935 of file em_timer.h .

References TIMER_TypeDef::DTLOCK , TIMER0 , and TIMER_DTLOCK_LOCKKEY_UNLOCK .

__STATIC_INLINE bool TIMER_Valid ( const TIMER_TypeDef * ref )

Validate the TIMER register block pointer.

Parameters
[in] ref Pointer to TIMER peripheral register block.
Returns
true if ref points to a valid timer, false otherwise.

Definition at line 472 of file em_timer.h .

References TIMER0 , TIMER1 , WTIMER0 , and WTIMER1 .