LESENSE_AltExDesc_TypeDef Struct ReferenceEMLIB > LESENSE

Alternate excitation descriptor structure.

Definition at line 925 of file em_lesense.h .

#include < em_lesense.h >

Data Fields

bool alwaysEx
bool enablePin
LESENSE_AltExPinIdle_TypeDef idleConf

Field Documentation

bool LESENSE_AltExDesc_TypeDef::alwaysEx

Configure how to control the external alternate excitation pins. Only applies if altExMap has been set to lesenseAltExMapALTEX. If true, the excitation happens on the corresponding alternate excitation pin during the excitation periods of all enabled channels. If false, the excitation happens on the corresponding alternate excitation pin ONLY during the excitation period of the corresponding channel. The alwaysEx parameter is not valid when altExMap==lesenseAltExMapACMP.

Definition at line 941 of file em_lesense.h .

Referenced by LESENSE_AltExConfig() .

bool LESENSE_AltExDesc_TypeDef::enablePin

Configure alternate excitation pins. If set, the corresponding alternate excitation pin/signal is enabled.

Definition at line 928 of file em_lesense.h .

Referenced by LESENSE_AltExConfig() .

LESENSE_AltExPinIdle_TypeDef LESENSE_AltExDesc_TypeDef::idleConf

Configure idle phase setup of alternate excitation pins. The idleConf parameter is not valid when altExMap==lesenseAltExMapACMP.

Definition at line 932 of file em_lesense.h .

Referenced by LESENSE_AltExConfig() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_lesense.h