CMU_LFXOInit_TypeDef Struct ReferenceEMLIB > CMU

LFXO initialization structure. Init values should be obtained from a configuration tool, app note or xtal datasheet

Definition at line 1349 of file em_cmu.h .

#include < em_cmu.h >

Data Fields

uint8_t ctune
uint8_t gain
CMU_OscMode_TypeDef mode
uint8_t timeout

Field Documentation

uint8_t CMU_LFXOInit_TypeDef::ctune

CTUNE (load capacitance) value

Definition at line 1351 of file em_cmu.h .

Referenced by BSP_initClocks() , and CMU_LFXOInit() .

uint8_t CMU_LFXOInit_TypeDef::gain

Gain / max startup margin

Definition at line 1352 of file em_cmu.h .

Referenced by CMU_LFXOInit() .

CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode

Oscillator mode

Definition at line 1357 of file em_cmu.h .

Referenced by CMU_LFXOInit() .

uint8_t CMU_LFXOInit_TypeDef::timeout

Startup delay

Definition at line 1356 of file em_cmu.h .

Referenced by CMU_LFXOInit() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_cmu.h