ADC_InitScan_TypeDef Struct ReferenceEMLIB > ADC
Scan sequence init structure.
Definition at line
862
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
ADC_AcqTime_TypeDef | acqTime |
bool | diff |
bool | fifoOverwrite |
bool | leftAdjust |
bool | prsEnable |
ADC_PRSSEL_TypeDef | prsSel |
ADC_Ref_TypeDef | reference |
bool | rep |
ADC_Res_TypeDef | resolution |
bool | scanDmaEm2Wu |
ADC_InitScanInput_TypeDef | scanInputConfig |
Field Documentation
ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line
870
of file
em_adc.h
.
Referenced by ADC_InitScan() .
bool ADC_InitScan_TypeDef::diff |
Select if single ended or differential input.
Definition at line
900
of file
em_adc.h
.
Referenced by ADC_InitScan() , ADC_ScanDifferentialInputAdd() , and ADC_ScanSingleEndedInputAdd() .
bool ADC_InitScan_TypeDef::fifoOverwrite |
When true, the FIFO overwrites old data when full. If false, then the FIFO discards new data. The SINGLEOF IRQ is triggered in both cases.
Definition at line
919
of file
em_adc.h
.
Referenced by ADC_InitScan() .
bool ADC_InitScan_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line
906
of file
em_adc.h
.
Referenced by ADC_InitScan() .
bool ADC_InitScan_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line
903
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsEnable
is enabled.
Definition at line
867
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference |
Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.
Definition at line
876
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
bool ADC_InitScan_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line
909
of file
em_adc.h
.
Referenced by ADC_InitScan() .
ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution |
bool ADC_InitScan_TypeDef::scanDmaEm2Wu |
When true, DMA is available in EM2 for scan conversion
Definition at line
913
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
ADC_InitScanInput_TypeDef ADC_InitScan_TypeDef::scanInputConfig |
Scan input configuration. Use ADC_ScanInputClear() , ADC_ScanSingleEndedInputAdd() or ADC_ScanDifferentialInputAdd() to update this struct.
Definition at line
896
of file
em_adc.h
.
Referenced by ADC_InitScan() , ADC_ScanDifferentialInputAdd() , ADC_ScanInputClear() , and ADC_ScanSingleEndedInputAdd() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_adc.h