WDOGEMLIB
Detailed Description
Watchdog (WDOG) Peripheral API.
This module contains functions to control the WDOG peripheral of Silicon Labs 32-bit MCUs and SoCs. The WDOG resets the system in case of a fault condition.
Data Structures |
|
struct | WDOG_Init_TypeDef |
Macros |
|
#define | DEFAULT_WDOG WDOG0 |
#define | WDOG_INIT_DEFAULT |
Enumerations |
|
enum |
WDOG_ClkSel_TypeDef
{
wdogClkSelULFRCO = _WDOG_CTRL_CLKSEL_ULFRCO, wdogClkSelLFRCO = _WDOG_CTRL_CLKSEL_LFRCO, wdogClkSelLFXO = _WDOG_CTRL_CLKSEL_LFXO } |
enum |
WDOG_PeriodSel_TypeDef
{
wdogPeriod_9 = 0x0, wdogPeriod_17 = 0x1, wdogPeriod_33 = 0x2, wdogPeriod_65 = 0x3, wdogPeriod_129 = 0x4, wdogPeriod_257 = 0x5, wdogPeriod_513 = 0x6, wdogPeriod_1k = 0x7, wdogPeriod_2k = 0x8, wdogPeriod_4k = 0x9, wdogPeriod_8k = 0xA, wdogPeriod_16k = 0xB, wdogPeriod_32k = 0xC, wdogPeriod_64k = 0xD, wdogPeriod_128k = 0xE, wdogPeriod_256k = 0xF } |
enum |
WDOG_WarnSel_TypeDef
{
wdogWarnDisable = 0, wdogWarnTime25pct = 1, wdogWarnTime50pct = 2, wdogWarnTime75pct = 3 } |
enum |
WDOG_WinSel_TypeDef
{
wdogIllegalWindowDisable = 0, wdogIllegalWindowTime12_5pct = 1, wdogIllegalWindowTime25_0pct = 2, wdogIllegalWindowTime37_5pct = 3, wdogIllegalWindowTime50_0pct = 4, wdogIllegalWindowTime62_5pct = 5, wdogIllegalWindowTime75_0pct = 6, wdogIllegalWindowTime87_5pct = 7 } |
Functions |
|
__STATIC_INLINE void | WDOG_Enable (bool enable) |
Enable/disable the watchdog timer.
|
|
__STATIC_INLINE void | WDOG_Feed (void) |
Feed the watchdog.
|
|
__STATIC_INLINE void | WDOG_Init (const WDOG_Init_TypeDef *init) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
|
|
__STATIC_INLINE void | WDOG_Lock (void) |
Lock the watchdog configuration.
|
|
void | WDOGn_Enable ( WDOG_TypeDef *wdog, bool enable) |
Enable/disable the watchdog timer.
|
|
void | WDOGn_Feed ( WDOG_TypeDef *wdog) |
Feed the watchdog.
|
|
void | WDOGn_Init ( WDOG_TypeDef *wdog, const WDOG_Init_TypeDef *init) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
|
|
__STATIC_INLINE void | WDOGn_IntClear ( WDOG_TypeDef *wdog, uint32_t flags) |
Clear one or more pending WDOG interrupts.
|
|
__STATIC_INLINE void | WDOGn_IntDisable ( WDOG_TypeDef *wdog, uint32_t flags) |
Disable one or more WDOG interrupts.
|
|
__STATIC_INLINE void | WDOGn_IntEnable ( WDOG_TypeDef *wdog, uint32_t flags) |
Enable one or more WDOG interrupts.
|
|
__STATIC_INLINE uint32_t | WDOGn_IntGet ( WDOG_TypeDef *wdog) |
Get pending WDOG interrupt flags.
|
|
__STATIC_INLINE uint32_t | WDOGn_IntGetEnabled ( WDOG_TypeDef *wdog) |
Get enabled and pending WDOG interrupt flags.
|
|
__STATIC_INLINE void | WDOGn_IntSet ( WDOG_TypeDef *wdog, uint32_t flags) |
Set one or more pending WDOG interrupts from SW.
|
|
void | WDOGn_Lock ( WDOG_TypeDef *wdog) |
Lock the watchdog configuration.
|
|
Macro Definition Documentation
#define DEFAULT_WDOG WDOG0 |
Default WDOG instance for deprecated functions.
Definition at line
323
of file
em_wdog.h
.
Referenced by WDOG_Enable() , WDOG_Feed() , WDOG_Init() , and WDOG_Lock() .
#define WDOG_INIT_DEFAULT |
Suggested default config for WDOG init structure.
Definition at line
163
of file
em_wdog.h
.
Enumeration Type Documentation
enum WDOG_ClkSel_TypeDef |
Watchdog period selection.
Definition at line
67
of file
em_wdog.h
.
enum WDOG_WarnSel_TypeDef |
Select watchdog warning timeout period as percentage of timeout.
Definition at line
88
of file
em_wdog.h
.
enum WDOG_WinSel_TypeDef |
Select watchdog illegal window limit.
Definition at line
98
of file
em_wdog.h
.
Function Documentation
__STATIC_INLINE void WDOG_Enable | ( | bool |
enable
|
) |
Enable/disable the watchdog timer.
- Deprecated:
- Deprecated function. New code should use WDOGn_Enable() . This function uses DEFAULT_WDOG .
- Parameters
-
[in] enable
true to enable watchdog, false to disable. Watchdog cannot be disabled if watchdog has been locked.
Definition at line
339
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Enable() .
__STATIC_INLINE void WDOG_Feed | ( | void |
|
) |
Feed the watchdog.
- Deprecated:
- Deprecated function. New code should use WDOGn_Feed() . This function uses DEFAULT_WDOG .
Definition at line
352
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Feed() .
__STATIC_INLINE void WDOG_Init | ( | const WDOG_Init_TypeDef * |
init
|
) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
- Deprecated:
- Deprecated function. New code should use Use WDOGn_Init() . This function uses DEFAULT_WDOG .
- Parameters
-
[in] init
Structure holding watchdog configuration. A default setting WDOG_INIT_DEFAULT is available for init.
Definition at line
370
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Init() .
__STATIC_INLINE void WDOG_Lock | ( | void |
|
) |
Lock the watchdog configuration.
- Deprecated:
- Deprecated function. New code should use WDOGn_Lock() . This function uses DEFAULT_WDOG .
Definition at line
383
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Lock() .
void WDOGn_Enable | ( | WDOG_TypeDef * |
wdog,
|
bool |
enable
|
||
) |
Enable/disable the watchdog timer.
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block. [in] enable
true to enable watchdog, false to disable. Watchdog cannot be disabled if watchdog has been locked.
Definition at line
75
of file
em_wdog.c
.
References _WDOG_CTRL_EN_SHIFT , BUS_RegBitRead() , BUS_RegBitWrite() , WDOG_TypeDef::CTRL , WDOG_TypeDef::SYNCBUSY , WDOG_CTRL_LOCK , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Enable() .
void WDOGn_Feed | ( | WDOG_TypeDef * |
wdog
|
) |
Feed the watchdog.
When the watchdog is activated, it must be fed (ie clearing the counter) before it reaches the defined timeout period. Otherwise, the watchdog will generate a reset.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block.
Definition at line
109
of file
em_wdog.c
.
References WDOG_TypeDef::CMD , WDOG_TypeDef::CTRL , WDOG_TypeDef::SYNCBUSY , WDOG_CMD_CLEAR , WDOG_CTRL_EN , WDOG_SYNCBUSY_CMD , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Feed() .
void WDOGn_Init | ( | WDOG_TypeDef * |
wdog,
|
const WDOG_Init_TypeDef * |
init
|
||
) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block. [in] init
Structure holding watchdog configuration. A default setting WDOG_INIT_DEFAULT is available for init.
Definition at line
149
of file
em_wdog.c
.
References _WDOG_CTRL_CLKSEL_SHIFT , _WDOG_CTRL_PERSEL_SHIFT , _WDOG_CTRL_WARNSEL_MASK , _WDOG_CTRL_WARNSEL_SHIFT , _WDOG_CTRL_WINSEL_MASK , _WDOG_CTRL_WINSEL_SHIFT , WDOG_Init_TypeDef::clkSel , WDOG_TypeDef::CTRL , WDOG_Init_TypeDef::debugRun , WDOG_Init_TypeDef::em2Run , WDOG_Init_TypeDef::em3Run , WDOG_Init_TypeDef::em4Block , WDOG_Init_TypeDef::enable , WDOG_Init_TypeDef::lock , WDOG_Init_TypeDef::perSel , WDOG_Init_TypeDef::resetDisable , WDOG_Init_TypeDef::swoscBlock , WDOG_TypeDef::SYNCBUSY , WDOG_Init_TypeDef::warnSel , WDOG_CTRL_DEBUGRUN , WDOG_CTRL_EM2RUN , WDOG_CTRL_EM3RUN , WDOG_CTRL_EM4BLOCK , WDOG_CTRL_EN , WDOG_CTRL_LOCK , WDOG_CTRL_SWOSCBLOCK , WDOG_CTRL_WDOGRSTDIS , WDOG_SYNCBUSY_CTRL , and WDOG_Init_TypeDef::winSel .
Referenced by WDOG_Init() .
__STATIC_INLINE void WDOGn_IntClear | ( | WDOG_TypeDef * |
wdog,
|
uint32_t |
flags
|
||
) |
Clear one or more pending WDOG interrupts.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block. [in] flags
WDOG interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.
Definition at line
216
of file
em_wdog.h
.
References WDOG_TypeDef::IFC .
__STATIC_INLINE void WDOGn_IntDisable | ( | WDOG_TypeDef * |
wdog,
|
uint32_t |
flags
|
||
) |
Disable one or more WDOG interrupts.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block. [in] flags
WDOG interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.
Definition at line
232
of file
em_wdog.h
.
References WDOG_TypeDef::IEN .
__STATIC_INLINE void WDOGn_IntEnable | ( | WDOG_TypeDef * |
wdog,
|
uint32_t |
flags
|
||
) |
Enable one or more WDOG interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using WDOG_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block. [in] flags
WDOG interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.
Definition at line
253
of file
em_wdog.h
.
References WDOG_TypeDef::IEN .
__STATIC_INLINE uint32_t WDOGn_IntGet | ( | WDOG_TypeDef * |
wdog
|
) |
Get pending WDOG interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block.
- Returns
- Pending WDOG interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
Definition at line
272
of file
em_wdog.h
.
References WDOG_TypeDef::IF .
__STATIC_INLINE uint32_t WDOGn_IntGetEnabled | ( | WDOG_TypeDef * |
wdog
|
) |
Get enabled and pending WDOG interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block.
- Returns
- Pending and enabled WDOG interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
Definition at line
291
of file
em_wdog.h
.
References WDOG_TypeDef::IEN , and WDOG_TypeDef::IF .
__STATIC_INLINE void WDOGn_IntSet | ( | WDOG_TypeDef * |
wdog,
|
uint32_t |
flags
|
||
) |
Set one or more pending WDOG interrupts from SW.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block. [in] flags
WDOG interrupt sources to set to pending. Use a set of interrupt flags (WDOG_IFS_nnn).
Definition at line
312
of file
em_wdog.h
.
References WDOG_TypeDef::IFS .
void WDOGn_Lock | ( | WDOG_TypeDef * |
wdog
|
) |
Lock the watchdog configuration.
This prevents errors from overwriting the watchdog configuration, possibly disabling it. Only a reset can unlock the watchdog config, once locked.
If the LFRCO or LFXO clocks are used to clock the watchdog, one should consider using the option of inhibiting those clocks to be disabled, please see the WDOG_Enable() init structure.
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdog
Pointer to WDOG peripheral register block.
Definition at line
223
of file
em_wdog.c
.
References _WDOG_CTRL_LOCK_SHIFT , BUS_RegBitWrite() , WDOG_TypeDef::CTRL , WDOG_TypeDef::SYNCBUSY , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Lock() .