CapSenseKit Drivers
         Functions | 
       |
| uint32_t | CAPLESENSE_getNormalizedVal (uint8_t channel) | 
| 
         Get the current normalized channelValue for a channel.
          | 
       |
| uint8_t | CAPLESENSE_getSegmentChannel (uint8_t capSegment) | 
| 
         Get the channelValue for a sensor segment.
          | 
       |
| int32_t | CAPLESENSE_getSliderPosition (void) | 
| 
         Get the position of the slider.
          | 
       |
| uint32_t | CAPLESENSE_getVal (uint8_t channel) | 
| 
         Get the current channelValue for a channel.
          | 
       |
| void | CAPLESENSE_Init (bool sleep) | 
| 
         Initializes the capacative sense system without LESENSE.
          | 
       |
| void | CAPLESENSE_setupCallbacks (void(*scanCb)(void), void(*chCb)(void)) | 
| 
         LESENSE callback setup.
          | 
       |
| void | CAPLESENSE_setupLESENSE (bool sleep) | 
| 
         Setup the LESENSE for capavitive sensing.
          | 
       |
| void | CAPLESENSE_Sleep (void) | 
| 
         Send the capacative sense system to sleep mode.
          | 
       |
| uint32_t | CAPSENSE_getNormalizedVal (uint8_t channel) | 
| 
         Get the current normalized channelValue for a channel.
          | 
       |
| bool | CAPSENSE_getPressed (uint8_t channel) | 
| 
         Get the state of the Gecko Button.
          | 
       |
| int32_t | CAPSENSE_getSliderPosition (void) | 
| 
         Get the position of the slider.
          | 
       |
| uint32_t | CAPSENSE_getVal (uint8_t channel) | 
| 
         Get the current channelValue for a channel.
          | 
       |
| void | CAPSENSE_Init (void) | 
| 
         Initializes the capacitive sense system.
          | 
       |
| void | CAPSENSE_Sense (void) | 
| 
         This function iterates through all the capsensors and reads and initiates a reading. Uses EM1 while waiting for the result from each sensor.
          | 
       |
Function Documentation
| uint32_t CAPLESENSE_getNormalizedVal | ( | uint8_t | 
           
            channel
           
           | 
          ) | 
Get the current normalized channelValue for a channel.
- Parameters
 - 
         
channelThe channel.  
- Returns
 - The channel value in range (0-256).
 
        Definition at line
        
         425
        
        of file
        
         caplesense.c
        
        .
       
References channelMaxValues , and channelValues .
| uint8_t CAPLESENSE_getSegmentChannel | ( | uint8_t | 
           
            capSegment
           
           | 
          ) | 
Get the channelValue for a sensor segment.
- Parameters
 - 
         
capSegment 
- Returns
 - channel
 
        Definition at line
        
         389
        
        of file
        
         caplesense.c
        
        .
       
| int32_t CAPLESENSE_getSliderPosition | ( | void | 
           
           
           | 
          ) | 
Get the position of the slider.
- Returns
 - The position of the slider if it can be determined, -1 otherwise.
 
        Definition at line
        
         436
        
        of file
        
         caplesense.c
        
        .
       
References channelMaxValues , and channelValues .
| uint32_t CAPLESENSE_getVal | ( | uint8_t | 
           
            channel
           
           | 
          ) | 
Get the current channelValue for a channel.
- Parameters
 - 
         
channelThe channel.  
- Returns
 - The channelValue.
 
        Definition at line
        
         415
        
        of file
        
         caplesense.c
        
        .
       
References channelValues .
| void CAPLESENSE_Init | ( | bool | 
           
            sleep
           
           | 
          ) | 
Initializes the capacative sense system without LESENSE.
- Parameters
 - 
         
sleepIf true, go into sleep mode.  
        Definition at line
        
         501
        
        of file
        
         caplesense.c
        
        .
       
References CAPLESENSE_setupACMP() , CAPLESENSE_setupCMU() , CAPLESENSE_setupGPIO() , CAPLESENSE_setupLESENSE() , CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , and CORE_EXIT_ATOMIC .
| void CAPLESENSE_setupCallbacks | ( | void(*)(void) | 
           
            scanCb,
           
           | 
         
| void(*)(void) | 
           
            chCb
           
           | 
         ||
| ) | 
LESENSE callback setup.
- Parameters
 - 
         
scanCbScan callback chCbChannel callback  
        Definition at line
        
         330
        
        of file
        
         caplesense.c
        
        .
       
References lesenseChCb , and lesenseScanCb .
| void CAPLESENSE_setupLESENSE | ( | bool | 
           
            sleep
           
           | 
          ) | 
Setup the LESENSE for capavitive sensing.
- Parameters
 - 
         
sleepIf true, go into sleep mode.  
        Definition at line
        
         163
        
        of file
        
         caplesense.c
        
        .
       
References channelsInUse , LESENSE_Init_TypeDef::coreCtrl , LESENSE , LESENSE_ChannelAllConfig() , LESENSE_ChannelThresSet() , LESENSE_ClkDivSet() , LESENSE_Init() , LESENSE_IntClear() , LESENSE_IntDisable() , LESENSE_IntEnable() , LESENSE_IRQn , LESENSE_ResultBufferClear() , LESENSE_ScanFreqSet() , LESENSE_ScanResultDataBufferGet() , LESENSE_ScanStart() , LESENSE_ScanStop() , LESENSE_STATUS_BUFHALFFULL , LESENSE_STATUS_SCANACTIVE , LESENSE_StatusGet() , lesenseACMPModeMuxThres , lesenseBiasModeDutyCycle , lesenseBufTrigHalf , lesenseClkDiv_1 , lesenseClkDiv_8 , lesenseClkLF , lesenseDACConvModeDisable , lesenseDACIfData , lesenseDACOutModeDisable , lesenseDACRefBandGap , lesenseDecInputSensorSt , lesenseDMAWakeUpDisable , lesensePRSCh0 , lesensePRSCh1 , lesensePRSCh2 , lesensePRSCh3 , lesenseScanConfDirMap , lesenseScanStartPeriodic , lesenseWarmupModeNormal , and LESENSE_CoreCtrlDesc_TypeDef::scanStart .
Referenced by CAPLESENSE_Init() .
| uint32_t CAPSENSE_getNormalizedVal | ( | uint8_t | 
           
            channel
           
           | 
          ) | 
Get the current normalized channelValue for a channel.
- Parameters
 - 
         
channelThe channel.  
- Returns
 - The channel value in range (0-256).
 
        Definition at line
        
         132
        
        of file
        
         capsense.c
        
        .
       
References channelMaxValues , and channelValues .
| bool CAPSENSE_getPressed | ( | uint8_t | 
           
            channel
           
           | 
          ) | 
Get the state of the Gecko Button.
- Parameters
 - 
         
channelThe channel.  
- Returns
 - true if the button is "pressed" false otherwise.
 
        Definition at line
        
         144
        
        of file
        
         capsense.c
        
        .
       
References channelMaxValues , and channelValues .
| int32_t CAPSENSE_getSliderPosition | ( | void | 
           
           
           | 
          ) | 
Get the position of the slider.
- Returns
 - The position of the slider if it can be determined, -1 otherwise.
 
        Definition at line
        
         164
        
        of file
        
         capsense.c
        
        .
       
References channelMaxValues , and channelValues .
| uint32_t CAPSENSE_getVal | ( | uint8_t | 
           
            channel
           
           | 
          ) | 
Get the current channelValue for a channel.
- Parameters
 - 
         
channelThe channel.  
- Returns
 - The channelValue.
 
        Definition at line
        
         122
        
        of file
        
         capsense.c
        
        .
       
References channelValues .
| void CAPSENSE_Init | ( | void | 
           
           
           | 
          ) | 
Initializes the capacitive sense system.
Capacitive sensing uses two timers: TIMER0 and TIMER1 as well as ACMP. ACMP is set up in cap-sense (oscillator mode). TIMER1 counts the number of pulses generated by ACMP_CAPSENSE. When TIMER0 expires it generates an interrupt. The number of pulses counted by TIMER1 is then stored in channelValues
        Definition at line
        
         284
        
        of file
        
         capsense.c
        
        .
       
References ACMP_CAPSENSE_INIT_DEFAULT , ACMP_CapsenseInit() , CMU , CMU_ClockEnable() , cmuClock_HFPER , cmuClock_PRS , cmuClock_TIMER0 , cmuClock_TIMER1 , PRS , PRS_CH_CTRL_EDSEL_POSEDGE , TIMER0 , TIMER0_IRQn , TIMER1 , TIMER_CC_CTRL_ICEDGE_BOTH , TIMER_CC_CTRL_ICEVCTRL_RISING , TIMER_CC_CTRL_INSEL_PRS , TIMER_CC_CTRL_MODE_INPUTCAPTURE , TIMER_CC_CTRL_PRSSEL_PRSCH0 , TIMER_CTRL_CLKSEL_CC1 , TIMER_CTRL_PRESC_DIV1024 , TIMER_CTRL_PRESC_DIV512 , and TIMER_IEN_OF .