DEVINFO_TypeDef Struct ReferenceDevices > EZR32LG_DEVINFO
       Definition at line
       
        47
       
       of file
       
        ezr32lg_devinfo.h
       
       .
      
         Data Fields | 
       |
| __IM uint32_t | ADC0CAL0 | 
| __IM uint32_t | ADC0CAL1 | 
| __IM uint32_t | ADC0CAL2 | 
| __IM uint32_t | AUXHFRCOCAL0 | 
| __IM uint32_t | AUXHFRCOCAL1 | 
| __IM uint32_t | CAL | 
| __IM uint32_t | DAC0CAL0 | 
| __IM uint32_t | DAC0CAL1 | 
| __IM uint32_t | DAC0CAL2 | 
| __IM uint32_t | HFRCOCAL0 | 
| __IM uint32_t | HFRCOCAL1 | 
| __IM uint32_t | MEMINFO | 
| __IM uint32_t | MSIZE | 
| __IM uint32_t | PART | 
| __IM uint32_t | RADIO0 | 
| __IM uint32_t | RADIO1 | 
| __IM uint32_t | RADIO2 | 
| uint32_t | RESERVED0 [2] | 
| uint32_t | RESERVED2 | 
| __IM uint32_t | UNIQUEH | 
| __IM uint32_t | UNIQUEL | 
Field Documentation
| __IM uint32_t DEVINFO_TypeDef::ADC0CAL0 | 
ADC0 Calibration register 0
        Definition at line
        
         51
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::ADC0CAL1 | 
ADC0 Calibration register 1
        Definition at line
        
         52
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::ADC0CAL2 | 
ADC0 Calibration register 2
        Definition at line
        
         53
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL0 | 
AUXHFRCO calibration register 0
        Definition at line
        
         58
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL1 | 
AUXHFRCO calibration register 1
        Definition at line
        
         59
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::CAL | 
Calibration temperature and checksum
        Definition at line
        
         50
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::DAC0CAL0 | 
DAC calibrartion register 0
        Definition at line
        
         55
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::DAC0CAL1 | 
DAC calibrartion register 1
        Definition at line
        
         56
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::DAC0CAL2 | 
DAC calibrartion register 2
        Definition at line
        
         57
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::HFRCOCAL0 | 
HFRCO calibration register 0
        Definition at line
        
         60
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::HFRCOCAL1 | 
HFRCO calibration register 1
        Definition at line
        
         61
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::MEMINFO | 
Memory information
        Definition at line
        
         62
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::MSIZE | 
Flash and SRAM Memory size in KiloBytes
        Definition at line
        
         67
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::PART | 
Part description
        Definition at line
        
         68
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::RADIO0 | 
Radio information 0
        Definition at line
        
         48
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::RADIO1 | 
Radio information 1
        Definition at line
        
         49
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::RADIO2 | 
Radio information 2
        Definition at line
        
         64
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| uint32_t DEVINFO_TypeDef::RESERVED0[2] | 
Reserved
        Definition at line
        
         54
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| uint32_t DEVINFO_TypeDef::RESERVED2 | 
Reserved
        Definition at line
        
         63
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::UNIQUEH | 
High 32 bits of device unique number
        Definition at line
        
         66
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
| __IM uint32_t DEVINFO_TypeDef::UNIQUEL | 
Low 32 bits of device unique number
        Definition at line
        
         65
        
        of file
        
         ezr32lg_devinfo.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_devinfo.h