MSC_TypeDef Struct ReferenceDevices > EZR32LG_MSC
       Definition at line
       
        48
       
       of file
       
        ezr32lg_msc.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | ADDRB | 
| __IM uint32_t | CACHEHITS | 
| __IM uint32_t | CACHEMISSES | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | MASSLOCK | 
| __IOM uint32_t | READCTRL | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [3] | 
| uint32_t | RESERVED2 [1] | 
| __IM uint32_t | STATUS | 
| __IOM uint32_t | TIMEBASE | 
| __IOM uint32_t | WDATA | 
| __IOM uint32_t | WRITECMD | 
| __IOM uint32_t | WRITECTRL | 
Field Documentation
| __IOM uint32_t MSC_TypeDef::ADDRB | 
Page Erase/Write Address Buffer
        Definition at line
        
         53
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IM uint32_t MSC_TypeDef::CACHEHITS | 
Cache Hits Performance Counter
        Definition at line
        
         66
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IM uint32_t MSC_TypeDef::CACHEMISSES | 
Cache Misses Performance Counter
        Definition at line
        
         67
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::CMD | 
Command Register
        Definition at line
        
         65
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::CTRL | 
Memory System Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         63
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IM uint32_t MSC_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         60
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         62
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         61
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         64
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::MASSLOCK | 
Mass Erase Lock Register
        Definition at line
        
         70
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::READCTRL | 
Read Control Register
        Definition at line
        
         50
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| uint32_t MSC_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         55
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| uint32_t MSC_TypeDef::RESERVED1[3] | 
Reserved for future use
        Definition at line
        
         59
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| uint32_t MSC_TypeDef::RESERVED2[1] | 
Reserved for future use
        Definition at line
        
         68
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IM uint32_t MSC_TypeDef::STATUS | 
Status Register
        Definition at line
        
         57
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::TIMEBASE | 
Flash Write and Erase Timebase
        Definition at line
        
         69
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::WDATA | 
Write Data Register
        Definition at line
        
         56
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::WRITECMD | 
Write Command Register
        Definition at line
        
         52
        
        of file
        
         ezr32lg_msc.h
        
        .
       
| __IOM uint32_t MSC_TypeDef::WRITECTRL | 
Write Control Register
        Definition at line
        
         51
        
        of file
        
         ezr32lg_msc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_msc.h