EMUEMLIB
Detailed Description
Energy Management Unit (EMU) Peripheral API.
This module contains functions to control the EMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The EMU handles the different low energy modes in Silicon Labs microcontrollers.
         Data Structures | 
       |
| struct | EMU_BUPDInit_TypeDef | 
| struct | EMU_EM23Init_TypeDef | 
| struct | EMU_EM4Init_TypeDef | 
         Macros | 
       |
| #define | EMU_BUPDINIT_DEFAULT | 
| #define | EMU_EM23INIT_DEFAULT | 
| #define | EMU_EM4INIT_DEFAULT | 
         Enumerations | 
       |
| enum | 
         
          EMU_BODMode_TypeDef
         
         {
          emuBODMode_Active , emuBODMode_Inactive }  | 
       
| enum | 
         
          EMU_EM4Osc_TypeDef
         
         {
          emuEM4Osc_ULFRCO = EMU_EM4CONF_OSC_ULFRCO, emuEM4Osc_LFXO = EMU_EM4CONF_OSC_LFXO, emuEM4Osc_LFRCO = EMU_EM4CONF_OSC_LFRCO }  | 
       
| enum | 
         
          EMU_Power_TypeDef
         
         {
          emuPower_None = EMU_BUINACT_PWRCON_NONE, emuPower_BUMain = EMU_BUINACT_PWRCON_BUMAIN, emuPower_MainBU = EMU_BUINACT_PWRCON_MAINBU, emuPower_NoDiode = EMU_BUINACT_PWRCON_NODIODE }  | 
       
| enum | EMU_PowerConfig_TypeDef { emuPowerConfig_DcdcToDvdd } | 
| enum | 
         
          EMU_Probe_TypeDef
         
         {
          emuProbe_Disable = EMU_BUCTRL_PROBE_DISABLE, emuProbe_VDDDReg = EMU_BUCTRL_PROBE_VDDDREG, emuProbe_BUIN = EMU_BUCTRL_PROBE_BUIN, emuProbe_BUOUT = EMU_BUCTRL_PROBE_BUOUT }  | 
       
| enum | 
         
          EMU_Resistor_TypeDef
         
         {
          emuRes_Res0 = EMU_PWRCONF_PWRRES_RES0, emuRes_Res1 = EMU_PWRCONF_PWRRES_RES1, emuRes_Res2 = EMU_PWRCONF_PWRRES_RES2, emuRes_Res3 = EMU_PWRCONF_PWRRES_RES3 }  | 
       
         Functions | 
       |
| void | EMU_BUPDInit (const EMU_BUPDInit_TypeDef *bupdInit) | 
| 
         Configure Backup Power Domain settings.
          | 
       |
| __STATIC_INLINE void | EMU_BUPinEnable (bool enable) | 
| 
         Disable BU_VIN support.
          | 
       |
| __STATIC_INLINE void | EMU_BUReady (void) | 
| 
         Halts until backup power functionality is ready.
          | 
       |
| void | EMU_BUThresholdSet ( EMU_BODMode_TypeDef mode, uint32_t value) | 
| 
         Configure the Backup Power Domain BOD Threshold value.
          | 
       |
| void | EMU_BUThresRangeSet ( EMU_BODMode_TypeDef mode, uint32_t value) | 
| 
         Configure the Backup Power Domain BOD Threshold Range.
          | 
       |
| void | EMU_DCDCConductionModeSet (EMU_DcdcConductionMode_TypeDef conductionMode, bool rcoDefaultSet) | 
| 
         Set DCDC LN regulator conduction mode.
          | 
       |
| bool | EMU_DCDCInit (const EMU_DCDCInit_TypeDef *dcdcInit) | 
| 
         Configure the DCDC regulator.
          | 
       |
| void | EMU_DCDCLnRcoBandSet (EMU_DcdcLnRcoBand_TypeDef band) | 
| 
         Set DCDC Low-noise RCO band.
          | 
       |
| void | EMU_DCDCModeSet (EMU_DcdcMode_TypeDef dcdcMode) | 
| 
         Set DCDC regulator operating mode.
          | 
       |
| void | EMU_DCDCOptimizeSlice (uint32_t em0LoadCurrentmA) | 
| 
         Optimize the DCDC slice count based on the estimated average load current in EM0.
          | 
       |
| bool | EMU_DCDCOutputVoltageSet (uint32_t mV, bool setLpVoltage, bool setLnVoltage) | 
| 
         Set the DCDC output voltage.
          | 
       |
| bool | EMU_DCDCPowerOff (void) | 
| 
         Power off the DCDC regulator.
          | 
       |
| void | EMU_EM23Init (const EMU_EM23Init_TypeDef *em23Init) | 
| 
         Update the EMU module with Energy Mode 2 and 3 configuration.
          | 
       |
| __STATIC_INLINE void | EMU_EM2Block (void) | 
| 
         Block entering EM2 or higher number energy modes.
          | 
       |
| __STATIC_INLINE void | EMU_EM2UnBlock (void) | 
| 
         Unblock entering EM2 or higher number energy modes.
          | 
       |
| void | EMU_EM4Init (const EMU_EM4Init_TypeDef *em4Init) | 
| 
         Update the EMU module with Energy Mode 4 configuration.
          | 
       |
| __STATIC_INLINE void | EMU_EM4Lock (bool enable) | 
| 
         Enable or disable EM4 lock configuration.
          | 
       |
| __STATIC_INLINE void | EMU_EnterEM1 (void) | 
| 
         Enter energy mode 1 (EM1).
          | 
       |
| void | EMU_EnterEM2 (bool restore) | 
| 
         Enter energy mode 2 (EM2).
          | 
       |
| void | EMU_EnterEM3 (bool restore) | 
| 
         Enter energy mode 3 (EM3).
          | 
       |
| void | EMU_EnterEM4 (void) | 
| 
         Enter energy mode 4 (EM4).
          | 
       |
| __STATIC_INLINE void | EMU_IntClear (uint32_t flags) | 
| 
         Clear one or more pending EMU interrupts.
          | 
       |
| __STATIC_INLINE void | EMU_IntDisable (uint32_t flags) | 
| 
         Disable one or more EMU interrupts.
          | 
       |
| __STATIC_INLINE void | EMU_IntEnable (uint32_t flags) | 
| 
         Enable one or more EMU interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | EMU_IntGet (void) | 
| 
         Get pending EMU interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | EMU_IntGetEnabled (void) | 
| 
         Get enabled and pending EMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
          | 
       |
| __STATIC_INLINE void | EMU_IntSet (uint32_t flags) | 
| 
         Set one or more pending EMU interrupts.
          | 
       |
| __STATIC_INLINE void | EMU_Lock (void) | 
| 
         Lock EMU registers in order to protect them against unintended modification.
          | 
       |
| void | EMU_MemPwrDown (uint32_t blocks) | 
| 
         Power down memory block.
          | 
       |
| void | EMU_RamPowerDown (uint32_t start, uint32_t end) | 
| 
         Power down RAM memory blocks.
          | 
       |
| void | EMU_RamPowerUp (void) | 
| 
         Power up all available RAM memory blocks.
          | 
       |
| void | EMU_Restore (void) | 
| 
         Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after
         
          EMU_EnterEM2()
         
         or
         
          EMU_EnterEM3()
         
         are called with the restore parameter set to false. Calling this function is equivalent to calling
         
          EMU_EnterEM2()
         
         or
         
          EMU_EnterEM3()
         
         with the restore parameter set to true, but it allows the application to evaluate the wakeup reason before restoring state.
          | 
       |
| void | EMU_Save (void) | 
| 
         Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before
         
          EMU_EnterEM2()
         
         or
         
          EMU_EnterEM3()
         
         are called with the restore parameter set to false. Calling this function is equivalent to calling
         
          EMU_EnterEM2()
         
         or
         
          EMU_EnterEM3()
         
         with the restore parameter set to true, but it allows the state to be saved without going to sleep. The state can be restored manually by calling
         
          EMU_Restore()
         
         .
          | 
       |
| __STATIC_INLINE void | EMU_Unlock (void) | 
| 
         Unlock the EMU so that writing to locked registers again is possible.
          | 
       |
| void | EMU_UpdateOscConfig (void) | 
| 
         Update EMU module with CMU oscillator selection/enable status.
          | 
       |
Macro Definition Documentation
| #define EMU_BUPDINIT_DEFAULT | 
Default Backup Power Domain configuration.
        Definition at line
        
         553
        
        of file
        
         em_emu.h
        
        .
       
| #define EMU_EM23INIT_DEFAULT | 
Default initialization of EM2 and 3 configuration.
        Definition at line
        
         458
        
        of file
        
         em_emu.h
        
        .
       
Referenced by BSP_initEmu() .
| #define EMU_EM4INIT_DEFAULT | 
Default initialization of EM4 configuration (Series 0).
        Definition at line
        
         490
        
        of file
        
         em_emu.h
        
        .
       
Referenced by UTIL_shutdown() .
Enumeration Type Documentation
| enum EMU_BODMode_TypeDef | 
| enum EMU_EM4Osc_TypeDef | 
| enum EMU_Power_TypeDef | 
Backup Power Domain power connection.
        Definition at line
        
         102
        
        of file
        
         em_emu.h
        
        .
       
| enum EMU_Probe_TypeDef | 
| enum EMU_Resistor_TypeDef | 
Backup Power Domain resistor selection.
        Definition at line
        
         88
        
        of file
        
         em_emu.h
        
        .
       
Function Documentation
| void EMU_BUPDInit | ( | const EMU_BUPDInit_TypeDef * | 
           
            bupdInit
           
           | 
          ) | 
Configure Backup Power Domain settings.
- Parameters
 - 
         
[in] bupdInitBackup power domain initialization structure.  
        Definition at line
        
         1298
        
        of file
        
         em_emu.c
        
        .
       
References _EMU_BUACT_PWRCON_MASK , _EMU_BUCTRL_BODCAL_MASK , _EMU_BUCTRL_BODCAL_SHIFT , _EMU_BUCTRL_EN_MASK , _EMU_BUCTRL_EN_SHIFT , _EMU_BUCTRL_PROBE_MASK , _EMU_BUCTRL_STATEN_MASK , _EMU_BUCTRL_STATEN_SHIFT , _EMU_BUINACT_PWRCON_MASK , _EMU_PWRCONF_PWRRES_MASK , _EMU_PWRCONF_VOUTMED_MASK , _EMU_PWRCONF_VOUTMED_SHIFT , _EMU_PWRCONF_VOUTSTRONG_MASK , _EMU_PWRCONF_VOUTSTRONG_SHIFT , _EMU_PWRCONF_VOUTWEAK_MASK , _EMU_PWRCONF_VOUTWEAK_SHIFT , _RMU_CTRL_BURSTEN_SHIFT , EMU_BUPDInit_TypeDef::activePower , EMU_BUPDInit_TypeDef::bodCal , BUS_RegBitWrite() , EMU , EMU_BUPinEnable() , EMU_BUPDInit_TypeDef::enable , EMU_BUPDInit_TypeDef::inactivePower , EMU_BUPDInit_TypeDef::probe , EMU_BUPDInit_TypeDef::resistor , RMU , EMU_BUPDInit_TypeDef::statusPinEnable , EMU_BUPDInit_TypeDef::voutMed , EMU_BUPDInit_TypeDef::voutStrong , and EMU_BUPDInit_TypeDef::voutWeak .
| __STATIC_INLINE void EMU_BUPinEnable | ( | bool | 
           
            enable
           
           | 
          ) | 
Disable BU_VIN support.
- Parameters
 - 
         
[in] enableIf true, enables BU_VIN input pin support, if false disables it.  
        Definition at line
        
         944
        
        of file
        
         em_emu.h
        
        .
       
References _EMU_ROUTE_BUVINPEN_SHIFT , BUS_RegBitWrite() , and EMU .
Referenced by EMU_BUPDInit() .
| void EMU_BUThresholdSet | ( | EMU_BODMode_TypeDef | 
           
            mode,
           
           | 
         
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Configure the Backup Power Domain BOD Threshold value.
- Note
 - These values are precalibrated.
 
- Parameters
 - 
         
[in] modeActive or Inactive mode [in] value 
        Definition at line
        
         1356
        
        of file
        
         em_emu.c
        
        .
       
References _EMU_BUACT_BUEXTHRES_MASK , _EMU_BUACT_BUEXTHRES_SHIFT , _EMU_BUINACT_BUENTHRES_MASK , _EMU_BUINACT_BUENTHRES_SHIFT , EMU , emuBODMode_Active , and emuBODMode_Inactive .
| void EMU_BUThresRangeSet | ( | EMU_BODMode_TypeDef | 
           
            mode,
           
           | 
         
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Configure the Backup Power Domain BOD Threshold Range.
- Note
 - These values are precalibrated.
 
- Parameters
 - 
         
[in] modeActive or Inactive mode [in] value 
        Definition at line
        
         1381
        
        of file
        
         em_emu.c
        
        .
       
References _EMU_BUACT_BUEXRANGE_MASK , _EMU_BUACT_BUEXRANGE_SHIFT , _EMU_BUINACT_BUENRANGE_MASK , _EMU_BUINACT_BUENRANGE_SHIFT , EMU , emuBODMode_Active , and emuBODMode_Inactive .
| void EMU_DCDCConductionModeSet | ( | EMU_DcdcConductionMode_TypeDef | 
           
            conductionMode,
           
           | 
         
| bool | 
           
            rcoDefaultSet
           
           | 
         ||
| ) | 
Set DCDC LN regulator conduction mode.
- Parameters
 - 
         
[in] conductionModeDCDC LN conduction mode. [in] rcoDefaultSetThe default DCDC RCO band for the conductionMode will be used if true. Otherwise, the current RCO configuration is used.  
        Definition at line
        
         1940
        
        of file
        
         em_emu.c
        
        .
       
References EMU , EMU_DCDCLnRcoBandSet() , EMU_DCDCModeSet() , EMU_DCDCOptimizeSlice() , EMU_IntClear() , and EMU_IntGet() .
| bool EMU_DCDCInit | ( | const EMU_DCDCInit_TypeDef * | 
           
            dcdcInit
           
           | 
          ) | 
Configure the DCDC regulator.
- Note
 - Do not call this function if the power circuit is configured for NODCDC as described in the Power Configurations section of the Reference Manual. Instead, call EMU_DCDCPowerOff() .
 
- Parameters
 - 
         
[in] dcdcInitThe DCDC initialization structure.  
- Returns
 - True if initialization parameters are valid.
 
        Definition at line
        
         1994
        
        of file
        
         em_emu.c
        
        .
       
References BUS_RegBitWrite() , EMU , EMU_DCDCModeSet() , EMU_DCDCOptimizeSlice() , and EMU_DCDCOutputVoltageSet() .
| void EMU_DCDCLnRcoBandSet | ( | EMU_DcdcLnRcoBand_TypeDef | 
           
            band
           
           | 
          ) | 
Set DCDC Low-noise RCO band.
- Parameters
 - 
         
[in] bandRCO band to set.  
        Definition at line
        
         2348
        
        of file
        
         em_emu.c
        
        .
       
References BUS_RegBitRead() , EMU , and EMU_DCDCOptimizeSlice() .
Referenced by EMU_DCDCConductionModeSet() .
| void EMU_DCDCModeSet | ( | EMU_DcdcMode_TypeDef | 
           
            dcdcMode
           
           | 
          ) | 
Set DCDC regulator operating mode.
- Parameters
 - 
         
[in] dcdcModeDCDC mode.  
        Definition at line
        
         1868
        
        of file
        
         em_emu.c
        
        .
       
References BUS_RegBitWrite() , EMU , EMU_IntClear() , and EMU_IntGet() .
Referenced by EMU_DCDCConductionModeSet() , EMU_DCDCInit() , and EMU_EnterEM4() .
| void EMU_DCDCOptimizeSlice | ( | uint32_t | 
           
            em0LoadCurrentmA
           
           | 
          ) | 
Optimize the DCDC slice count based on the estimated average load current in EM0.
- Parameters
 - 
         
[in] em0LoadCurrent_mAEstimated average EM0 load current in mA.  
        Definition at line
        
         2289
        
        of file
        
         em_emu.c
        
        .
       
References EMU .
Referenced by EMU_DCDCConductionModeSet() , EMU_DCDCInit() , and EMU_DCDCLnRcoBandSet() .
| bool EMU_DCDCOutputVoltageSet | ( | uint32_t | 
           
            mV,
           
           | 
         
| bool | 
           
            setLpVoltage,
           
           | 
         ||
| bool | 
           
            setLnVoltage
           
           | 
         ||
| ) | 
Set the DCDC output voltage.
- Parameters
 - 
         
[in] mVTarget DCDC output voltage in mV.  
- Returns
 - True if the mV parameter is valid.
 
        Definition at line
        
         2138
        
        of file
        
         em_emu.c
        
        .
       
References DEVINFO , EMU , SL_MAX , and SL_MIN .
Referenced by EMU_DCDCInit() .
| bool EMU_DCDCPowerOff | ( | void | 
           
           
           | 
          ) | 
Power off the DCDC regulator.
This function powers off the DCDC controller. This function should only be used if the external power circuit is wired for no DCDC. If the external power circuit is wired for DCDC usage, use EMU_DCDCInit() and set the DCDC in bypass mode to disable DCDC.
- Returns
 - Return false if the DCDC could not be disabled.
 
        Definition at line
        
         2377
        
        of file
        
         em_emu.c
        
        .
       
References EMU .
| void EMU_EM23Init | ( | const EMU_EM23Init_TypeDef * | 
           
            em23Init
           
           | 
          ) | 
Update the EMU module with Energy Mode 2 and 3 configuration.
- Parameters
 - 
         
[in] em23InitEnergy Mode 2 and 3 configuration structure.  
        Definition at line
        
         1213
        
        of file
        
         em_emu.c
        
        .
       
References EMU_EM23Init_TypeDef::em23VregFullEn , EMU , and EMU_CTRL_EMVREG .
Referenced by BSP_initEmu() .
| void EMU_EM4Init | ( | const EMU_EM4Init_TypeDef * | 
           
            em4Init
           
           | 
          ) | 
Update the EMU module with Energy Mode 4 configuration.
- Parameters
 - 
         
[in] em4InitEnergy Mode 4 configuration structure.  
        Definition at line
        
         1239
        
        of file
        
         em_emu.c
        
        .
       
References _EMU_EM4CONF_BUBODRSTDIS_MASK , _EMU_EM4CONF_BUBODRSTDIS_SHIFT , _EMU_EM4CONF_BURTCWU_MASK , _EMU_EM4CONF_BURTCWU_SHIFT , _EMU_EM4CONF_LOCKCONF_MASK , _EMU_EM4CONF_LOCKCONF_SHIFT , _EMU_EM4CONF_OSC_MASK , _EMU_EM4CONF_VREGEN_MASK , _EMU_EM4CONF_VREGEN_SHIFT , EMU_EM4Init_TypeDef::buBodRstDis , EMU_EM4Init_TypeDef::buRtcWakeup , EMU , EMU_EM4Init_TypeDef::lockConfig , EMU_EM4Init_TypeDef::osc , and EMU_EM4Init_TypeDef::vreg .
Referenced by UTIL_shutdown() .
| __STATIC_INLINE void EMU_EM4Lock | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or disable EM4 lock configuration.
- Parameters
 - 
         
[in] enableIf true, locks down EM4 configuration.  
        Definition at line
        
         919
        
        of file
        
         em_emu.h
        
        .
       
References _EMU_EM4CONF_LOCKCONF_SHIFT , BUS_RegBitWrite() , and EMU .
| void EMU_EnterEM2 | ( | bool | 
           
            restore
           
           | 
          ) | 
Enter energy mode 2 (EM2).
When entering EM2, high-frequency clocks are disabled, i.e., HFXO, HFRCO and AUXHFRCO (for AUXHFRCO, see exception note below). When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM2.
        However, prior to entering EM2, the core may have been using another oscillator than HFRCO. The
        
         restore
        
        parameter gives the user the option to restore all HF oscillators according to state prior to entering EM2, as well as the clock used to clock the core. This restore procedure is handled by SW. However, since handled by SW, it will not be restored before completing the interrupt function(s) waking up the core!
       
- Note
 - If restoring core clock to use the HFXO oscillator, which has been disabled during EM2 mode, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. Such a feature is however outside the scope of the implementation in this function.
 - If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can not be used.
 
- If HFXO is re-enabled by this function, and NOT used to clock the core, this function will not wait for HFXO to stabilize. This must be considered by the application if trying to use features relying on that oscillator upon return.
 
- 
         If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM2. It will thus remain enabled when returning to EM0 regardless of the
         
restoreparameter. 
- 
         If HFXO autostart and select is enabled by using CMU_HFXOAutostartEnable(), the starting and selecting of the core clocks will be identical to the user independently of the value of the
         
restoreparameter when waking up on the wakeup sources corresponding to the autostart and select setting. 
- If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM2 level, then the EM0 level is also restored.
 
Note that the hardware will automatically update the HFRCO frequency in the case where voltage scaling is used in EM2/EM3 and not in EM0/EM1. When the restore argument to this function is true then software will restore the original HFRCO frequency after EM2/EM3 wake up. If the restore argument is false then the HFRCO frequency is 19 MHz when coming out of EM2/EM3 and all wait states are at a safe value.
- Parameters
 - 
         
[in] restore- true - save and restore oscillators, clocks and voltage scaling, see function details.
 - false - do not save and restore oscillators and clocks, see function details.
 
 
- 
         The
         
restoreoption should only be used if all clock control is done via the CMU API. 
        Definition at line
        
         545
        
        of file
        
         em_emu.c
        
        .
       
References CORE_CRITICAL_SECTION , and SystemCoreClockUpdate() .
Referenced by CAPLESENSE_Sleep() , UTIL_sleep() , and UTIL_waitForEvent() .
| void EMU_EnterEM3 | ( | bool | 
           
            restore
           
           | 
          ) | 
Enter energy mode 3 (EM3).
When entering EM3, the high-frequency clocks are disabled by hardware, i.e., HFXO, HFRCO, and AUXHFRCO (for AUXHFRCO, see exception note below). In addition, the low-frequency clocks, i.e., LFXO and LFRCO are disabled by software. When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM3.
        However, prior to entering EM3, the core may have been using an oscillator other than HFRCO. The
        
         restore
        
        parameter gives the user the option to restore all HF/LF oscillators according to state prior to entering EM3, as well as the clock used to clock the core. This restore procedure is handled by software. However, since it is handled by software, it will not be restored before completing the interrupt function(s) waking up the core!
       
- Note
 - If restoring core clock to use an oscillator other than HFRCO, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. This feature is, however, outside the scope of the implementation in this function.
 - If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can't be used.
 
- If HFXO/LFXO/LFRCO are re-enabled by this function, and NOT used to clock the core, this function will not wait for those oscillators to stabilize. This must be considered by the application if trying to use features relying on those oscillators upon return.
 
- 
         If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM3. It will, therefore, remain enabled when returning to EM0 regardless of the
         
restoreparameter. 
- If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM3 level, then the EM0 level is also restored.
 
- Parameters
 - 
         
[in] restore- true - save and restore oscillators, clocks and voltage scaling, see function details.
 - false - do not save and restore oscillators and clocks, see function details.
 
 
- 
         The
         
restoreoption should only be used if all clock control is done via the CMU API. 
        Definition at line
        
         670
        
        of file
        
         em_emu.c
        
        .
       
References CMU , CMU_Lock() , CMU_LOCK_LOCKKEY_LOCKED , CMU_OSCENCMD_LFRCODIS , CMU_OSCENCMD_LFXODIS , CMU_Unlock() , CORE_CRITICAL_SECTION , and SystemCoreClockUpdate() .
| void EMU_EnterEM4 | ( | void | 
           
           
           | 
          ) | 
Enter energy mode 4 (EM4).
- Note
 - Only a power on reset or external reset pin can wake the device from EM4.
 
        Definition at line
        
         794
        
        of file
        
         em_emu.c
        
        .
       
References _EMU_CTRL_EM4CTRL_MASK , _EMU_CTRL_EM4CTRL_SHIFT , BUS_RegMaskedClear() , CMU , CMU_OSCENCMD_HFRCOEN , CMU_STATUS_HFRCORDY , DEVINFO , EMU , EMU_BASE , EMU_DCDCModeSet() , and EMU_Unlock() .
Referenced by UTIL_shutdown() .
| __STATIC_INLINE void EMU_IntClear | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Clear one or more pending EMU interrupts.
- Parameters
 - 
         
[in] flagsPending EMU interrupt sources to clear. Use one or more valid interrupt flags for the EMU module (EMU_IFC_nnn).  
        Definition at line
        
         824
        
        of file
        
         em_emu.h
        
        .
       
References EMU .
Referenced by disableInterrupts() , EMU_DCDCConductionModeSet() , EMU_DCDCModeSet() , and TEMPDRV_IRQHandler() .
| __STATIC_INLINE void EMU_IntDisable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Disable one or more EMU interrupts.
- Parameters
 - 
         
[in] flagsEMU interrupt sources to disable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn).  
        Definition at line
        
         837
        
        of file
        
         em_emu.h
        
        .
       
References EMU .
Referenced by disableInterrupts() , and updateInterrupts() .
| __STATIC_INLINE void EMU_IntEnable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Enable one or more EMU interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using EMU_IntClear() prior to enabling the interrupt.
 
- Parameters
 - 
         
[in] flagsEMU interrupt sources to enable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn).  
        Definition at line
        
         855
        
        of file
        
         em_emu.h
        
        .
       
References EMU .
Referenced by updateInterrupts() .
| __STATIC_INLINE uint32_t EMU_IntGet | ( | void | 
           
           
           | 
          ) | 
Get pending EMU interrupt flags.
- Note
 - Event bits are not cleared by the use of this function.
 
- Returns
 - EMU interrupt sources pending. Returns one or more valid interrupt flags for the EMU module (EMU_IF_nnn).
 
        Definition at line
        
         871
        
        of file
        
         em_emu.h
        
        .
       
References EMU .
Referenced by EMU_DCDCConductionModeSet() , and EMU_DCDCModeSet() .
| __STATIC_INLINE uint32_t EMU_IntGetEnabled | ( | void | 
           
           
           | 
          ) | 
Get enabled and pending EMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Interrupt flags are not cleared by the use of this function.
 
- Returns
 - 
         Pending and enabled EMU interrupt sources Return value is the bitwise AND of
         
- the enabled interrupt sources in EMU_IEN and
 - the pending interrupt flags EMU_IF.
 
 
        Definition at line
        
         890
        
        of file
        
         em_emu.h
        
        .
       
References EMU .
Referenced by TEMPDRV_IRQHandler() .
| __STATIC_INLINE void EMU_IntSet | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Set one or more pending EMU interrupts.
- Parameters
 - 
         
[in] flagsEMU interrupt sources to set to pending. Use one or more valid interrupt flags for the EMU module (EMU_IFS_nnn).  
        Definition at line
        
         906
        
        of file
        
         em_emu.h
        
        .
       
References EMU .
| __STATIC_INLINE void EMU_Lock | ( | void | 
           
           
           | 
          ) | 
Lock EMU registers in order to protect them against unintended modification.
- Note
 - If locking EMU registers, they must be unlocked prior to using any EMU API functions modifying EMU registers, excluding interrupt control and regulator control if the architecture has a EMU_PWRCTRL register. An exception to this is the energy mode entering API (EMU_EnterEMn()), which can be used when the EMU registers are locked.
 
        Definition at line
        
         962
        
        of file
        
         em_emu.h
        
        .
       
References EMU , and EMU_LOCK_LOCKKEY_LOCK .
Referenced by RMU_ResetCauseClear() .
| void EMU_MemPwrDown | ( | uint32_t | 
           
            blocks
           
           | 
          ) | 
Power down memory block.
- Parameters
 - 
         
[in] blocksSpecifies a logical OR of bits indicating memory blocks to power down. Bit 0 selects block 1, bit 1 selects block 2, and so on. Memory block 0 cannot be disabled. See the reference manual for available memory blocks for a device.  
- Note
 - Only a POR reset can power up the specified memory block(s) after power down.
 
- Deprecated:
 - This function is deprecated, use EMU_RamPowerDown() instead which maps a user provided memory range into RAM blocks to power down.
 
        Definition at line
        
         932
        
        of file
        
         em_emu.c
        
        .
       
References EMU .
| void EMU_RamPowerDown | ( | uint32_t | 
           
            start,
           
           | 
         
| uint32_t | 
           
            end
           
           | 
         ||
| ) | 
Power down RAM memory blocks.
This function will power down all the RAM blocks that are within a given range. The RAM block layout is different between device families, so this function can be used in a generic way to power down a RAM memory region which is known to be unused.
This function will only power down blocks which are completely enclosed by the memory range given by [start, end).
This is an example to power down all RAM blocks except the first one. The first RAM block is special in that it cannot be powered down by the hardware. The size of the first RAM block is device-specific. See the reference manual to find the RAM block sizes.
- Note
 - Only a reset can power up the specified memory block(s) after power down on a series 0 device.
 
- Parameters
 - 
         
[in] startThe start address of the RAM region to power down. This address is inclusive. [in] endThe end address of the RAM region to power down. This address is exclusive. If this parameter is 0, all RAM blocks contained in the region from start to the upper RAM address will be powered down.  
        Definition at line
        
         978
        
        of file
        
         em_emu.c
        
        .
       
References EMU , RAM_MEM_BASE , SRAM_BASE , and SRAM_SIZE .
| void EMU_RamPowerUp | ( | void | 
           
           
           | 
          ) | 
Power up all available RAM memory blocks.
This function will power up all the RAM blocks on a device, this means that the RAM blocks are retained in EM2/EM3. Note that this functionality is not supported on Series 0 devices. Only a reset will power up the RAM blocks on a series 0 device.
        Definition at line
        
         1050
        
        of file
        
         em_emu.c
        
        .
       
References EMU .
| void EMU_UpdateOscConfig | ( | void | 
           
           
           | 
          ) | 
Update EMU module with CMU oscillator selection/enable status.
- Deprecated:
 - Oscillator status is saved in EMU_EnterEM2() and EMU_EnterEM3() .
 
        Definition at line
        
         1094
        
        of file
        
         em_emu.c
        
        .