DMA_CfgChannel_TypeDef Struct ReferenceEMLIB > DMA
Configuration structure for a channel.
       Definition at line
       
        159
       
       of file
       
        em_dma.h
       
       .
      
      
       #include <
       
     
        em_dma.h
       
       >
      
         Data Fields | 
       |
| DMA_CB_TypeDef * | cb | 
| 
         User definable callback handling configuration.
          | 
       |
| bool | enableInt | 
| bool | highPri | 
| uint32_t | select | 
Field Documentation
| DMA_CB_TypeDef * DMA_CfgChannel_TypeDef::cb | 
User definable callback handling configuration.
Refer to structure definition for details. The callback is invoked when specified DMA cycle is complete (when dma_done signal asserted). Callback is invoked in interrupt context, and should be efficient and non-blocking. Set to NULL to not use the callback feature.
- Note
 - Referenced structure is used by the interrupt handler, and must be available until no longer used. Thus, in most cases it should not be located on the stack.
 
        Definition at line
        
         196
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgChannel() .
| bool DMA_CfgChannel_TypeDef::enableInt | 
Select if interrupt will be enabled for channel (triggering interrupt handler when dma_done signal is asserted). It should normally be enabled if using the callback feature for a channel, and disabled if not using the callback feature.
        Definition at line
        
         173
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgChannel() .
| bool DMA_CfgChannel_TypeDef::highPri | 
Select if channel priority is in the high or default priority group with respect to arbitration. Within a priority group, lower numbered channels have higher priority than higher numbered channels.
        Definition at line
        
         165
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgChannel() .
| uint32_t DMA_CfgChannel_TypeDef::select | 
Channel control specifying the source of DMA signals. If accessing peripherals, use one of the DMAREQ_nnn defines available for the peripheral. Set to 0 for memory-to-memory DMA cycles.
        Definition at line
        
         180
        
        of file
        
         em_dma.h
        
        .
       
Referenced by DMA_CfgChannel() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_dma.h