USB_HC_TypeDef Struct ReferenceDevices
USB_HC EZR32LG USB HC.
       Definition at line
       
        46
       
       of file
       
        ezr32lg_usb_hc.h
       
       .
      
      
       #include <
       
     
        ezr32lg_usb_hc.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | CHAR | 
| __IOM uint32_t | DMAADDR | 
| __IOM uint32_t | INT | 
| __IOM uint32_t | INTMSK | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [2] | 
| __IOM uint32_t | TSIZ | 
Field Documentation
| __IOM uint32_t USB_HC_TypeDef::CHAR | 
Host Channel x Characteristics Register
        Definition at line
        
         47
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
| __IOM uint32_t USB_HC_TypeDef::DMAADDR | 
Host Channel x DMA Address Register
        Definition at line
        
         52
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
| __IOM uint32_t USB_HC_TypeDef::INT | 
Host Channel x Interrupt Register
        Definition at line
        
         49
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
| __IOM uint32_t USB_HC_TypeDef::INTMSK | 
Host Channel x Interrupt Mask Register
        Definition at line
        
         50
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
| uint32_t USB_HC_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         48
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
| uint32_t USB_HC_TypeDef::RESERVED1[2] | 
Reserved future
        Definition at line
        
         53
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
| __IOM uint32_t USB_HC_TypeDef::TSIZ | 
Host Channel x Transfer Size Register
        Definition at line
        
         51
        
        of file
        
         ezr32lg_usb_hc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_usb_hc.h