EMU_TypeDef Struct ReferenceDevices > EZR32LG_EMU
       Definition at line
       
        48
       
       of file
       
        ezr32lg_emu.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | AUXCTRL | 
| __IOM uint32_t | BUACT | 
| __IOM uint32_t | BUBODBUVINCAL | 
| __IOM uint32_t | BUBODUNREGCAL | 
| __IOM uint32_t | BUCTRL | 
| __IOM uint32_t | BUINACT | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | EM4CONF | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | PWRCONF | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [6] | 
| uint32_t | RESERVED2 [1] | 
| __IOM uint32_t | ROUTE | 
| __IM uint32_t | STATUS | 
Field Documentation
| __IOM uint32_t EMU_TypeDef::AUXCTRL | 
Auxiliary Control Register
        Definition at line
        
         55
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::BUACT | 
Backup mode active configuration register
        Definition at line
        
         62
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::BUBODBUVINCAL | 
BU_VIN Backup BOD calibration
        Definition at line
        
         69
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::BUBODUNREGCAL | 
Unregulated power Backup BOD calibration
        Definition at line
        
         70
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::BUCTRL | 
Backup Power configuration register
        Definition at line
        
         59
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::BUINACT | 
Backup mode inactive configuration register
        Definition at line
        
         61
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::EM4CONF | 
Energy mode 4 configuration register
        Definition at line
        
         58
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         68
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         65
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         67
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         66
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         52
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::PWRCONF | 
Power connection configuration register
        Definition at line
        
         60
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         51
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED1[6] | 
Reserved for future use
        Definition at line
        
         54
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED2[1] | 
Reserved for future use
        Definition at line
        
         57
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::ROUTE | 
I/O Routing Register
        Definition at line
        
         64
        
        of file
        
         ezr32lg_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::STATUS | 
Status register
        Definition at line
        
         63
        
        of file
        
         ezr32lg_emu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_emu.h