AES_TypeDef Struct ReferenceDevices > EZR32LG_AES
       Definition at line
       
        48
       
       of file
       
        ezr32lg_aes.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DATA | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | KEYHA | 
| __IOM uint32_t | KEYHB | 
| __IOM uint32_t | KEYHC | 
| __IOM uint32_t | KEYHD | 
| __IOM uint32_t | KEYLA | 
| __IOM uint32_t | KEYLB | 
| __IOM uint32_t | KEYLC | 
| __IOM uint32_t | KEYLD | 
| uint32_t | RESERVED0 [3] | 
| __IM uint32_t | STATUS | 
| __IOM uint32_t | XORDATA | 
Field Documentation
| __IOM uint32_t AES_TypeDef::CMD | 
Command Register
        Definition at line
        
         50
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::DATA | 
DATA Register
        Definition at line
        
         56
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         52
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IM uint32_t AES_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         53
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         55
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         54
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYHA | 
KEY High Register
        Definition at line
        
         63
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYHB | 
KEY High Register
        Definition at line
        
         64
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYHC | 
KEY High Register
        Definition at line
        
         65
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYHD | 
KEY High Register
        Definition at line
        
         66
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYLA | 
KEY Low Register
        Definition at line
        
         59
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYLB | 
KEY Low Register
        Definition at line
        
         60
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYLC | 
KEY Low Register
        Definition at line
        
         61
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::KEYLD | 
KEY Low Register
        Definition at line
        
         62
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| uint32_t AES_TypeDef::RESERVED0[3] | 
Reserved for future use
        Definition at line
        
         58
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IM uint32_t AES_TypeDef::STATUS | 
Status Register
        Definition at line
        
         51
        
        of file
        
         ezr32lg_aes.h
        
        .
       
| __IOM uint32_t AES_TypeDef::XORDATA | 
XORDATA Register
        Definition at line
        
         57
        
        of file
        
         ezr32lg_aes.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_aes.h