CALIBRATE_TypeDef Struct ReferenceDevices > EZR32LG_CALIBRATE
       Definition at line
       
        49
       
       of file
       
        ezr32lg_calibrate.h
       
       .
      
         Data Fields | 
       |
| __IM uint32_t | ADDRESS | 
| __IM uint32_t | VALUE | 
Field Documentation
| __IM uint32_t CALIBRATE_TypeDef::ADDRESS | 
Address of calibration register
        Definition at line
        
         50
        
        of file
        
         ezr32lg_calibrate.h
        
        .
       
| __IM uint32_t CALIBRATE_TypeDef::VALUE | 
Default value for calibration register
        Definition at line
        
         51
        
        of file
        
         ezr32lg_calibrate.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_calibrate.h