BURTC_TypeDef Struct ReferenceDevices > EZR32LG_BURTC
       Definition at line
       
        48
       
       of file
       
        ezr32lg_burtc.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | CMD | 
| __IM uint32_t | CNT | 
| __IOM uint32_t | COMP0 | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | FREEZE | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LFXOFDET | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | LPMODE | 
| __IOM uint32_t | POWERDOWN | 
| uint32_t | RESERVED0 [48] | 
| BURTC_RET_TypeDef | RET [128] | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IM uint32_t | TIMESTAMP | 
Field Documentation
| __IOM uint32_t BURTC_TypeDef::CMD | 
Command Register
        Definition at line
        
         56
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IM uint32_t BURTC_TypeDef::CNT | 
Counter Value Register
        Definition at line
        
         51
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::COMP0 | 
Counter Compare Value
        Definition at line
        
         52
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::FREEZE | 
Freeze Register
        Definition at line
        
         64
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         62
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IM uint32_t BURTC_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         59
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         61
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         60
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::LFXOFDET | 
LFXO
        Definition at line
        
         54
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         58
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::LPMODE | 
Low power mode configuration
        Definition at line
        
         50
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IOM uint32_t BURTC_TypeDef::POWERDOWN | 
Retention RAM power-down Register
        Definition at line
        
         57
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| uint32_t BURTC_TypeDef::RESERVED0[48] | 
Reserved registers
        Definition at line
        
         67
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| BURTC_RET_TypeDef BURTC_TypeDef::RET[128] | 
RetentionReg
        Definition at line
        
         68
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IM uint32_t BURTC_TypeDef::STATUS | 
Status Register
        Definition at line
        
         55
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IM uint32_t BURTC_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         65
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
| __IM uint32_t BURTC_TypeDef::TIMESTAMP | 
Backup mode timestamp
        Definition at line
        
         53
        
        of file
        
         ezr32lg_burtc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_burtc.h